Hi,
I need your help guys
… recently I updated my ESP8266 Thing with the NodeMCU Firmware. But now I want to go back on default AT Firmware. I have some problem to Flash Firmware with the latest version of the firmware. I have found nothing on the sparkfun website to talk about it or how to do that.
Firmware : AI-v0.9.5.0 AT Firmware.bin
Flash Tool : ESP8266 Flash Downloader
Address : 0x00000
Error that I receive at the end.
Writing at 0x0007dc00… (99 %)
Writing at 0x0007e000… (99 %)
Writing at 0x0007e400… (99 %)
Writing at 0x0007e800… (99 %)
Writing at 0x0007ec00… (99 %)
Leaving…
Failed to leave Flash mode
I don’t understand what’s is wrong. My final objectif is return the unit with the default AT Firmware latest version.
Regards,