Hi,
I purchased one of these a little while ago and now have time to work on it.
I can load my program OK (via Arduino 1.8.13 on mac, ESP8266 3.0.1 core).
But it quite often fails to boot with the following output. Seems to hand at the ~ld
18:03:14.255 → ets Jan 8 2013,rst cause:1, boot mode:(3,6)
18:03:14.255 →
18:03:14.255 → load 0x4010f000, len 3460, room 16
18:03:14.288 → tail 4
18:03:14.288 → chksum 0xcc
18:03:14.288 → load 0x3fff20b8, len 40, room 4
18:03:14.288 → tail 4
18:03:14.288 → chksum 0xc9
18:03:14.288 → csum 0xc9
18:03:14.288 → v0004d6f0
18:03:14.323 → ~ld
18:03:18.922 →
When it does boot it crashes when attempting to connect to wifi. Note this program is working fine on my older unit with ESP-07
18:00:56.681 → ets Jan 8 2013,rst cause:1, boot mode:(3,6)
18:00:56.681 →
18:00:56.681 → load 0x4010f000, len 3460, room 16
18:00:56.681 → tail 4
18:00:56.681 → chksum 0xcc
18:00:56.681 → load 0x3fff20b8, len 40, room 4
18:00:56.681 → tail 4
18:00:56.681 → chksum 0xc9
18:00:56.681 → csum 0xc9
18:00:56.681 → v0004d6f0
18:00:56.716 → ~ld
18:00:56.753 → Initialising
18:00:56.753 → read rtc memory complete
18:00:56.753 → No valid data - reset to defaults
18:00:56.753 → I/O setup complete
18:00:56.786 → Connecting to Wifi …
18:00:56.786 → …⸮@⸮rjrA(⸮⸮S⸮u⸮К⸮⸮X%(⸮⸮⸮y⸮eh)⸮"8⸮t⸮͊N⸮⸮I
18:01:08.871 → A⸮1⸮-1)dЋUJ!⸮⸮A⸮!⸮N⸮*Q"HhI⸮A,⸮ZMmr,R⸮+⸮⸮YJvA ⸮y⸮!!⸮$|⸮⸮⸮⸮⸮A,⸮[
⸮⸮A,⸮[
G,9E-␟⸮ ⸮x⸮xjxjx⸮x*&⸮"⸮⸮&2⸮⸮($ᑢ⸮V<jxj8j8.x⸮axjxjxjxjx*&⸮V"5⸮⸮"N b⸮(&b⸮⸮⸮⸮ᩡ⸮⸮⸮⸮⸮xjxjx/8jx*⸮hf@n ⸮2F⸮⸮ArF24⸮⸮⸮⸮⸮⸮
18:01:29.586 → ets Jan 8 2013,rst cause:1, boot mode:(3,6)
18:01:29.586 →
18:01:29.586 → load 0x4010f000, len 3460, room 16
18:01:29.586 → tail 4
I has also exceptioned a few times with the output decoded to:
Exception 0: Illegal instruction
PC: 0x40104c02
EXCVADDR: 0x00000000
Decoding stack results
0x40100a23: umm_free_core(umm_heap_context_t*, void*) at /Users/alanforster/Library/Arduino15/packages/esp8266/hardware/esp8266/3.0.1/cores/esp8266/umm_malloc/umm_malloc.cpp line 549
0x40100c02: free(void*) at /Users/alanforster/Library/Arduino15/packages/esp8266/hardware/esp8266/3.0.1/cores/esp8266/umm_malloc/umm_malloc.cpp line 595
0x40209686: loop_task(ETSEvent*) at /Users/alanforster/Library/Arduino15/packages/esp8266/hardware/esp8266/3.0.1/cores/esp8266/core_esp8266_main.cpp line 215
0x401003d4: ets_post(uint8, ETSSignal, ETSParam) at /Users/alanforster/Library/Arduino15/packages/esp8266/hardware/esp8266/3.0.1/cores/esp8266/core_esp8266_main.cpp line 181
0x402021ed: ESP8266WiFiSTAClass::begin(char const*, char const*, int, unsigned char const*, bool) at /Users/alanforster/Library/Arduino15/packages/esp8266/hardware/esp8266/3.0.1/libraries/ESP8266WiFi/src/ESP8266WiFiSTA.cpp line 208
0x402021ca: ESP8266WiFiSTAClass::begin(char const*, char const*, int, unsigned char const*, bool) at /Users/alanforster/Library/Arduino15/packages/esp8266/hardware/esp8266/3.0.1/libraries/ESP8266WiFi/src/ESP8266WiFiSTA.cpp line 204
0x402021f3: ESP8266WiFiSTAClass::begin(char const*, char const*, int, unsigned char const*, bool) at /Users/alanforster/Library/Arduino15/packages/esp8266/hardware/esp8266/3.0.1/libraries/ESP8266WiFi/src/ESP8266WiFiSTA.cpp line 208
0x401004f4: millis() at /Users/alanforster/Library/Arduino15/packages/esp8266/hardware/esp8266/3.0.1/cores/esp8266/core_esp8266_wiring.cpp line 193
0x40100a23: umm_free_core(umm_heap_context_t*, void*) at /Users/alanforster/Library/Arduino15/packages/esp8266/hardware/esp8266/3.0.1/cores/esp8266/umm_malloc/umm_malloc.cpp line 549
0x4020a7dc: uart_write(uart_t*, char const*, size_t) at /Users/alanforster/Library/Arduino15/packages/esp8266/hardware/esp8266/3.0.1/cores/esp8266/uart.cpp line 546
0x40100c2c: malloc(size_t) at /Users/alanforster/Library/Arduino15/packages/esp8266/hardware/esp8266/3.0.1/cores/esp8266/umm_malloc/umm_malloc.cpp line 821
0x4020184c: setup() at /Users/alanforster/Documents/Arduino/ChookDoor/ChookDoor.ino line 349
0x40209830: loop_wrapper() at /Users/alanforster/Library/Arduino15/packages/esp8266/hardware/esp8266/3.0.1/cores/esp8266/core_esp8266_main.cpp line 205
Any thoughts?