Hey all,
Currently I have set up the Arduino pro Mini (3v) and the Ethernet SD shield and running the SDFatInfo code with a software reset for the Ethernet. I have been playing around with some different code and different settings trying to get it to work. Any body know why/what is going on.
Current setup:
Pin 9 digital reset pin
Pin 10’s connected
Pin 4’s connected
Code:
pinMode(WIZNET_RESET_PIN, OUTPUT);
digitalWrite(WIZNET_RESET_PIN, HIGH);
delay(50);
digitalWrite(WIZNET_RESET_PIN, LOW);
delay(50);
digitalWrite(WIZNET_RESET_PIN, HIGH);
delay(100);
pinMode(10, OUTPUT); // set the SS pin as an output (necessary!)
digitalWrite(10, HIGH); // but turn off the W5100 chip!
uint8_t r = card.init(SPI_HALF_SPEED, 4); // Use digital 4 as the SD SS line
Is there a problem with the Pro mini clock speed and the Ethernet shield ...
Serial output I recive
Code:
type any character to start
card.init failed
SD error
errorCode: 1
errorData: 0
type any character to start
Thanks all