Hello,
I`ve heard that it is very tricky to programm external flash-storages; so I want to ask if it is possible to programm a SST_39LF800A (flash) with the JTAG from the µC AT91SAM7SE32. The external flash-RAM is connected to the µC over the data- and address bus. I want to use OpenOCD.
Or is there a better solution to work with another flash-RAM with 8MB with internal JTAG-interface (do you know such a flash-RAM)?
http://www.sst.com/products.xhtml/paral … ST39LF800A
http://www.atmel.org/dyn/resources/prod … /6222s.pdf
with best regards
saoirse