ez430-RF2500 edge trigger help

I am trying to transmit an rpm from a pulse that is getting monitored on P2.0 on the end device.

Seems like my tachCount does not increment. P2.) does not detect it.

I can manually define a number for tachCount and it show up on the AP side. But when I rely on the actual signal. Nothing happens.

Can someone take a look at my interupt routine to see if I am not seeing something?

Thanks

void updateTach(void)

P2IE &= ~(TACH); // Disable tachometer interrupt

_NOP(); // Wait 1 instruction cycle

tachRPM = (tachCount/PULSESPERREVOLUTION)*60;// Convert pulse count to RPM

P2IE |= (TACH); // Re-enable tachometer interrupt

}

// PORT2 Interrupt Service Routine

#pragma vector=PORT2_VECTOR

__interrupt void isrPORT2(void)

{

if (P2IFG & TACH) { // Tachometer pulse detected ?//defined TACH BIT0

tachCount++; // Increment tach counter

P2IFG &= ~TACH; // Clear interrupt flag//

}

}

//Version: ED_rr1.1. addition END

/*------------------------------------------------------------------------------

  • ADC10 interrupt service routine

------------------------------------------------------------------------------*/

#pragma vector=ADC10_VECTOR

__interrupt void ADC10_ISR(void)

{

__bic_SR_register_on_exit(CPUOFF); // Clear CPUOFF bit from 0(SR)

}

/*------------------------------------------------------------------------------

  • Timer A0 interrupt service routine

------------------------------------------------------------------------------*/

#pragma vector=TIMERA0_VECTOR

__interrupt void Timer_A (void)

{

__bic_SR_register_on_exit(LPM3_bits); // Clear LPM3 bit from 0(SR)

}