Is there an efficient way to copy all the user profiles from one Facet mosaic receiver to another? Is there some way via USB to a computer and then from the computer to the second receiver? I feel like I’m overlooking a feature for doing this, and I’m hoping to avoid re-entering by hand several profiles’ worth of settings.
Use an SD card. Generally speaking, the settings on the SD card will overwrite the settings on a unit. So insert an SD card, make all the settings to the unit you need - these settings will be stored both on the local unit and the SD card. Then power down the unit. Insert the SD card into a new Facet mosaic, and upon power up, the unit will mount the SD card, find the settings file, and apply those settings, overwriting any local settings. We like to think of it as a ‘golden card’ system. We tried to design it so that once you have a good setup, you should be able to deploy it quickly.
@sparky If I recall correctly, the uSD card in a Facet mosaic is under the control of the mosaic-X5, rather than the ESP32. Is the ESP32 able to pass a file, containing the user profiles, to the mosaic-X5 for writing to the card? And, also able to request that the mosaic-X5 read such a file from the card and pass it to the ESP32?
@sparky I removed the uSD card from a Facet mosaic (strictly, a Facet mosaic L-Band, but they’re the same, right?) that was configured with multiple user profiles, after powering down that receiver, and placed the card into another Facet mosaic, then powered the latter receiver on. The profiles from the first receiver did not appear on the second receiver. Looking at the contents of the uSD card on a computer, all I see aside from mosaic-X5 log files are an autorun.inf file and a receiver.ico file.
Both receivers are running ESP32 firmware v2.2 and mosaic-X5 firmware 4.15.0.
Is there something I have to explicitly do to cause the creation of the settings file that you referred to?
Thank you for supporting our product - it was a lot of fun to develop. The X5 is such a great chip…
Correct, on Facet mosaic, the SD card is connected directly to the X5, not to the ESP32. The ESP32 has no direct access to it. The upside is that the X5 can log RINEX directly; the downside is that the RTK Everywhere settings are stored in ESP32 flash memory only.
The ESP32 does have limited access to the “Disk” file system through the COM port. It can list disk info (ldi / lstDiskInfo) which includes the total space, free space and the names and sizes of all files. It can list a recorded file (lrf / lstRecordedFile) to the COM port. It can remove a file or files (erf / exeRemoveFile). But I’m not seeing a way to write to a file…
I’ll keep digging. The X5 is so very clever, it’s a full-on embedded computer, there is probably a way. Maybe a way to daisy chain the COM port to DSK1…
I’ll keep thinking about this. If I find anything, I’ll let you know and add it as a Feature Request for the next RTK Everywhere firmware version.
@PaulZC OK, manual copying of profiles for now. Thanks for thinking about ways to automate the process. And I agree, the mosaic-X5 is very cool, and the Facet mosaic is a very nice product.
To write the contents and close the file, I had to unmount the disk. But that’s a minor complication.
So, here’s a way we could transfer the RTK Everywhere configuration from one unit to another:
Add a new “Write profile to X5 DSK” option.
This would write the RTK Everywhere profile(s) to log.ecm as outlined above.
Unmount the SD card (exeManageDisk,DSK1,Unmount).
Powering off the Facet mosaic would probably work too - it sends a exePowerMode,Standby before turning the power off.
User transfers the SD card to the second unit.
Add a new “Read profile from X5 DSK” option.
The ESP32 reads the log.ecm file using lstRecordedFile, strips off the Week Time-Of-Week prefix from each line, writes the plain ASCII text to the profile file (in flash (LittleFS)).
@PaulZC Hi, Paul. Thank you for being so responsive! Another thought: Could something be implemented via USB? Using a USB cable to a computer to get a profiles / settings file from a Facet mosaic’s ESP32, or to send one in the other direction, would be very useful. Might that be easier or cleaner to implement?
If we make the ESP32 code unmount the SD cards, they would appear as mass storage (flash drives) over USB. You could drag and drop the log.ecm file from one to the other.
Or, we could set up a different daisy-chain through the USB1 or USB2 virtual COM ports and use those for the file transfer, but you would need some simple code running on your computer to forward the data from the donor USB to the recipient USB. A few lines of Python would do it. But maybe not a great solution for some users…?
Another solution would be the DATA port → DATA port “crossover cable” idea I described on GitHub.
@PaulZC Thank you again for your consideration of all this. The approach using a crossover cable is my least favorite; it’s nice to avoid special hardware. The few lines of Python approach would be acceptable, as I’m primarily a MacOS / NetBSD / Linux user (I don’t know where that would leave the Windows users).
Out of curiosity, a few minutes ago, I had a Facet mosaic cabled to a MacBook that’s running Mint Linux (that computer is my support tool for my Facet mosaic receivers). I used the mosaic-X5’s web interface to unmount the uSD card, and sure enough, it showed up in the Linux filesystem. It appeared to require a power-cycle (or at least reboot) of the receiver to get the mosaic-X5 to mount the card again.
Having the uSD card appear as mass storage to a computer could be convenient and would avoid the wear and tear of physically removing and insert the card (e.g. to put it in a computer’s card reader), but having to physically move the card is not much of a problem.
I assume that your suggested “Write profile…” and “Read profile…” options are meant to be menu items in the receiver’s configuration menu. I do like the idea of the user having to explicitly initiate writing and especially reading of the settings/profiles file on the uSD card, to reduce the risk of accidental overwriting of settings or profiles.
Overall, the most appealing experience to me would be to be able to write the settings/profiles to the uSD card by using an ESP32 config menu item, and to be able to read or load the settings/profiles by using another ESP32 config menu item. But I’m not the one writing the code.