Hi need some help I am trying to get PWM working using fast PWM on the ATMEGA128. I have had so many problems!! I have got to the point where I can generate a 1ms pulse but it will only pulse once. It appears to reset the timer at the TOP ICRn and the pulse is the same as what is in the OCR1A register however when the counter resets the pin does not go high again. Any ideas???
# include <avr/io.h>
#include <avr/interrupt.h>
void init_servo(void)
{
/* Reset Control Register*/
TCCR1B = 0x00;
/* Set Output Register*/
DDRB=0xFF;
/*Reset Counter*/
TCNT1H = 0;
TCNT1L = 0;
/*Set TOP to 40000 for 20ms period*/
ICR1H = 40000U >> 8;
ICR1L = 40000U & 0xff;
/*
Enable 2 PWM ports */
TCCR1A = 0x52;
/* Prescaler of 8
ICR1 = overflow value
Fast PWM,mode 14(WGM13 & WGM12 HIGH) */
TCCR1B = 0x1A;//start timer
}
void set_servo_A(unsigned value)
{
OCR1AH = value >> 8;
OCR1AL = value & 0xff;
}
void main(void)
{
init_servo();
set_servo_A(2000); //-90 degrees
for(;;)
{
}
}
Are you setting the COM bits correctly? It looks like for WGM=14, then COMnn=(0,1) doesn’t do anything useful. Probably you want COMnn=(1,0) or (1,1) — try setting TCCR1A to 0xA2 or 0xF2?
Since the previous post I had changed the value of TCCR1A to 0xa2. From my understanding this should give me a high pulse for 1ms(as I have set it) and low for the remainder, loop at the top and go high when it reaches the bottom.
It does not go high when first started , I can set the port to high and it will go low when it reaches the compare value (OCRn) but when it loops at TOP it stays low. Ive tried so many combinations to get this to work, im at a loss!
I tested this using AVR studio. The only thing I can think of is that it is an error with the simulator.
I noticed that with the ATMEGA128 the adressing bits were the same as other I/O ports. When I contacted atmel seems they had a error with the file for that chip. Anyway they released the temp fix and I installed that but still no change.
It just seems odd to me that it would do one pulse but never any more… This is proving quite challlenging for me… I only started programming three weeks ago and I have run into so many problems!