Hello,
I’m new to both Sparkfun and Arduino, be gentle with me ![]()
So I’m trying to set up the Soil Moisture sensor with Sparkfun ESP32-C3 Micro Pro board, following this guide:
As the title says, I run into this error and simply can’t figure the cause.
Well, I’m missing a library, obviously.
I’ve read somewhere else that it might be avr-libc, but that doesn’t seem to be in the Library Manager (Arduino IDE 2.3.6).
The sketch I’m trying to compile is here:
/******************************************************************************
Zio Qwiic Soil Moisture Sensor Example 1 - Basic Reading
Harry
September 25, 2018
Default address is 0x28.
******************************************************************************/
#include "SparkFun_Soil_Moisture_Sensor.h"
#define COMMAND_LED_OFF 0x00
#define COMMAND_LED_ON 0x01
#define COMMAND_GET_VALUE 0x05
#define COMMAND_NOTHING_NEW 0x99
const byte qwiicAddress = 0x28; //Default Address
uint16_t ADC_VALUE=0;
void setup() {
Serial.begin(9600);
Serial.println("Zio Qwiic Soil Moisture Sensor Master Awake");
Wire.begin();
testForConnectivity();
ledOn();
delay(1000);
}
void loop() {
get_value();
ledOn();
delay(1000);
ledOff();
delay(1000);
}
// LED is off, and a -1 if an error occurred.
void get_value() {
Wire.beginTransmission(qwiicAddress);
Wire.write(COMMAND_GET_VALUE); // command for status
Wire.endTransmission(); // stop transmitting //this looks like it was essential.
Wire.requestFrom(qwiicAddress, 2); // request 1 bytes from slave device qwiicAddress
while (Wire.available()) { // slave may send less than requested
uint8_t ADC_VALUE_L = Wire.read();
// Serial.print("ADC_VALUE_L: ");
// Serial.println(ADC_VALUE_L,DEC);
uint8_t ADC_VALUE_H = Wire.read();
// Serial.print("ADC_VALUE_H: ");
// Serial.println(ADC_VALUE_H,DEC);
ADC_VALUE=ADC_VALUE_H;
ADC_VALUE<<=8;
ADC_VALUE|=ADC_VALUE_L;
Serial.print("ADC_VALUE: ");
Serial.println(ADC_VALUE,DEC);
}
uint16_t x=Wire.read();
}
void ledOn() {
Wire.beginTransmission(qwiicAddress);
Wire.write(COMMAND_LED_ON);
Wire.endTransmission();
}
void ledOff() {
Wire.beginTransmission(qwiicAddress);
Wire.write(COMMAND_LED_OFF);
Wire.endTransmission();
}
// testForConnectivity() checks for an ACK from an Sensor. If no ACK
// program freezes and notifies user.
void testForConnectivity() {
Wire.beginTransmission(qwiicAddress);
//check here for an ACK from the slave, if no ACK don't allow change?
if (Wire.endTransmission() != 0) {
Serial.println("Check connections. No slave attached.");
while (1);
}
}
The only thing I can really think of, is that I’m running this Sketch from my downloads folder. I tried moving it to some proper Arduino folder, but the install isn’t where the documentation says it should be - and where it actually is installed, it doesn’t have the suggested folder structure :-/
I’m on a mac, btw.
Any and all suggestions would be very welcome. Thanks ![]()