In my project RX like WRL-10532 (RF Link Receiver - 4800bps (434MHz)) will be mounted on the edge rotating disc with RPM around 8000, and TX will be stationary nearby. So my question is will these modules work at this RPM or there will be a problem of Doppler shift,
I want to make sure before purchasing that i have right hardware, If these modules can’t work then please suggest me the other options.
Now the Doppler shift is a ratio of the tangential speed to that of the speed of light. If the shift is more than the Rx can handle you will have problems.
You also need to worry about accelerations tearing the board apart!