I have blown up many FemtoBuck and also some PicoBuck and can’t figure out where the problem is…
There are 7 Osram Oslon HyperRed LED on a Metal PCB Module, and two are in series connected to one Femtobuck. My multimeter is total crap, the current messureing is gone, so I soldered a 10 Ohm Resistor between the two modules to measure the current over the the voltage of this resistor.
Every time I turn on the Power Supply (Meanwell UHP-500) at 36V the PicoBuck goes up in smoke… and with lower Voltage 33V to 35V the current through the Modules changes, sometimes it is 200mA, than 600mA, than 400mA.
Looks like the PicoBuck do not regulate the current, it also gets very hot.
I have soldered the FemtoBuck with a primitive 230V soldering iron, this could be one source of error.
-
Does the soldering took to long and the BUCK may got some heat damage?
-
Or may it be a ESD damage that happend from this soldering iron?
-
Or maybe the UHP-500 is not worth what Meanwell is telling and I have a high ripple Voltage?
From seeing, that the Current is not regulated by the FemtoBuck I speculate that it possible Nr. 1 or Nr. 2 therefore I ordered a new Soldering station (ERSA i-CON NANO) with ESD protection that arrived this morning. Furthermore I will buy some 9V Block batteries connect them in series to cancel out the a ripple voltage from the Power Supply.
Does anyone have another Idea what could be the problem?
Thanks ![]()