Works really well. One question, even when a relay is off, it leaks a small amount of current. From what I understand this is normal. It does however cause the LEDs in the (240v) device I’m controlling to flicker even when the relay is off. Is there a good way to filter out this interference?
I am afraid the bleeder will not help guys. That is to discharge a capacitor faster in case there is voltage left after power-off.
A TRIAC (as used in solid relays) will always produce a leak current. The datasheet is showing 4 to 6 mA depending on the solid-state relay used and that has that could be enough to trigger LED’s. The only way to reduce (BUT not eliminate) is the design. e.g. Look at https://components101.com/triacs/leakag … inimize-it . Maybe in this case it is better to have a mechanical relay.