Hi ![]()
I need to use a library but it does not work in Arduino Due, as it uses SoftwareSerial and Arduino Due has more than 1 serial port to use. I tried to adapt the library but it did not work, I will make the library code available and if someone can help me find the error or help me fix the problem I thank you very much because I really need this library.
FPS_GT511C3_h
#ifndef FPS_GT511C3_h
#define FPS_GT511C3_h
#include "Arduino.h"
#include "SoftwareSerial.h"
#ifndef __GNUC__
#pragma region -= Command_Packet =-
#endif //__GNUC__
/*
Command_Packet represents the 12 byte command that we send to the finger print scanner
*/
class Command_Packet
{
public:
class Commands
{
public:
enum Commands_Enum
{
NotSet = 0x00, // Default value for enum. Scanner will return error if sent this.
Open = 0x01, // Open Initialization
Close = 0x02, // Close Termination
UsbInternalCheck = 0x03, // UsbInternalCheck Check if the connected USB device is valid
ChangeEBaudRate = 0x04, // ChangeBaudrate Change UART baud rate
SetIAPMode = 0x05, // SetIAPMode Enter IAP Mode In this mode, FW Upgrade is available
CmosLed = 0x12, // CmosLed Control CMOS LED
GetEnrollCount = 0x20, // Get enrolled fingerprint count
CheckEnrolled = 0x21, // Check whether the specified ID is already enrolled
EnrollStart = 0x22, // Start an enrollment
Enroll1 = 0x23, // Make 1st template for an enrollment
Enroll2 = 0x24, // Make 2nd template for an enrollment
Enroll3 = 0x25, // Make 3rd template for an enrollment, merge three templates into one template, save merged template to the database
IsPressFinger = 0x26, // Check if a finger is placed on the sensor
DeleteID = 0x40, // Delete the fingerprint with the specified ID
DeleteAll = 0x41, // Delete all fingerprints from the database
Verify1_1 = 0x50, // Verification of the capture fingerprint image with the specified ID
Identify1_N = 0x51, // Identification of the capture fingerprint image with the database
VerifyTemplate1_1 = 0x52, // Verification of a fingerprint template with the specified ID
IdentifyTemplate1_N = 0x53, // Identification of a fingerprint template with the database
CaptureFinger = 0x60, // Capture a fingerprint image(256x256) from the sensor
MakeTemplate = 0x61, // Make template for transmission
GetImage = 0x62, // Download the captured fingerprint image(256x256)
GetRawImage = 0x63, // Capture & Download raw fingerprint image(320x240)
GetTemplate = 0x70, // Download the template of the specified ID
SetTemplate = 0x71, // Upload the template of the specified ID
GetDatabaseStart = 0x72, // Start database download, obsolete
GetDatabaseEnd = 0x73, // End database download, obsolete
UpgradeFirmware = 0x80, // Not supported
UpgradeISOCDImage = 0x81, // Not supported
Ack = 0x30, // Acknowledge.
Nack = 0x31 // Non-acknowledge
};
};
Commands::Commands_Enum Command;
byte Parameter[4]; // Parameter 4 bytes, changes meaning depending on command
byte* GetPacketBytes(); // returns the bytes to be transmitted
void ParameterFromInt(int i);
Command_Packet();
private:
static const byte COMMAND_START_CODE_1 = 0x55; // Static byte to mark the beginning of a command packet - never changes
static const byte COMMAND_START_CODE_2 = 0xAA; // Static byte to mark the beginning of a command packet - never changes
static const byte COMMAND_DEVICE_ID_1 = 0x01; // Device ID Byte 1 (lesser byte) - theoretically never changes
static const byte COMMAND_DEVICE_ID_2 = 0x00; // Device ID Byte 2 (greater byte) - theoretically never changes
byte command[2]; // Command 2 bytes
word _CalculateChecksum(); // Checksum is calculated using byte addition
byte GetHighByte(word w);
byte GetLowByte(word w);
};
#ifndef __GNUC__
#pragma endregion
#endif //__GNUC__
#ifndef __GNUC__
#pragma region -= Response_Packet =-
#endif //__GNUC__
/*
Response_Packet represents the returned data from the finger print scanner
*/
class Response_Packet
{
public:
class ErrorCodes
{
public:
enum Errors_Enum
{
NO_ERROR = 0x0000, // Default value. no error
NACK_TIMEOUT = 0x1001, // Obsolete, capture timeout
NACK_INVALID_BAUDRATE = 0x1002, // Obsolete, Invalid serial baud rate
NACK_INVALID_POS = 0x1003, // The specified ID is not between 0~199
NACK_IS_NOT_USED = 0x1004, // The specified ID is not used
NACK_IS_ALREADY_USED = 0x1005, // The specified ID is already used
NACK_COMM_ERR = 0x1006, // Communication Error
NACK_VERIFY_FAILED = 0x1007, // 1:1 Verification Failure
NACK_IDENTIFY_FAILED = 0x1008, // 1:N Identification Failure
NACK_DB_IS_FULL = 0x1009, // The database is full
NACK_DB_IS_EMPTY = 0x100A, // The database is empty
NACK_TURN_ERR = 0x100B, // Obsolete, Invalid order of the enrollment (The order was not as: EnrollStart -> Enroll1 -> Enroll2 -> Enroll3)
NACK_BAD_FINGER = 0x100C, // Too bad fingerprint
NACK_ENROLL_FAILED = 0x100D, // Enrollment Failure
NACK_IS_NOT_SUPPORTED = 0x100E, // The specified command is not supported
NACK_DEV_ERR = 0x100F, // Device Error, especially if Crypto-Chip is trouble
NACK_CAPTURE_CANCELED = 0x1010, // Obsolete, The capturing is canceled
NACK_INVALID_PARAM = 0x1011, // Invalid parameter
NACK_FINGER_IS_NOT_PRESSED = 0x1012, // Finger is not pressed
INVALID = 0XFFFF // Used when parsing fails
};
static Errors_Enum ParseFromBytes(byte high, byte low);
};
Response_Packet(byte* buffer, bool UseSerialDebug);
ErrorCodes::Errors_Enum Error;
byte RawBytes[12];
byte ParameterBytes[4];
byte ResponseBytes[2];
bool ACK;
static const byte COMMAND_START_CODE_1 = 0x55; // Static byte to mark the beginning of a command packet - never changes
static const byte COMMAND_START_CODE_2 = 0xAA; // Static byte to mark the beginning of a command packet - never changes
static const byte COMMAND_DEVICE_ID_1 = 0x01; // Device ID Byte 1 (lesser byte) - theoretically never changes
static const byte COMMAND_DEVICE_ID_2 = 0x00; // Device ID Byte 2 (greater byte) - theoretically never changes
int IntFromParameter();
private:
bool CheckParsing(byte b, byte propervalue, byte alternatevalue, const char* varname, bool UseSerialDebug);
word CalculateChecksum(byte* buffer, int length);
byte GetHighByte(word w);
byte GetLowByte(word w);
};
#ifndef __GNUC__
#pragma endregion
#endif //__GNUC__
#ifndef __GNUC__
#pragma region -= Data_Packet =-
#endif //__GNUC__
// Data Mule packet for receiving large data(in 128 byte pieces) from the FPS
// This class can only transmit one packet at a time
//class Data_Packet
//{
//public:
// static int CheckSum;
// int PacketID;
// int ValidByteLength;
// byte Data[128];
// void StartNewPacket();
// bool IsLastPacket;
//private:
// static int NextPacketID;
//};
#ifndef __GNUC__
#pragma endregion
#endif //__GNUC__
/*
Object for controlling the GT-511C3 Finger Print Scanner (FPS)
*/
class FPS_GT511C3
{
public:
// Enables verbose debug output using hardware Serial
bool UseSerialDebug;
#ifndef __GNUC__
#pragma region -= Constructor/Destructor =-
#endif //__GNUC__
// Creates a new object to interface with the fingerprint scanner
FPS_GT511C3(uint8_t rx, uint8_t tx);
// destructor
~FPS_GT511C3();
#ifndef __GNUC__
#pragma endregion
#endif //__GNUC__
#ifndef __GNUC__
#pragma region -= Device Commands =-
#endif //__GNUC__
//Initialises the device and gets ready for commands
void Open();
// Does not actually do anything (according to the datasheet)
// I implemented open, so had to do closed too... lol
void Close();
// Turns on or off the LED backlight
// LED must be on to see fingerprints
// Parameter: true turns on the backlight, false turns it off
// Returns: True if successful, false if not
bool SetLED(bool on);
// Changes the baud rate of the connection
// Parameter: 9600 - 115200
// Returns: True if success, false if invalid baud
// NOTE: Untested (don't have a logic level changer and a voltage divider is too slow)
bool ChangeBaudRate(unsigned long baud);
// Gets the number of enrolled fingerprints
// Return: The total number of enrolled fingerprints
int GetEnrollCount();
// checks to see if the ID number is in use or not
// Parameter: 0-2999, if using GT-521F52
// 0-199, if using GT-521F32/GT-511C3
// Return: True if the ID number is enrolled, false if not
bool CheckEnrolled(int id);
// Starts the Enrollment Process
// Parameter: 0-2999, if using GT-521F52
// 0-199, if using GT-521F32/GT-511C3
// Return:
// 0 - ACK
// 1 - Database is full
// 2 - Invalid Position
// 3 - Position(ID) is already used
int EnrollStart(int id);
// Gets the first scan of an enrollment
// Return:
// 0 - ACK
// 1 - Enroll Failed
// 2 - Bad finger
// 3 - ID in use
int Enroll1();
// Gets the Second scan of an enrollment
// Return:
// 0 - ACK
// 1 - Enroll Failed
// 2 - Bad finger
// 3 - ID in use
int Enroll2();
// Gets the Third scan of an enrollment
// Finishes Enrollment
// Return:
// 0 - ACK
// 1 - Enroll Failed
// 2 - Bad finger
// 3 - ID in use
int Enroll3();
// Checks to see if a finger is pressed on the FPS
// Return: true if finger pressed, false if not
bool IsPressFinger();
// Deletes the specified ID (enrollment) from the database
// Returns: true if successful, false if position invalid
bool DeleteID(int ID);
// Deletes all IDs (enrollments) from the database
// Returns: true if successful, false if db is empty
bool DeleteAll();
// Checks the currently pressed finger against a specific ID
// Parameter: 0-2999, if using GT-521F52 (id number to be checked)
// 0-199, if using GT-521F32/GT-511C3 (id number to be checked)
// Returns:
// 0 - Verified OK (the correct finger)
// 1 - Invalid Position
// 2 - ID is not in use
// 3 - Verified FALSE (not the correct finger)
int Verify1_1(int id);
// Checks the currently pressed finger against all enrolled fingerprints
// Returns:
// Verified against the specified ID (found, and here is the ID number)
// 0-2999, if using GT-521F52
// 0-199, if using GT-521F32/GT-511C3
// Failed to find the fingerprint in the database
// 3000, if using GT-521F52
// 200, if using GT-521F32/GT-511C3
int Identify1_N();
// Captures the currently pressed finger into onboard ram
// Parameter: true for high quality image(slower), false for low quality image (faster)
// Generally, use high quality for enrollment, and low quality for verification/identification
// Returns: True if ok, false if no finger pressed
bool CaptureFinger(bool highquality);
#ifndef __GNUC__
#pragma endregion
#endif //__GNUC__
#ifndef __GNUC__
#pragma region -= Not implemented commands =-
#endif //__GNUC__
// Gets an image that is 258x202 (52116 bytes) and returns it in 407 Data_Packets
// Use StartDataDownload, and then GetNextDataPacket until done
// Returns: True (device confirming download starting)
// Not implemented due to memory restrictions on the arduino
// may revisit this if I find a need for it
//bool GetImage();
// Gets an image that is qvga 160x120 (19200 bytes) and returns it in 150 Data_Packets
// Use StartDataDownload, and then GetNextDataPacket until done
// Returns: True (device confirming download starting)
// Not implemented due to memory restrictions on the arduino
// may revisit this if I find a need for it
//bool GetRawImage();
// Gets a template from the fps (498 bytes) in 4 Data_Packets
// Use StartDataDownload, and then GetNextDataPacket until done
// Parameter: 0-199 ID number
// Returns:
// 0 - ACK Download starting
// 1 - Invalid position
// 2 - ID not used (no template to download
// Not implemented due to memory restrictions on the arduino
// may revisit this if I find a need for it
//int GetTemplate(int id);
// Uploads a template to the fps
// Parameter: the template (498 bytes)
// Parameter: the ID number to upload
// Parameter: Check for duplicate fingerprints already on fps
// Returns:
// 0-199 - ID duplicated
// 200 - Uploaded ok (no duplicate if enabled)
// 201 - Invalid position
// 202 - Communications error
// 203 - Device error
// Not implemented due to memory restrictions on the arduino
// may revisit this if I find a need for it
//int SetTemplate(byte* tmplt, int id, bool duplicateCheck);
// Commands that are not implemented (and why)
// VerifyTemplate1_1 - Couldn't find a good reason to implement this on an arduino
// IdentifyTemplate1_N - Couldn't find a good reason to implement this on an arduino
// MakeTemplate - Couldn't find a good reason to implement this on an arduino
// UsbInternalCheck - not implemented - Not valid config for arduino
// GetDatabaseStart - historical command, no longer supported
// GetDatabaseEnd - historical command, no longer supported
// UpgradeFirmware - Data Sheet says not supported
// UpgradeISOCDImage - Data Sheet says not supported
// SetIAPMode - for upgrading firmware (which is not supported)
// Ack and Nack are listed as a commands for some unknown reason... not implemented
#ifndef __GNUC__
#pragma endregion
#endif //__GNUC__
#ifndef __GNUC__
#pragma endregion
#endif //__GNUC__
void serialPrintHex(byte data);
void SendToSerial(byte data[], int length);
// resets the Data_Packet class, and gets ready to download
// Not implemented due to memory restrictions on the arduino
// may revisit this if I find a need for it
//void StartDataDownload();
// Returns the next data packet
// Not implemented due to memory restrictions on the arduino
// may revisit this if I find a need for it
//Data_Packet GetNextDataPacket();
private:
void SendCommand(byte cmd[], int length);
Response_Packet* GetResponse();
uint8_t pin_RX,pin_TX;
SoftwareSerial _serial;
};
#endif
FPS_GT511C3.cpp
#include "FPS_GT511C3.h"
#ifndef __GNUC__
#pragma region -= Command_Packet Definitions =-
#endif //__GNUC__
// returns the 12 bytes of the generated command packet
// remember to call delete on the returned array
byte* Command_Packet::GetPacketBytes()
{
byte* packetbytes= new byte[12];
// update command before calculating checksum (important!)
word cmd = Command;
command[0] = GetLowByte(cmd);
command[1] = GetHighByte(cmd);
word checksum = _CalculateChecksum();
packetbytes[0] = COMMAND_START_CODE_1;
packetbytes[1] = COMMAND_START_CODE_2;
packetbytes[2] = COMMAND_DEVICE_ID_1;
packetbytes[3] = COMMAND_DEVICE_ID_2;
packetbytes[4] = Parameter[0];
packetbytes[5] = Parameter[1];
packetbytes[6] = Parameter[2];
packetbytes[7] = Parameter[3];
packetbytes[8] = command[0];
packetbytes[9] = command[1];
packetbytes[10] = GetLowByte(checksum);
packetbytes[11] = GetHighByte(checksum);
return packetbytes;
}
// Converts the int to bytes and puts them into the paramter array
void Command_Packet::ParameterFromInt(int i)
{
Parameter[0] = (i & 0x000000ff);
Parameter[1] = (i & 0x0000ff00) >> 8;
Parameter[2] = (i & 0x00ff0000) >> 16;
Parameter[3] = (i & 0xff000000) >> 24;
}
// Returns the high byte from a word
byte Command_Packet::GetHighByte(word w)
{
return (byte)(w>>8)&0x00FF;
}
// Returns the low byte from a word
byte Command_Packet::GetLowByte(word w)
{
return (byte)w&0x00FF;
}
word Command_Packet::_CalculateChecksum()
{
word w = 0;
w += COMMAND_START_CODE_1;
w += COMMAND_START_CODE_2;
w += COMMAND_DEVICE_ID_1;
w += COMMAND_DEVICE_ID_2;
w += Parameter[0];
w += Parameter[1];
w += Parameter[2];
w += Parameter[3];
w += command[0];
w += command[1];
return w;
}
Command_Packet::Command_Packet()
{
};
#ifndef __GNUC__
#pragma endregion
#endif //__GNUC__
#ifndef __GNUC__
#pragma region -= Response_Packet Definitions =-
#endif //__GNUC__
// creates and parses a response packet from the finger print scanner
Response_Packet::Response_Packet(byte* buffer, bool UseSerialDebug)
{
CheckParsing(buffer[0], COMMAND_START_CODE_1, COMMAND_START_CODE_1, "COMMAND_START_CODE_1", UseSerialDebug);
CheckParsing(buffer[1], COMMAND_START_CODE_2, COMMAND_START_CODE_2, "COMMAND_START_CODE_2", UseSerialDebug);
CheckParsing(buffer[2], COMMAND_DEVICE_ID_1, COMMAND_DEVICE_ID_1, "COMMAND_DEVICE_ID_1", UseSerialDebug);
CheckParsing(buffer[3], COMMAND_DEVICE_ID_2, COMMAND_DEVICE_ID_2, "COMMAND_DEVICE_ID_2", UseSerialDebug);
CheckParsing(buffer[8], 0x30, 0x31, "AckNak_LOW", UseSerialDebug);
if (buffer[8] == 0x30) ACK = true; else ACK = false;
CheckParsing(buffer[9], 0x00, 0x00, "AckNak_HIGH", UseSerialDebug);
word checksum = CalculateChecksum(buffer, 10);
byte checksum_low = GetLowByte(checksum);
byte checksum_high = GetHighByte(checksum);
CheckParsing(buffer[10], checksum_low, checksum_low, "Checksum_LOW", UseSerialDebug);
CheckParsing(buffer[11], checksum_high, checksum_high, "Checksum_HIGH", UseSerialDebug);
Error = ErrorCodes::ParseFromBytes(buffer[5], buffer[4]);
ParameterBytes[0] = buffer[4];
ParameterBytes[1] = buffer[5];
ParameterBytes[2] = buffer[6];
ParameterBytes[3] = buffer[7];
ResponseBytes[0]=buffer[8];
ResponseBytes[1]=buffer[9];
for (int i=0; i < 12; i++)
{
RawBytes[i]=buffer[i];
}
}
// parses bytes into one of the possible errors from the finger print scanner
Response_Packet::ErrorCodes::Errors_Enum Response_Packet::ErrorCodes::ParseFromBytes(byte high, byte low)
{
Errors_Enum e = INVALID;
if (high == 0x00)
{
}
// grw 01/03/15 - replaced if clause with else clause for any non-zero high byte
// if (high == 0x01)
// {
else {
switch(low)
{
case 0x00: e = NO_ERROR; break;
case 0x01: e = NACK_TIMEOUT; break;
case 0x02: e = NACK_INVALID_BAUDRATE; break;
case 0x03: e = NACK_INVALID_POS; break;
case 0x04: e = NACK_IS_NOT_USED; break;
case 0x05: e = NACK_IS_ALREADY_USED; break;
case 0x06: e = NACK_COMM_ERR; break;
case 0x07: e = NACK_VERIFY_FAILED; break;
case 0x08: e = NACK_IDENTIFY_FAILED; break;
case 0x09: e = NACK_DB_IS_FULL; break;
case 0x0A: e = NACK_DB_IS_EMPTY; break;
case 0x0B: e = NACK_TURN_ERR; break;
case 0x0C: e = NACK_BAD_FINGER; break;
case 0x0D: e = NACK_ENROLL_FAILED; break;
case 0x0E: e = NACK_IS_NOT_SUPPORTED; break;
case 0x0F: e = NACK_DEV_ERR; break;
case 0x10: e = NACK_CAPTURE_CANCELED; break;
case 0x11: e = NACK_INVALID_PARAM; break;
case 0x12: e = NACK_FINGER_IS_NOT_PRESSED; break;
}
}
return e;
}
// Gets an int from the parameter bytes
int Response_Packet::IntFromParameter()
{
int retval = 0;
retval = (retval << 8) + ParameterBytes[3];
retval = (retval << 8) + ParameterBytes[2];
retval = (retval << 8) + ParameterBytes[1];
retval = (retval << 8) + ParameterBytes[0];
return retval;
}
// calculates the checksum from the bytes in the packet
word Response_Packet::CalculateChecksum(byte* buffer, int length)
{
word checksum = 0;
for (int i=0; i<length; i++)
{
checksum +=buffer[i];
}
return checksum;
}
// Returns the high byte from a word
byte Response_Packet::GetHighByte(word w)
{
return (byte)(w>>8)&0x00FF;
}
// Returns the low byte from a word
byte Response_Packet::GetLowByte(word w)
{
return (byte)w&0x00FF;
}
// checks to see if the byte is the proper value, and logs it to the serial channel if not
bool Response_Packet::CheckParsing(byte b, byte propervalue, byte alternatevalue, const char* varname, bool UseSerialDebug)
{
bool retval = (b != propervalue) && (b != alternatevalue);
if ((UseSerialDebug) && (retval))
{
Serial.print("Response_Packet parsing error ");
Serial.print(varname);
Serial.print(" ");
Serial.print(propervalue, HEX);
Serial.print(" || ");
Serial.print(alternatevalue, HEX);
Serial.print(" != ");
Serial.println(b, HEX);
}
return retval;
}
#ifndef __GNUC__
#pragma endregion
#endif //__GNUC__
#ifndef __GNUC__
#pragma region -= Data_Packet =-
#endif //__GNUC__
//void Data_Packet::StartNewPacket()
//{
// Data_Packet::NextPacketID = 0;
// Data_Packet::CheckSum = 0;
//}
#ifndef __GNUC__
#pragma endregion
#endif //__GNUC__
#ifndef __GNUC__
#pragma region -= FPS_GT511C3 Definitions =-
#endif //__GNUC__
#ifndef __GNUC__
#pragma region -= Constructor/Destructor =-
#endif //__GNUC__
// Creates a new object to interface with the fingerprint scanner
FPS_GT511C3::FPS_GT511C3(uint8_t rx, uint8_t tx)
: _serial(rx,tx)
{
pin_RX = rx;
pin_TX = tx;
_serial.begin(9600);
this->UseSerialDebug = false;
};
// destructor
FPS_GT511C3::~FPS_GT511C3()
{
_serial.~SoftwareSerial();
}
#ifndef __GNUC__
#pragma endregion
#endif //__GNUC__
#ifndef __GNUC__
#pragma region -= Device Commands =-
#endif //__GNUC__
//Initialises the device and gets ready for commands
void FPS_GT511C3::Open()
{
if (UseSerialDebug) Serial.println("FPS - Open");
Command_Packet* cp = new Command_Packet();
cp->Command = Command_Packet::Commands::Open;
cp->Parameter[0] = 0x00;
cp->Parameter[1] = 0x00;
cp->Parameter[2] = 0x00;
cp->Parameter[3] = 0x00;
byte* packetbytes = cp->GetPacketBytes();
delete cp;
SendCommand(packetbytes, 12);
Response_Packet* rp = GetResponse();
delete rp;
delete packetbytes;
}
// According to the DataSheet, this does nothing...
// Implemented it for completeness.
void FPS_GT511C3::Close()
{
if (UseSerialDebug) Serial.println("FPS - Close");
Command_Packet* cp = new Command_Packet();
cp->Command = Command_Packet::Commands::Close;
cp->Parameter[0] = 0x00;
cp->Parameter[1] = 0x00;
cp->Parameter[2] = 0x00;
cp->Parameter[3] = 0x00;
byte* packetbytes = cp->GetPacketBytes();
delete cp;
SendCommand(packetbytes, 12);
Response_Packet* rp = GetResponse();
delete rp;
delete packetbytes;
};
// Turns on or off the LED backlight
// Parameter: true turns on the backlight, false turns it off
// Returns: True if successful, false if not
bool FPS_GT511C3::SetLED(bool on)
{
Command_Packet* cp = new Command_Packet();
cp->Command = Command_Packet::Commands::CmosLed;
if (on)
{
if (UseSerialDebug) Serial.println("FPS - LED on");
cp->Parameter[0] = 0x01;
}
else
{
if (UseSerialDebug) Serial.println("FPS - LED off");
cp->Parameter[0] = 0x00;
}
cp->Parameter[1] = 0x00;
cp->Parameter[2] = 0x00;
cp->Parameter[3] = 0x00;
byte* packetbytes = cp->GetPacketBytes();
delete cp;
SendCommand(packetbytes, 12);
Response_Packet* rp = GetResponse();
bool retval = true;
if (rp->ACK == false) retval = false;
delete rp;
delete packetbytes;
return retval;
};
// Changes the baud rate of the connection
// Parameter: 9600, 19200, 38400, 57600, 115200
// Returns: True if success, false if invalid baud
// NOTE: Untested (don't have a logic level changer and a voltage divider is too slow)
bool FPS_GT511C3::ChangeBaudRate(unsigned long baud)
{
if ((baud == 9600) || (baud == 19200) || (baud == 38400) || (baud == 57600) || (baud == 115200))
{
if (UseSerialDebug) Serial.println("FPS - ChangeBaudRate");
Command_Packet* cp = new Command_Packet();
cp->Command = Command_Packet::Commands::Open;
cp->ParameterFromInt(baud);
byte* packetbytes = cp->GetPacketBytes();
delete cp;
SendCommand(packetbytes, 12);
Response_Packet* rp = GetResponse();
bool retval = rp->ACK;
if (retval)
{
_serial.end();
_serial.begin(baud);
}
delete rp;
delete packetbytes;
return retval;
}
return false;
}
// Gets the number of enrolled fingerprints
// Return: The total number of enrolled fingerprints
int FPS_GT511C3::GetEnrollCount()
{
if (UseSerialDebug) Serial.println("FPS - GetEnrolledCount");
Command_Packet* cp = new Command_Packet();
cp->Command = Command_Packet::Commands::GetEnrollCount;
cp->Parameter[0] = 0x00;
cp->Parameter[1] = 0x00;
cp->Parameter[2] = 0x00;
cp->Parameter[3] = 0x00;
byte* packetbytes = cp->GetPacketBytes();
delete cp;
SendCommand(packetbytes, 12);
Response_Packet* rp = GetResponse();
int retval = rp->IntFromParameter();
delete rp;
delete packetbytes;
return retval;
}
// checks to see if the ID number is in use or not
// Parameter: 0-2999, if using GT-521F52
// 0-199, if using GT-521F32/GT-511C3
// Return: True if the ID number is enrolled, false if not
bool FPS_GT511C3::CheckEnrolled(int id)
{
if (UseSerialDebug) Serial.println("FPS - CheckEnrolled");
Command_Packet* cp = new Command_Packet();
cp->Command = Command_Packet::Commands::CheckEnrolled;
cp->ParameterFromInt(id);
byte* packetbytes = cp->GetPacketBytes();
delete cp;
SendCommand(packetbytes, 12);
delete packetbytes;
Response_Packet* rp = GetResponse();
bool retval = false;
retval = rp->ACK;
delete rp;
return retval;
}
// Starts the Enrollment Process
// Parameter: 0-2999, if using GT-521F52
// 0-199, if using GT-521F32/GT-511C3
// Return:
// 0 - ACK
// 1 - Database is full
// 2 - Invalid Position
// 3 - Position(ID) is already used
int FPS_GT511C3::EnrollStart(int id)
{
if (UseSerialDebug) Serial.println("FPS - EnrollStart");
Command_Packet* cp = new Command_Packet();
cp->Command = Command_Packet::Commands::EnrollStart;
cp->ParameterFromInt(id);
byte* packetbytes = cp->GetPacketBytes();
delete cp;
SendCommand(packetbytes, 12);
delete packetbytes;
Response_Packet* rp = GetResponse();
int retval = 0;
if (rp->ACK == false)
{
if (rp->Error == Response_Packet::ErrorCodes::NACK_DB_IS_FULL) retval = 1;
if (rp->Error == Response_Packet::ErrorCodes::NACK_INVALID_POS) retval = 2;
if (rp->Error == Response_Packet::ErrorCodes::NACK_IS_ALREADY_USED) retval = 3;
}
delete rp;
return retval;
}
// Gets the first scan of an enrollment
// Return:
// 0 - ACK
// 1 - Enroll Failed
// 2 - Bad finger
// 3 - ID in use
int FPS_GT511C3::Enroll1()
{
if (UseSerialDebug) Serial.println("FPS - Enroll1");
Command_Packet* cp = new Command_Packet();
cp->Command = Command_Packet::Commands::Enroll1;
byte* packetbytes = cp->GetPacketBytes();
delete cp;
SendCommand(packetbytes, 12);
delete packetbytes;
Response_Packet* rp = GetResponse();
int retval = rp->IntFromParameter();
//Change to "retval < 3000", if using GT-521F52
//Leave "reval < 200", if using GT-521F32/GT-511C3
if (retval < 200) retval = 3; else retval = 0;
if (rp->ACK == false)
{
if (rp->Error == Response_Packet::ErrorCodes::NACK_ENROLL_FAILED) retval = 1;
if (rp->Error == Response_Packet::ErrorCodes::NACK_BAD_FINGER) retval = 2;
}
delete rp;
if (rp->ACK) return 0; else return retval;
}
// Gets the Second scan of an enrollment
// Return:
// 0 - ACK
// 1 - Enroll Failed
// 2 - Bad finger
// 3 - ID in use
int FPS_GT511C3::Enroll2()
{
if (UseSerialDebug) Serial.println("FPS - Enroll2");
Command_Packet* cp = new Command_Packet();
cp->Command = Command_Packet::Commands::Enroll2;
byte* packetbytes = cp->GetPacketBytes();
delete cp;
SendCommand(packetbytes, 12);
delete packetbytes;
Response_Packet* rp = GetResponse();
int retval = rp->IntFromParameter();
//Change to "retval < 3000", if using GT-521F52
//Leave "reval < 200", if using GT-521F32/GT-511C3
if (retval < 200) retval = 3; else retval = 0;
if (rp->ACK == false)
{
if (rp->Error == Response_Packet::ErrorCodes::NACK_ENROLL_FAILED) retval = 1;
if (rp->Error == Response_Packet::ErrorCodes::NACK_BAD_FINGER) retval = 2;
}
delete rp;
if (rp->ACK) return 0; else return retval;
}
// Gets the Third scan of an enrollment
// Finishes Enrollment
// Return:
// 0 - ACK
// 1 - Enroll Failed
// 2 - Bad finger
// 3 - ID in use
int FPS_GT511C3::Enroll3()
{
if (UseSerialDebug) Serial.println("FPS - Enroll3");
Command_Packet* cp = new Command_Packet();
cp->Command = Command_Packet::Commands::Enroll3;
byte* packetbytes = cp->GetPacketBytes();
delete cp;
SendCommand(packetbytes, 12);
delete packetbytes;
Response_Packet* rp = GetResponse();
int retval = rp->IntFromParameter();
//Change to "retval < 3000", if using GT-521F52
//Leave "reval < 200", if using GT-521F32/GT-511C3
if (retval < 200) retval = 3; else retval = 0;
if (rp->ACK == false)
{
if (rp->Error == Response_Packet::ErrorCodes::NACK_ENROLL_FAILED) retval = 1;
if (rp->Error == Response_Packet::ErrorCodes::NACK_BAD_FINGER) retval = 2;
}
delete rp;
if (rp->ACK) return 0; else return retval;
}
// Checks to see if a finger is pressed on the FPS
// Return: true if finger pressed, false if not
bool FPS_GT511C3::IsPressFinger()
{
if (UseSerialDebug) Serial.println("FPS - IsPressFinger");
Command_Packet* cp = new Command_Packet();
cp->Command = Command_Packet::Commands::IsPressFinger;
byte* packetbytes = cp->GetPacketBytes();
delete cp;
SendCommand(packetbytes, 12);
Response_Packet* rp = GetResponse();
bool retval = false;
int pval = rp->ParameterBytes[0];
pval += rp->ParameterBytes[1];
pval += rp->ParameterBytes[2];
pval += rp->ParameterBytes[3];
if (pval == 0) retval = true;
delete rp;
delete packetbytes;
return retval;
}
// Deletes the specified ID (enrollment) from the database
// Parameter: 0-2999, if using GT-521F52 (id number to be deleted)
// 0-199, if using GT-521F32/GT-511C3(id number to be deleted)
// Returns: true if successful, false if position invalid
bool FPS_GT511C3::DeleteID(int id)
{
if (UseSerialDebug) Serial.println("FPS - DeleteID");
Command_Packet* cp = new Command_Packet();
cp->Command = Command_Packet::Commands::DeleteID;
cp->ParameterFromInt(id);
byte* packetbytes = cp->GetPacketBytes();
delete cp;
SendCommand(packetbytes, 12);
Response_Packet* rp = GetResponse();
bool retval = rp->ACK;
delete rp;
delete packetbytes;
return retval;
}
// Deletes all IDs (enrollments) from the database
// Returns: true if successful, false if db is empty
bool FPS_GT511C3::DeleteAll()
{
if (UseSerialDebug) Serial.println("FPS - DeleteAll");
Command_Packet* cp = new Command_Packet();
cp->Command = Command_Packet::Commands::DeleteAll;
byte* packetbytes = cp->GetPacketBytes();
SendCommand(packetbytes, 12);
Response_Packet* rp = GetResponse();
bool retval = rp->ACK;
delete rp;
delete packetbytes;
delete cp;
return retval;
}
// Checks the currently pressed finger against a specific ID
// Parameter: 0-2999, if using GT-521F52 (id number to be checked)
// 0-199, if using GT-521F32/GT-511C3 (id number to be checked)
// Returns:
// 0 - Verified OK (the correct finger)
// 1 - Invalid Position
// 2 - ID is not in use
// 3 - Verified FALSE (not the correct finger)
int FPS_GT511C3::Verify1_1(int id)
{
if (UseSerialDebug) Serial.println("FPS - Verify1_1");
Command_Packet* cp = new Command_Packet();
cp->Command = Command_Packet::Commands::Verify1_1;
cp->ParameterFromInt(id);
byte* packetbytes = cp->GetPacketBytes();
delete cp;
SendCommand(packetbytes, 12);
Response_Packet* rp = GetResponse();
int retval = 0;
if (rp->ACK == false)
{
retval = 3; // grw 01/03/15 - set default value of not verified before assignment
if (rp->Error == Response_Packet::ErrorCodes::NACK_INVALID_POS) retval = 1;
if (rp->Error == Response_Packet::ErrorCodes::NACK_IS_NOT_USED) retval = 2;
if (rp->Error == Response_Packet::ErrorCodes::NACK_VERIFY_FAILED) retval = 3;
}
delete rp;
delete packetbytes;
return retval;
}
// Checks the currently pressed finger against all enrolled fingerprints
// Returns:
// Verified against the specified ID (found, and here is the ID number)
// 0-2999, if using GT-521F52
// 0-199, if using GT-521F32/GT-511C3
// Failed to find the fingerprint in the database
// 3000, if using GT-521F52
// 200, if using GT-521F32/GT-511C3
int FPS_GT511C3::Identify1_N()
{
if (UseSerialDebug) Serial.println("FPS - Identify1_N");
Command_Packet* cp = new Command_Packet();
cp->Command = Command_Packet::Commands::Identify1_N;
byte* packetbytes = cp->GetPacketBytes();
delete cp;
SendCommand(packetbytes, 12);
Response_Packet* rp = GetResponse();
int retval = rp->IntFromParameter();
//Change to "retval > 3000" and "retval = 3000", if using GT-521F52
//Leave "reval > 200" and "retval = 200", if using GT-521F32/GT-511C3
if (retval > 200) retval = 200;
delete rp;
delete packetbytes;
return retval;
}
// Captures the currently pressed finger into onboard ram use this prior to other commands
// Parameter: true for high quality image(slower), false for low quality image (faster)
// Generally, use high quality for enrollment, and low quality for verification/identification
// Returns: True if ok, false if no finger pressed
bool FPS_GT511C3::CaptureFinger(bool highquality)
{
if (UseSerialDebug) Serial.println("FPS - CaptureFinger");
Command_Packet* cp = new Command_Packet();
cp->Command = Command_Packet::Commands::CaptureFinger;
if (highquality)
{
cp->ParameterFromInt(1);
}
else
{
cp->ParameterFromInt(0);
}
byte* packetbytes = cp->GetPacketBytes();
delete cp;
SendCommand(packetbytes, 12);
Response_Packet* rp = GetResponse();
bool retval = rp->ACK;
delete rp;
delete packetbytes;
return retval;
}
#ifndef __GNUC__
#pragma endregion
#endif //__GNUC__
#ifndef __GNUC__
#pragma region -= Not imlemented commands =-
#endif //__GNUC__
// Gets an image that is 258x202 (52116 bytes) and returns it in 407 Data_Packets
// Use StartDataDownload, and then GetNextDataPacket until done
// Returns: True (device confirming download starting)
// Not implemented due to memory restrictions on the arduino
// may revisit this if I find a need for it
//bool FPS_GT511C3::GetImage()
//{
// Not implemented due to memory restrictions on the arduino
// may revisit this if I find a need for it
//return false;
//}
// Gets an image that is qvga 160x120 (19200 bytes) and returns it in 150 Data_Packets
// Use StartDataDownload, and then GetNextDataPacket until done
// Returns: True (device confirming download starting)
// Not implemented due to memory restrictions on the arduino
// may revisit this if I find a need for it
//bool FPS_GT511C3::GetRawImage()
//{
// Not implemented due to memory restrictions on the arduino
// may revisit this if I find a need for it
//return false;
//}
// Gets a template from the fps (498 bytes) in 4 Data_Packets
// Use StartDataDownload, and then GetNextDataPacket until done
// Parameter: 0-199 ID number
// Returns:
// 0 - ACK Download starting
// 1 - Invalid position
// 2 - ID not used (no template to download
// Not implemented due to memory restrictions on the arduino
// may revisit this if I find a need for it
//int FPS_GT511C3::GetTemplate(int id)
//{
// Not implemented due to memory restrictions on the arduino
// may revisit this if I find a need for it
//return false;
//}
// Uploads a template to the fps
// Parameter: the template (498 bytes)
// Parameter: the ID number to upload
// Parameter: Check for duplicate fingerprints already on fps
// Returns:
// 0-199 - ID duplicated
// 200 - Uploaded ok (no duplicate if enabled)
// 201 - Invalid position
// 202 - Communications error
// 203 - Device error
// Not implemented due to memory restrictions on the arduino
// may revisit this if I find a need for it
//int FPS_GT511C3::SetTemplate(byte* tmplt, int id, bool duplicateCheck)
//{
// Not implemented due to memory restrictions on the arduino
// may revisit this if I find a need for it
//return -1;
//}
// resets the Data_Packet class, and gets ready to download
// Not implemented due to memory restrictions on the arduino
// may revisit this if I find a need for it
//void FPS_GT511C3::StartDataDownload()
//{
// Not implemented due to memory restrictions on the arduino
// may revisit this if I find a need for it
//}
// Returns the next data packet
// Not implemented due to memory restrictions on the arduino
// may revisit this if I find a need for it
//Data_Packet GetNextDataPacket()
//{
// return 0;
//}
// Commands that are not implemented (and why)
// VerifyTemplate1_1 - Couldn't find a good reason to implement this on an arduino
// IdentifyTemplate1_N - Couldn't find a good reason to implement this on an arduino
// MakeTemplate - Couldn't find a good reason to implement this on an arduino
// UsbInternalCheck - not implemented - Not valid config for arduino
// GetDatabaseStart - historical command, no longer supported
// GetDatabaseEnd - historical command, no longer supported
// UpgradeFirmware - Data sheet says not supported
// UpgradeISOCDImage - Data sheet says not supported
// SetIAPMode - for upgrading firmware (which data sheet says is not supported)
// Ack and Nack are listed as commands for some unknown reason... not implemented
#ifndef __GNUC__
#pragma endregion
#endif //__GNUC__
#ifndef __GNUC__
#pragma region -= Private Methods =-
#endif //__GNUC__
// Sends the command to the software serial channel
void FPS_GT511C3::SendCommand(byte cmd[], int length)
{
_serial.write(cmd, length);
if (UseSerialDebug)
{
Serial.print("FPS - SEND: ");
SendToSerial(cmd, length);
Serial.println();
}
};
// Gets the response to the command from the software serial channel (and waits for it)
Response_Packet* FPS_GT511C3::GetResponse()
{
byte firstbyte = 0;
bool done = false;
_serial.listen();
while (done == false)
{
firstbyte = (byte)_serial.read();
if (firstbyte == Response_Packet::COMMAND_START_CODE_1)
{
done = true;
}
}
byte* resp = new byte[12];
resp[0] = firstbyte;
for (int i=1; i < 12; i++)
{
while (_serial.available() == false) delay(10);
resp[i]= (byte) _serial.read();
}
Response_Packet* rp = new Response_Packet(resp, UseSerialDebug);
delete resp;
if (UseSerialDebug)
{
Serial.print("FPS - RECV: ");
SendToSerial(rp->RawBytes, 12);
Serial.println();
Serial.println();
}
return rp;
};
// sends the bye aray to the serial debugger in our hex format EX: "00 AF FF 10 00 13"
void FPS_GT511C3::SendToSerial(byte data[], int length)
{
boolean first=true;
Serial.print("\"");
for(int i=0; i<length; i++)
{
if (first) first=false; else Serial.print(" ");
serialPrintHex(data[i]);
}
Serial.print("\"");
}
// sends a byte to the serial debugger in the hex format we want EX "0F"
void FPS_GT511C3::serialPrintHex(byte data)
{
char tmp[16];
sprintf(tmp, "%.2X",data);
Serial.print(tmp);
}
#ifndef __GNUC__
#pragma endregion
#endif //__GNUC__
#ifndef __GNUC__
#pragma endregion
#endif //__GNUC__
Thank you all; ![]()