Fio V3 - can't load sketch on recent purchased Fio

I recently bought 2 Fi0 V3 (DEV-11520, March 11th). I have used this arduino variant in the past.

Sadly I can not load my sketch onto either of the new devices. I can, however, load the software on to a Fio V3 that I purchased in late January. They are all the same version and I can see no discernible difference. They are all red PCBs, they are labeled Fio V3, and all have 11-1-11 on the back.

When I load to the older one, I can see the TX/RX lights blink and the charge light seems to pulse; code runs. On the new ones, I see no change at all.

Is there a possibility that these new ones do not have the boot loader software?

Thanks in advance for any tips,

Chris.

Any tips on how to determine which bootloader is installed? Or if a bootloader is working properly?

Thanks,

Chris.