This is a very basic question, as I am not a techie!
I am interested in some basic information about how push-pull solenoids work. I understand that they are built as an electro-magnet, so that a small, brief electric current from a timer will trip the switch.
I was wondering first, how much power they draw when they go off? I understand that the voltage is very small.
Second, I was wondering how much fire hazard they create?
I have a timed feeder for my horse, which was built by a handyman friend with push-pull solenoids attached to timers. The solenoids run for a minute, dropping a tray of hay to the horse’s stall. A number of people have these at my barn. Here is a photo. You put hay on each drop tray, and so the horse gets fed four times over each 24 hours. You have to re-set the whole thing once a day.
http://s988.photobucket.com/user/Overom … g.html?o=1
We were having discussion at the barn as to whether these pose much of a fire hazard (huge fear for horse people) and whether the solenoids need to be enclosed to keep them free of hay. Heat or a spark could cause a fire in hay, and as you see from the design, hay can end up touching the solenoids.
I’ve been using this feeder for almost five years, and the solenoids do not get hot while they are running. Each solenoid runs for one minute in 24 hours, then the current is shut off by the timer. The only place that there is a “live” connection is the coupling that runs from the timer to the solenoid.
We were also having a discussion whether the voltage draw from the solenoids could cause a fuse to blow on the barn circuit board. Usually, no two feeders are firing at the same time. Also, if the voltage is very low, then I can’t imagine it would be more draw than a light bulb, for instance? If this is a problem, we could make sure no two timers fire at the same time.
Any fairly clear, simple on-line sources to back up your answer would also be great, to help me explain things to other barn members who don’t really understand how things work ![]()