Hello,
i’m very new to this whole thing. Yesterday i received my first SparkFun Pro Micro 5V.
I spent more or less whole day (after work) messing with Arduino IDE upload problems. Main problem was, my Pro Micro was disconnected after few seconds every time i plugged it in USB.
Today i tried uploading “empty” sketch (few times). Setup() and Loop() are empty (BareMinimum), so now it stays connected. But if i try to upload “Blinky, Hello World” sketch from learn.sparkfun.com website, then i it starts disconnecting after few seconds again. Or uploading “Blink” sketch from Arduino IDE.
I attached screenshot of Arduino IDE Tools Menu, where you can see i have selected correct Board/Processor/etc. I’m not sure about programmer. Like i said i’m new.
And here is also output from Arduino IDE after uploading “BareMinimum” sketch. A bit more info might be helpful to figure out what is going on.
I used [ code ], because it displays it a bit better (readable). Last few lines sort of don’t make any sense to me. “avrdude: Device signature” etc. and “Wrong microcontroller …”.
Any help is appreciated.
avrdude: Version 6.3-20190619
Copyright (c) 2000-2005 Brian Dean, http://www.bdmicro.com/
Copyright (c) 2007-2014 Joerg Wunsch
System wide configuration file is "/home/USER/Arduino/hardware/sparkfun/avr/avrdude.conf"
User configuration file is "/home/USER/.avrduderc"
User configuration file does not exist or is not a regular file, skipping
Using Port : /dev/ttyACM0
Using Programmer : avr109
Overriding Baud Rate : 57600
AVR Part : ATmega32U4
Chip Erase delay : 9000 us
PAGEL : PD7
BS2 : PA0
RESET disposition : dedicated
RETRY pulse : SCK
serial program mode : yes
parallel program mode : yes
Timeout : 200
StabDelay : 100
CmdexeDelay : 25
SyncLoops : 32
ByteDelay : 0
PollIndex : 3
PollValue : 0x53
Memory Detail :
Block Poll Page Polled
Memory Type Mode Delay Size Indx Paged Size Size #Pages MinW MaxW ReadBack
----------- ---- ----- ----- ---- ------ ------ ---- ------ ----- ----- ---------
eeprom 65 20 4 0 no 1024 4 0 9000 9000 0x00 0x00
flash 65 6 128 0 yes 32768 128 256 4500 4500 0x00 0x00
lfuse 0 0 0 0 no 1 0 0 9000 9000 0x00 0x00
hfuse 0 0 0 0 no 1 0 0 9000 9000 0x00 0x00
efuse 0 0 0 0 no 1 0 0 9000 9000 0x00 0x00
lock 0 0 0 0 no 1 0 0 9000 9000 0x00 0x00
calibration 0 0 0 0 no 1 0 0 0 0 0x00 0x00
signature 0 0 0 0 no 3 0 0 0 0 0x00 0x00
Programmer Type : butterfly
Description : Atmel AppNote AVR109 Boot Loader
Connecting to programmer: .
Found programmer: Id = "CATERIN"; type = S
Software Version = 1.0; No Hardware Version given.
Programmer supports auto addr increment.
Programmer supports buffered memory access with buffersize=128 bytes.
Programmer supports the following devices:
Device code: 0x44
avrdude: devcode selected: 0x44
avrdude: AVR device initialized and ready to accept instructions
Reading | ################################################## | 100% 0.29s
avrdude: Device signature = 0x0d3f0d
avrdude: Expected signature for ATmega32U4 is 1E 95 87
Double check chip, or use -F to override this check.
avrdude done. Thank you.
Wrong microcontroller found. Did you select the right board from the Tools > Board menu?