Flash debbuging crashes Insight

Hi

Time ago I started programming and debugging LPC2129. After some time I was able to debug in Insight with the code in RAM. When trying to debug

in flash an error shows up something like this:

warning: (Internal error: pc 0x10 in read in psymtab, but not in

symtab.)

For avoiding that error there are 2 ways: rebuilding gdb

viewtopic.php?t=6074

or changing from dwarf2 to stabs (I’m using WinArm). I tried this second

option (using

monitor arm7_9 force_hw_brkpts enable

inside the Insight’s console), however, when debugging at the very

begining of my code Insight crashes =(. This is WinXp 2ndSP. I’m from

Mexico so a window shows up with the next message:

La instrucción en “0x00462b19” hace referencia a la memoria en

“0x00000038”. La memoria no se puede “read”

Does anyone has had the same problem or knows how to solve it?? In the

mean time I will debug from RAM, but sooner the 16KB will not be enough.

Thanks in advanced =)

It’s me again

In fact Insight still crashes under several circumstances, eg, when I reload the same .elf that is currently running, as well as when trying to debug in flash. I haven’t found the binaries for installing a newer release in XP, does anyone can tell me where I can download the latest release for XP?? Thanks =)