Flash to Ram on the STR710 Arm eval board

Hello All

I was wondering if someone could help me with a small problem, I can flash files onto the internal and external flash and ram but what i want is to boot up from the internal flash then copy all the code from the external flash into the external memory and run it from there , so no code will be ran from the external flash it will just be a copy and on bootup it will be loading into the external ram and run from there.

Any help at all would be greatly appriated.

NoZ

I was a idiot in keil you can execute code from ram by selecting optoins on each file , I thought they were written and stored in ram but there not ONLY implemented in ram but written to wherever you want.

Hope this helps someone out

NoZ