GE863 Command Help Needed

Hi guys.

I am testing out the GE863 module now and i connected it for testing to a Basic Stamp

This is the first time i am working with this modules and i need a bit of help understanding the commands.

Now when i turn on the device all i get is the status LED flashing (as if searching for network) but i can’t seem to get anything else out of it.

Explain to me please what should the command look like if the datasheet says:

AT (Does this mean : serout pin,speed,[“AT”,13]?)

AT+IPR= (Does this mean : serout pin,speed,[“AT+IPR=9600”,13]) ?

or the command: AT+CPIN=****

shoudl it look like : serout pin,speed,[“AT+CPIN=1234”,13] ?

Please explain to me how my data should look like and in what format should i send it.