Gentoo, openocd-0.8, usb_blaster

Hi all,

I emerged the newest release of the openocd 0.8 from the main repo (~amd64) with flags (ftdi -usb).

during build I checked the configure switches, among others:

–disable-usb-blaster-2 --enable-usb_blaster_libftd

So the build should be able to work with usb blaster and not with usb blaster II → seems ok

but when i run the openocd with -f interfaces/altera-usb-blaster.cfg the program complains that there is no usb_blaster driver and lists avalible drivers amongst which there is no usb_blaster.

I checked the build log and found that the usb_blaster.c was built.

so my question, why is that ? Do usb_blaster need other configure switches turned on ?

PS.

I also emerge the openocd with usb flag turned on (so both usb and ftdi). The result was that the usb_blaster driver was found but the USB Blaster II programmer was choosed, and I need USB Blaster.

cheers.

Marek

resolved, it was a typo in the ebuild file.