i just got the gm862-gps eval kit in along with the TC5747 cam + breakout. Everything works great on the module except for the camera commands. this is what i get for all camera commands:
at#camon
+CME ERROR: operation not supported
anyone else experiencing this? am i doing something wrong?
yeah, same here… check out the GM862 product description, pg 67…
#CAMON and #CAMOFF aren’t supported on the -GPS module. I think you’re supposed to use the #CAMEN command to turn it on/off, but for me that doesn’t work.
Did you buy the GM862 w/ a full eval board (rs232 or usb)? I just got the normal breakout board (just SMT to header pins) and wired up the level converter & camera interface myself… when I try to use the #CAMEN=1 command, I just get “+CME Error: Camera Initialization Error”
hi, ya i hv disconnected the GPRS , but i stil cant turn on the CMOS camera. Actually i hv refer to the Telit website, cos my GM862 is bought from there. What i discover is all telit module , the supported camera is Agilent ADCM2650 or the Transchip TC5747. i think if i want to connect the CMOS camera to the module, hv to do a controller external circuit.