GM862-GPS - GPRS doesnt connect to google

i cant connect to www.google.com . . .

i sent following commands

AT+CGDCONT=2,“IP”,“WAP”,“0.0.0.0”,0,0

OK

at+cgqmin?

+CGQMIN: 1,0,0,0,0,0

+CGQMIN: 2,0,0,0,0,0

OK

at+cgqreq?

+CGQREQ: 1,0,0,3,0,0

+CGQREQ: 2,0,0,0,0,0

OK

at#scfg=3,2,300,90,600,200

OK

at#sgact=2,1

#SGACT: 10.35.2.89

OK

at#sd=3,0,80,“www.google.com

ERROR

what could be the reason for ERROR?

i’m using GM862 Evaluation Board - USB(sku: CEL-00281).

IS THERE ANYONE WHO CAN HELP ME?

which interface should i use?

selint0 or selint2?

i sent all above at commands by selint2. so i tryed by selint0 also.

but at#sgact, at#scfg, at#sd commands only replied “operation not supported”… what should i do?

i read that selint0 is for gprs use.

do i have to postpaid sim? now i’m prepaid user.

and i think there isnt any userid or password at this operator.

and error for sd=1,0,80,“www.google.com” is cannot resolve DN

but at#sgact=1,1 works well and can get ip address for response.

ok i got the answer for my error. it was wrong APN. even though i can gets the IP, that APN was for WAP connection.

now is the next round !! thanks