I am currently looking into a project that for work and want to know if anyone has tried this yet. We have several translator stations for our radio station around the country. Like 48 or so I think is the current number. Well we have inside each an old analog bag phone hooked up to a modem. With the old setup I can either listen to a radio we have tuned to the station and put in the box with it or I can power on the modem through out satellite link and talk to the receiver through RS-232. With the GM862 RS232 eval board from sparkfun can I use it like a remote RS-232 modem as well as change it to a different mode to allow me to read an audio input from the radio?
I would just buy one and play with it but they don’t let me play with to much stuff around here
Even if I have to use an external contact closure to change modes thats fine I have the ability to provide a contact closure through the satellite receiver. Let me know you thoughts on this
Thanks
Jonathan Bowen