Hello everyone,
I have the following hardware :
1)SparkFun Electronics - GM862 Cellular Quad Band Module with GPS
http://www.sparkfun.com/commerce/produc … ts_id=7917
with Firmware version 07.03.400
- SparkFun Electronics - GM862 Evaluation Kit - USB
http://www.sparkfun.com/commerce/produc … cts_id=280
and for future use
- SparkFun Electronics - GM862 Evaluation Board - Basic 50-Pin
http://www.sparkfun.com/commerce/produc … cts_id=277
and the following software :
RStern, Serial GSM Terminal Version 20090314.1
note: i have to use an external power supply, because
my old computer usb port, does not supply enought power.
step one:
I make a very simple script in python,
OK
step two:
i load the script to GM862GPS module, using
-GM862 Evaluation Kit - USB
-Rstern
OK
step three:
i execute the script,
Rstern push-button AT#EXECSCR
OK
target : i would like the same script
to run independently from my computer,
so…
step four:
i enable the script,
Rstern push-button AT#ESCRIPT
then …
i disconnected the module from the computer,
i powered the module, just with the external power supply
(without any usb powering), but the script did not run
Note : i tryied both low and high dtr, neither worked.
then i suspected there was not enought power, i tryed to
connected also the usp port, to get some extra power
(without using Rstern)
Note : i tryied both low and high dtr, neither worked.
here is my python code:
main.py
import myscript
myscript.pyo
import SER
import MOD
import MDM
MDM.send(‘ATD+393351234567;\r’, 0)
main script is the enabled one, not compiled,
that calls another script (a compiled one)
what is wrong?
am i missing something?
Thanks. Roberto.