GPRS module / always on IP connection?

Has anyone used the GSM GPRS module to create an always on network connection, where the module is constantly connected to the Internet without making a phone call? How easy would it be to have a PIC send and receive data over a connection like this?

I have played with the GPRS a bit. I am lost on the socket connection. What do I do to my computer to open a socket? What program can I run? Terminal maybe? Not sure. I will let you know as soon as we can get data moving back and forth to a PIC.

www.gm862.com is probably the place to ask. The US/GPRS section is very good source.

-Nathan

I get the gm862 to connect and run gprs continually until I shut it down, but the pic is having a hard time talking to it I see the serial passed from the pic into hyperterm but the gm862 does not recognize the text coming in as command information. I think I need to high and low the pins correctly. but the key is to give the at command a good amount of time before issuing another one.

does anybody tried sending data thru GPRS using PIC to the server/IP/Socket…if so help me in doing so.

sri…:
does anybody tried sending data thru GPRS using PIC to the server/IP/Socket…if so help me in doing so.

What part do you need help with? What GSM Module are you using?

hi thx for quick response

i am using PIC-GSM olimex board (SIM300DZ) module,i need to send data thru GPRS communication to the server using PIC Microcontroller,need help on AT commands order from intializing and to send and receive data.