Hi @mpicco ,
Yes, you need to include Wire1 when you begin the GNSS:
if (myGNSS.begin(Wire1) == false) //Connect to the u-blox module using Wire1 port
I just tried Example21_ModuleInfo and it is working well for me:

My setup:
Arduino IDE 1.8.19
Arduino UNO R4 Boards 1.0.5
Board: Arduino UNO R4 WiFi
SparkFun u-blox GNSS Arduino Library v2.2.27
NEO-M9N breakout connected via Qwiic
The I2C jumpers are closed on my NEO-M9N breakout
Two code changes are needed:
Wire1.begin();
and
if (myGNSS.begin(Wire1) == false) //Connect to the u-blox module using Wire1 port
I hope this helps,
Paul