Hello all,
after having hit my head a good hundred times with this one, my last hope is that some RF-knowledgeable forum member would be so kind as to cast some light over this issue…
I’ve designed a vehicle positioning device as my first RF project (you know, GPS + GSM/GPRS). I chose the so-called “chip antennas” for the design. Here is a photo of the finished thing :
http://paylet.billingpronto.com/100_4433.JPG
( excuse the big size, I did so intentionally in order we to be able to “see” the small details later)
it’s a double-layer design, being the GPS/GSM IC on the bottom layer. You can clearly see the blue chip antennas, being the one at the right for GSM (900Mhz) and the small one at the left for GPS (L1 freq, 1575Mhz).
Notice the big vias just besides the feed pad of both antennas. That’s the point where I wanted to pick up the signal from.
My GPS/GSM IC uses ultra-miniature coaxial connectors, which in turn can be mated to the appropiate ultra-miniature coaxial cables.
Here you can see those mini-coaxials ( notice the female-to-female configuration)
http://paylet.billingpronto.com/mini-coaxial.jpg
The GPS IC has a male receptacle. The idea is that you buy another male receptacle, put it on your PCB, and then mate the GPS IC’s antenna input with your antenna’s output by using the female-female coaxial. Thus you don’t have to make a microstrip on your pcb. Until now, no problem.
Now comes the time when I though that I was smarter than I really am, only for discovering that I have no idea about RF (life’s sad, yes
).
In order to cut costs (those minicoaxial are really expensive, not to mention the male receptacles), I decided to cut the female-female coaxial and make two cables from one. Then, I could solder the cut end of each cable directly to the antenna via on the pcb, and plug the female ends on the GPS IC’s male receptacles.
Thus I was saving a whole coaxial and two receptacles for each PCB. So far, so good…
pity that it won’t work. :oops:
For one, the GSM part works flawlessly. I get a consistent RSSI of 20-24 from a maximum of 31, GPRS transmission is flawlessly, and I can even reprogram my PICs on the fly sending the code via GPRS, which proves that the link quality is ok.
But the GPS part… oh man, it won’t take a single read. The NMEA data I get from the IC is the same as if I were to try with absolutely no antenna (the sirfIII gps chip has a “test nmea pattern” which is output when it has no antenna signal. You can easily recognize that pattern since the GSV sentences will show the satellite azimut and power to all ‘000’ ).
I need some advice from you guys, regarding the stupid things I will have - for sure - done here in order this not to work. Whithin my RF inexpertise, I though that removing a few milimeters of coaxial external shielding and soldering the inner conductor to my vias, wouldn’t harm the signal integrity.
Alas, and it is so for the GSM part, which works flawlessly. But the GPS won’t work . Is that due to the GPS much higher working frequency, thus being more sensible to these “experiments” ?
Am I really destroying the GPS signal by cutting&soldering the coax ?
thank you very much for your time !