hello sparkfun,
so, i’m an electronics newbie, but i’m trying put something together
for a class that i’m in. anyway, i’m using an atmega32 and probably
the dual axis gyro/accelerometer… and i need to incorporate
wireless into my device. easy implemetation, and a decent range are
priorities. it will be embedded into a large inflatable object, so it
won’t have direct line of sight… but just need to pass through the
thin vinyl. and i’m using a mac w/o built in bluetooth. would
bluetooth bluesmirf be the way to go? does your usb module work with
the built in bluetooth software in os x, or would i need a different
third party dongle? also, it would be used in a crowded performance
environment… do i have to worry about interference with bluetooth?
the zigbee modules seem like they may be more robust in that type of
environment, but also seem to be harder to implement. is that true?
any help is greatly appreciated. thanks so much.
mark