Hand soldering/using SMD/SMT parts on board.

oakgraphics:
…what is a good size for SMD/SMT parts on a pcb? I am looking for something that I can reduce the size of diodes, resistors, caps, on my pcboards at the same time something I can hand-assemble.

Greetings (No Name Supplied),

First time to SMD/SMT? Hand tools? 1206 is your best choice.

oakgraphics:
I am a hobbiest - for sure. So my budget is not great. But what would be good tools for it? (soldering gun/tips, etc.

Soldering iron with exchangeable tips. I use a MetCal.

oakgraphics:
I know the basic parts (I guess) like 0201, 0402, 0603, 0804,1206 (is that correct? Is there a sizing chart somewhere?)

It’s a moving target. The industry creates new parts. There are some modifications to existing parts to cater for different assembly and rework techniques. Trying to memorize the system is probably not a good use of your time.

If your goal is to build something that works you can use any parts you can find. If your goal is to make a limited run (two or more) consider making life a bit easier by careful design. If you’re going to do more than a couple of dozen of the same design consider farming it out to someone with production tools.

oakgraphics:
Seems like 0804 and 1206 are popular, but thier sizes seem large (expecially the 1206).

Really? What is your starting point? If you have been making prototypes or PCBs with TH (Through Hole) components then 1206 gives at least a two fold decrease in board area.

oakgraphics:
If you don’t hand solder them - what do you do?

I use solder paste and a hot air gun ($35 for a year’s worth of solder in a syringe that you store in the 'fridge, about $50 for the “hair dryer” style gun). I’ve done boards up to 100 x 150mm with around 200 components this way. There are some risks of localized heating distorting the board but with care this can be avoided.

Prior to that I use a small point soldering iron tip, and a slotted tip for removing 1206 parts. For ICs with quad pins (TQFP etc.) I used the drag soldering method with solder wick for clean up.

Comments Welcome!