I realize this is a simple problem but I do need help. When I try to compile the code below i get the me
“wire was not declared in this scope” error occurs where the line says “Wire.begin();” The “Wire.begin” shows orange on my arduino loader whereas the line below RTC shows black. What do I need to do?
the code:
#include < wire.h >
#include “RTClib.h”
RTC_DS1307 RTC;
// Pin connected to ST_CP of 74HC595
int latchPin = 8;
// Pin connected to SH_CP of 74HC595
int clockPin = 12;
// Pin connected to DS of 74HC595
int dataPin = 11;
// Holders for information you’re going to pass to shifting function
byte dataArray[10];
byte dataToSend[3];
void setup() {
// Set pins to output because they are addressed in the main loop
pinMode(latchPin, OUTPUT);
Serial.begin(9600);
Wire.begin();
RTC.begin();
// Set pins A2 and A3 so we can power the RTC breakout directly from each
pinMode(A2, OUTPUT);
digitalWrite(A2, LOW);
pinMode(A3, OUTPUT);
digitalWrite(A3, HIGH);
if (! RTC.isrunning()) {
Serial.println(“RTC is NOT running!”);
// following line sets the RTC to the date & time this sketch was compiled
RTC.adjust(DateTime(DATE, TIME));
}
// These are the bitmasks used to set the shift registers
// states 0 - 7 set one of each of the pins to be on
// state 8 turns all the pins on, and state 9 sets them all off
dataArray[0] = 0x01; //00000001
dataArray[1] = 0x02; //00000010
dataArray[2] = 0x04; //00000100
dataArray[3] = 0x08; //00001000
dataArray[4] = 0x10; //00010000
dataArray[5] = 0x20; //00100000
dataArray[6] = 0x40; //01000000
dataArray[7] = 0x80; //10000000
dataArray[8] = 0xFF; //11111111
dataArray[9] = 0x00; //00000000
// Function that blinks all the LEDs, feel free to eliminate…
// I got it directly from the Arduino ShiftOut tutorial and kept it in
blinkAll_2Bytes(2,500);
// Just runs through all the clock states each time its powered on…
// Feel free to eliminate
testAllStates();
}
void loop()
{
// Get the current hour and minute
DateTime now = RTC.now();
int hour = now.hour();
int min = now.minute();
// Print statements for debugging
/*
Serial.print(now.hour(), DEC);
Serial.print(‘:’);
Serial.print(now.minute(), DEC);
Serial.println();
*/
// We need to set the latch to 0 before each set of pin writes
digitalWrite(latchPin, 0);
// IT IS and OCLOCK are lit in all states
// Also initialize register 1 to 0’s
dataToSend[0] = dataArray[0];
dataToSend[1] = dataArray[9];
dataToSend[2] = dataArray[6];
// Add bytes needed to light other pins
if(min < 5)
{
//1:00 IT IS ONE OCLOCK
// no need to light anything else
}
else if(min < 10)
{
//1:05 IT IS FIVE MINUTES PAST ONE OCLOCK
dataToSend[0] += dataArray[6];
dataToSend[1] += dataArray[0];
}
else if(min < 15)
{
//1:10 IT IS TEN MINUTES PAST ONE OCLOCK
dataToSend[0] += dataArray[2] + dataArray[7];
dataToSend[1] += dataArray[0];
}
else if(min < 20)
{
//1:15 IT IS A QUARTER PAST ONE OCLOCK
dataToSend[0] += dataArray[1] + dataArray[4];
dataToSend[1] += dataArray[0];
}
else if(min < 25)
{
//1:20 IT IS TWENTY MINUTES PAST ONE OCLOCK
dataToSend[0] += dataArray[5] + dataArray[7];
dataToSend[1] += dataArray[0];
}
else if(min < 30)
{
//1:25 IT IS TWENTY FIVE MINUTES PAST ONE OCLOCK
dataToSend[0] += dataArray[5] + dataArray[6] + dataArray[7];
dataToSend[1] += dataArray[0];
}
else if(min < 35)
{
//1:30 IT IS HALF PAST ONE OCLOCK
dataToSend[0] += dataArray[3];
dataToSend[1] += dataArray[0];
}
else if(min < 40)
{
//1:35 IT IS TWENTY FIVE MINUTES TO TWO OCLOCK
dataToSend[0] += dataArray[5] + dataArray[6] + dataArray[7];
dataToSend[1] += dataArray[1];
}
else if(min < 45)
{
//1:40 IT IS TWENTY MINUTES TO TWO OCLOCK
dataToSend[0] += dataArray[5] + dataArray[7];
dataToSend[1] += dataArray[1];
}
else if(min < 50)
{
//1:45 IT IS A QUARTER TO TWO OCLOCK
dataToSend[0] += dataArray[1] + dataArray[4];
dataToSend[1] += dataArray[1];
}
else if(min < 55)
{
//1:50 IT IS TEN MINUTES TO TWO OCLOCK
dataToSend[0] += dataArray[2] + dataArray[7];
dataToSend[1] += dataArray[1];
}
else if(min < 60)
{
//1:55 IT IS FIVE MINUTES TO TWO OCLOCK
dataToSend[0] += dataArray[6] + dataArray[7];
dataToSend[1] += dataArray[1];
}
// Set hour register and pin
if(min < 35)
{
int reg = getHourRegister(hour);
int pin = getHourPin(hour);
dataToSend[reg] += dataArray[pin];
}
else
{
int reg = getHourRegister(hour + 1);
int pin = getHourPin(hour + 1);
dataToSend[reg] += dataArray[pin];
}
shiftOut(dataPin, clockPin, dataToSend[0]);
shiftOut(dataPin, clockPin, dataToSend[1]);
shiftOut(dataPin, clockPin, dataToSend[2]);
digitalWrite(latchPin, 1);
delay(5000);
}
// the heart of the program
void shiftOut(int myDataPin, int myClockPin, byte myDataOut) {
// This shifts 8 bits out MSB first,
//on the rising edge of the clock,
//clock idles low
//internal function setup
int i=0;
int pinState;
pinMode(myClockPin, OUTPUT);
pinMode(myDataPin, OUTPUT);
//clear everything out just in case to
//prepare shift register for bit shifting
digitalWrite(myDataPin, 0);
digitalWrite(myClockPin, 0);
//for each bit in the byte myDataOut
//NOTICE THAT WE ARE COUNTING DOWN in our for loop
//This means that %00000001 or “1” will go through such
//that it will be pin Q0 that lights.
for (i=7; i>=0; i–) {
digitalWrite(myClockPin, 0);
//if the value passed to myDataOut and a bitmask result
// true then… so if we are at i=6 and our value is
// %11010100 it would the code compares it to %01000000
// and proceeds to set pinState to 1.
if ( myDataOut & (1<<i) ) {
pinState= 1;
}
else {
pinState= 0;
}
//Sets the pin to HIGH or LOW depending on pinState
digitalWrite(myDataPin, pinState);
//register shifts bits on upstroke of clock pin
digitalWrite(myClockPin, 1);
//zero the data pin after shift to prevent bleed through
digitalWrite(myDataPin, 0);
}
//stop shifting
digitalWrite(myClockPin, 0);
}
//blinks the whole register based on the number of times you want to
//blink “n” and the pause between them “d”
//starts with a moment of darkness to make sure the first blink
//has its full visual effect.
void blinkAll_2Bytes(int n, int d)
{
digitalWrite(latchPin, 0);
shiftOut(dataPin, clockPin, 0);
shiftOut(dataPin, clockPin, 0);
digitalWrite(latchPin, 1);
delay(200);
for (int x = 0; x < n; x++)
{
digitalWrite(latchPin, 0);
shiftOut(dataPin, clockPin, 255);
shiftOut(dataPin, clockPin, 255);
digitalWrite(latchPin, 1);
delay(d);
digitalWrite(latchPin, 0);
shiftOut(dataPin, clockPin, 0);
shiftOut(dataPin, clockPin, 0);
digitalWrite(latchPin, 1);
delay(d);
}
}
// Returns the register used for the hour word
int getHourRegister(int hour)
{
if(hour > 12)
{
hour-=12;
}
if(hour <= 6)
{
return 1;
}
return 2;
}
// Returns the pin output for the hour word
int getHourPin(int hour)
{
if(hour > 12)
{
hour-=12;
}
if(hour == 1)
{
return 2;
}
else if(hour == 2)
{
return 3;
}
else if(hour == 3)
{
return 4;
}
else if(hour == 4)
{
return 5;
}
else if(hour == 5)
{
return 6;
}
else if(hour == 6)
{
return 7;
}
else if(hour == 7)
{
return 0;
}
else if(hour == 8)
{
return 1;
}
else if(hour == 9)
{
return 2;
}
else if(hour == 10)
{
return 3;
}
else if(hour == 11)
{
return 4;
}
else if(hour == 12)
{
return 5;
}
}
// Mostly cut and paste from above
int testAllStates()
{
int min = 0;
int hour = 12;
while(min < 60)
{
digitalWrite(latchPin, 0);
dataToSend[0] = dataArray[0];
dataToSend[1] = dataArray[9];
dataToSend[2] = dataArray[6];
// Add bytes needed to light other pins
if(min < 5)
{
//1:00 IT IS ONE OCLOCK
// no need to light anything else
}
else if(min < 10)
{
//1:05 IT IS FIVE MINUTES PAST ONE OCLOCK
dataToSend[0] += dataArray[6];
dataToSend[1] += dataArray[0];
}
else if(min < 15)
{
//1:10 IT IS TEN MINUTES PAST ONE OCLOCK
dataToSend[0] += dataArray[2] + dataArray[7];
dataToSend[1] += dataArray[0];
}
else if(min < 20)
{
//1:15 IT IS A QUARTER PAST ONE OCLOCK
dataToSend[0] += dataArray[1] + dataArray[4];
dataToSend[1] += dataArray[0];
}
else if(min < 25)
{
//1:20 IT IS TWENTY MINUTES PAST ONE OCLOCK
dataToSend[0] += dataArray[5] + dataArray[7];
dataToSend[1] += dataArray[0];
}
else if(min < 30)
{
//1:25 IT IS TWENTY FIVE MINUTES PAST ONE OCLOCK
dataToSend[0] += dataArray[5] + dataArray[6] + dataArray[7];
dataToSend[1] += dataArray[0];
}
else if(min < 35)
{
//1:30 IT IS HALF PAST ONE OCLOCK
dataToSend[0] += dataArray[3];
dataToSend[1] += dataArray[0];
}
else if(min < 40)
{
//1:35 IT IS TWENTY FIVE MINUTES TO TWO OCLOCK
dataToSend[0] += dataArray[5] + dataArray[6] + dataArray[7];
dataToSend[1] += dataArray[1];
}
else if(min < 45)
{
//1:40 IT IS TWENTY MINUTES TO TWO OCLOCK
dataToSend[0] += dataArray[5] + dataArray[7];
dataToSend[1] += dataArray[1];
}
else if(min < 50)
{
//1:45 IT IS A QUARTER TO TWO OCLOCK
dataToSend[0] += dataArray[1] + dataArray[4];
dataToSend[1] += dataArray[1];
}
else if(min < 55)
{
//1:50 IT IS TEN MINUTES TO TWO OCLOCK
dataToSend[0] += dataArray[2] + dataArray[7];
dataToSend[1] += dataArray[1];
}
else if(min < 60)
{
//1:55 IT IS FIVE MINUTES TO TWO OCLOCK
dataToSend[0] += dataArray[6] + dataArray[7];
dataToSend[1] += dataArray[1];
}
// Set hour register and pin
if(min < 35)
{
int reg = getHourRegister(hour);
int pin = getHourPin(hour);
dataToSend[reg] += dataArray[pin];
}
else
{
int reg = getHourRegister(hour + 1);
int pin = getHourPin(hour + 1);
dataToSend[reg] += dataArray[pin];
}
shiftOut(dataPin, clockPin, dataToSend[0]);
shiftOut(dataPin, clockPin, dataToSend[1]);
shiftOut(dataPin, clockPin, dataToSend[2]);
digitalWrite(latchPin, 1);
delay(200);
min+=1;
}
}