I wanted to interface the interrupt program which have given below into the keypad scanning program which is also given below :
For each key press i have to generate an interrupt whose function is to display a value in the grpahics lcd.
Interrupt program :
#include <NXP/iolpc2148.h>
#include <intrinsics.h>
#define XTALFREQ 12000000 //XTAL frequency in Hz
#define PCLKFREQ (XTALFREQ/4) //pclk must always be XTALFREQ/4?
int main(void);
__irq __arm void IRQ_ISR_Handler (void);
void Btn2DownISR(void);
void NonVectISR(void);
void feed (void);
int main(void)
{
/* Preliminary setup of the VIC. Assign all interrupt channels to IRQ */
VICIntSelect = 0; // Set all VIC interrupts to IRQ for now
VICIntEnClear = 0x00000000; // Diasable all interrupts
VICSoftIntClear = 0x00000000; // Clear all software interrutps
VICProtection = 0; // VIC registers can be accessed in User or
// privileged mode
VICVectAddr = 0; // Clear interrupt
VICDefVectAddr = 0; // Clear address of the default ISR
/*Configure the pins that the buttons are hooked up to to be external
interrupts */
PINSEL1_bit.P0_30=0x2; // Set Port pin P0.15 function to EINT3
//LED Conmfiguration
PINSEL2 = 0X00000000; // P1.24 TO P1.31 as GPIO
IO1DIR = 0XFF000000; // p1.24 TO P1.31 Configured as Output port.
VICProtection = 0; // Accesss VIC in USR | PROTECT
// VICDefVectAddr = (unsigned int)&NonVectISR; // Install default ISR addr
/* Set up the button 1 pressed interrupt on EINT0 */
VICIntSelect &= ~(1<<VIC_EINT3); // IRQ on external int 0.
VICVectAddr1 = (unsigned int)&Btn2DownISR; // Install ISR in VIC addr slot
VICVectCntl1 = 0x20 | VIC_EINT3; // Enable vec int for EINT 0.
VICIntEnable |= (1<<VIC_EINT3); // Enable EINT0 interrupt.
__enable_interrupt(); // Global interrupt enable
/*This is the foreground loop, which looks at data coming from the background
loop. The user can insert own code to react to timer and button driven
events */
while(1) // Foreground Loop
{
IO1SET=0XFF000000; // P1.24 TO P1.31 goes to high state
}
}
__irq __arm void irq_handler (void)
{
void (*interrupt_function)();
unsigned int vector;
vector = VICVectAddr; // Get interrupt vector.
interrupt_function = (void(*)())vector;
(*interrupt_function)(); // Call vectored interrupt function
VICVectAddr = 0; // Clear interrupt in VIC
}
__fiq __arm void fiq_handler (void)
{
while(1);
}
void Btn2DownISR(void)
{
EXTINT_bit.EINT3 = 1; // Try to reset external interrupt flag.
IO1CLR=0XFF000000; // P1.24 TO P1.31 goes to high state
}
keypadscannin program ::
#include<nxp/iolpc2148.h>
#define DESIRED_BAUDRATE 19200
#define CRYSTAL_FREQUENCY_IN_HZ 12000000
#define PCLK CRYSTAL_FREQUENCY_IN_HZ // since VPBDIV=0x01
#define DIVISOR (PCLK/(16*DESIRED_BAUDRATE))
//static void systemInit(void);
void Arm_Uart0_Init();
void ARM_INIT();
void serial_tx();
char serial_tr(char ch);
void delay_ms();
char arr=“Vi Microsystem Pvt Ltd \n”;
unsigned long int data = {0x0E000000,0x0D000000,0x0B000000,0x07000000};
void delay_ms()
{
int i,j;
for(i=0;i<=0xfff;i++)
for(j=0;j<=0xf0;j++);
}
char serial_tr(char ch)
{
if (ch==‘\n’)
{
while (!(U0LSR&0x20)); //wait until Transmit Holding Register is empty
U0THR=‘\r’; //then store to Transmit Holding Register
}
while (!(U0LSR&0x20)) {} //wait until Transmit Holding Register is empty
U0THR=ch; //then store to Transmit Holding Register
return ch;
}
void Arm_Uart0_Init() //UART Config.
{
U0LCR=0x83; // U0LCR: UART0 Line Control Register.
// 0x83: enable Divisor Latch access, set 8-bit word length.
// 1 stop bit, no parity, disable break transmission.
VPBDIV=0x01; // VPBDIV: VPB bus clock divider 0x01: PCLK = processor clock .
U0DLL=DIVISOR&0xFF; // U0DLL: UART0 Divisor Latch (LSB).
U0DLM=DIVISOR>>8; // U0DLM: UART0 Divisor Latch (MSB).
U0LCR=0x03 ; // U0LCR: UART0 Line Control Register
// 0x03: same as above, but disable Divisor Latch access.
// And same time U0THR (Transmitting register writing)holding the data.
U0FCR=0x05 ; // U0FCR: UART0 FIFO Control Register
// 0x05: Clear Tx FIFO and enable Rx and Tx FIFOs
serial_tx();
}
void serial_tx()
{
int i;
for(i=0;arr*!=‘\0’;i++)*
{
serial_tr(arr);
}
}
void ARM_INIT()
{
PINSEL0 = 0x00000005; //Pin selction for Serial Port.
PINSEL1 = 0x00000000; //Pin selection for GPIO.
IO0DIR = 0X00000005; //Pin dir. for output-1/input-input
IO0DIR = 0XF0000000;
Arm_Uart0_Init();
}
void main()
{
ARM_INIT();
while(1)
{
IO0PIN=0x00000000;
while((IO0PIN & 0x000F0000) == 0x000F0000);
IO0PIN=0x00000000;
IO0PIN=0xE0000000;
if(( IO0PIN & 0x000F0000 )!= 0x000F0000)
{
switch(IO0PIN & 0x000F0000)
{
case 0x00070000 : serial_tr(‘F’);break;
case 0x000B0000 : serial_tr(‘B’);break;
case 0x000D0000 : serial_tr(‘7’);break;
case 0x000E0000 : serial_tr(‘3’);break;
}
}
IO0PIN=0xD0000000;
if(( IO0PIN & 0x000F0000 )!= 0x000F0000)
{
switch(IO0PIN & 0x000F0000)
{
case 0x00070000 : serial_tr(‘E’);break;
case 0x000B0000 : serial_tr(‘A’);break;
case 0x000D0000 : serial_tr(‘6’);break;
case 0x000E0000 : serial_tr(‘2’);break;
}
}
IO0PIN=0xB0000000;
if(( IO0PIN & 0x000F0000 )!= 0x0F000000)
{
switch(IO0PIN & 0x000F0000)
{
case 0x00070000 : serial_tr(‘D’);break;
case 0x000B0000 : serial_tr(‘9’);break;
case 0x000D0000 : serial_tr(‘5’);break;
case 0x000E0000 : serial_tr(‘1’);break;
}
}
IO0PIN=0x70000000;
if(( IO0PIN & 0x000F0000 )!= 0x000F0000)
{
switch(IO0PIN & 0x000F0000)
{
case 0x00070000 : serial_tr(‘C’);break;
case 0x000B0000 : serial_tr(‘8’);break;
case 0x000D0000 : serial_tr(‘4’);break;
case 0x000E0000 : serial_tr(‘0’);break;
}
}
delay_ms();
}
}
Please Help …![]()