void CParallelPortDlg::UpdatePins()
{
int reg;
reg=_inp(STATUS);
if((reg & 0x40)==0) m_pin10=0; else m_pin10=1;
if((reg & 0x80)==0) m_pin11=0; else m_pin11=1;
if((reg & 0x20)==0) m_pin12=0; else m_pin12=1;
if((reg & 0x10)==0) m_pin13=0; else m_pin13=1;
if((reg & 0x08)==0) m_pin15=0; else m_pin15=1;
//////////
reg=_inp(DATA);
if((reg & 0x01)==0) m_pin2=0; else m_pin2=1;
if((reg & 0x02)==0) m_pin3=0; else m_pin3=1;
if((reg & 0x04)==0) m_pin4=0; else m_pin4=1;
if((reg & 0x08)==0) m_pin5=0; else m_pin5=1;
if((reg & 0x10)==0) m_pin6=0; else m_pin6=1;
if((reg & 0x20)==0) m_pin7=0; else m_pin7=2;
if((reg & 0x40)==0) m_pin8=0; else m_pin8=1;
if((reg & 0x80)==0) m_pin9=0; else m_pin9=1;
//////
reg = _inp(CONTROL);
if((reg & 0x01)==0) m_pin1=0; else m_pin1=1;
if((reg & 0x02)==0) m_pin14=0; else m_pin14=1;
if((reg & 0x04)==0) m_pin16=0; else m_pin16=1;
if((reg & 0x08)==0) m_pin17=0; else m_pin17=1;
UpdateData(FALSE);
}
This is code that programming LPT port but i dont understand where
(reg & 0x10)==0
(reg & 0x20)==0
(reg & 0x40)==0
(reg & 0x80)==0
i think they must be
(reg & 0x16)==0
(reg & 0x32)==0
(reg & 0x64)==0
(reg & 0x128)==0
pls help me!