To whom it may concern,
First-off, thank you for taking the time and reading this.
I am doing a school project that will keep a servo level by using an MPU6050 SparkFun Break out board. I am developing this by first experimenting through an Arduino UNO and, in the future, planing to connect it to a ProMini.
My problem is that the MPU6050 is not producing any readings when connected (directly) to the UNO.
Connections:
MPU6050 - Arduino UNO
VDD - 3.3V
GND - GND
INT - DIGITAL 2
SCL - A5
SDA - A4
I am using code and libraries from here: https://github.com/jrowberg/i2cdevlib/t … er/MPU6050
And have also received an MPU_Test code from Jeff which has previously worked for him but also failed for me.
These are the reading I get in the Serial Monitor when trying the DMP6, RAW, & MPU_TEST examples respectively:
DMP
o 0...
d flag...
.
Resetting MPU6050...?H
2
g
?H
2
g
i
êbG¤õ	êi
Checking hardware revision...
Revision @ user[16][6] = 0
Resetting m		êi
Reading OTP bank valid flag...
OTP bank is valid!
1
1
1
1929
ERROR! DMP code veri??H
RAW:
Initializing I2C devices...
Testing device connections...
MPU6050 connection failed
a/g:	0	0	0	0	0	0
a/g:	0	0	0	0	0	0
a/g:	0	0	0	0	0	0
a/g:	0	0	0	0	0	0
a/g:	0	0	0	0	0	0
a/g:	0	0	0	0	0	0
a/g:	0	0	0	0	0	0
a/g:	0	0	0	0	0	0
MPU_Test:
I2C bus connected.
Checking WHO_AM_I register contents: 0xFF
Disabling sleep mode...
-1	-1	-1	-1	-1	-1
-1	-1	-1	-1	-1	-1
-1	-1	-1	-1	-1	-1
-1	-1	-1	-1	-1	-1
-1	-1	-1	-1	-1	-1
I have spoken to SarkFun, Jeff, and got an ADXL345 to test the I2C connection on the UNO (which worked). After thinking that it was a faulty MPU, I received another one (tested at SparkFun’s location) but the problem still persists. Note: From what I know, Jeff tested the MPU on a MEGA1280 and an eval board from InvenSense.
I really appreciate your help. Thank you,
Roman