after using the hook up guide reconmended, 3 libraries installed. but still get error. so how to get the C02 reading without any errors. is there any code provided to use
i am also using this setup and faced the same problem
Oh i also have the same problem . I alr installed the libraries and do the same setup . Really need help here and provide us solutions to this or give us a code to read Co2 measurements
I can see that you are getting garbage values as output in your serial monitor. It usually happens due to a baud rate mismatch. You are selecting 9600 baud rate in the serial monitor. Check in your code if you have defined the same baud rate. Also, check if there is a problem with your connections. Check the continuity of your jumper wires. Here is another air quality monitor tutorial that you can see for some more ideas: Air Quality Monitor - Share Project - PCBWay
any other suggestion
not sure where the example is taken from but the call is not compatible. The Sparkfun library is expecting a char pointer.
bool getSerialNumber(char *serialNumber); // Returns true if serial number is read correctly
char serialNumber[13];
scd41.getSerialNumber(serialNumber);
Serial.println(serialNumber);