Hi, I just got the LPC2148 and I have encountered some problem early on:
I have the LPC2148 and I’ve been trying to compile the code and create a new SW.SFE file so that I can run it on the board. The issue is the compiler runs correctly, but doesn’t create the .SFE file. I was using the files on the Uber Boardv2_4.zip. (link:http://www.sparkfun.com/Code/Uber%20Board%20V21.zip)
On the other hand, when I compile the code from the bootloader Tutorial (link:http://www.sparkfun.com/tutorial/USB_Bo … e_Code.zip), the process occurs with no errors and the .SFE file is created with no issues. That file can then be put on an SD card and execute as directed.
Does anyone else have this issue?
Any help would be appreciated!
Thanks