Hello not sure if this is the right location for this but I am getting ready to start a project for my daughter who is Cos-playing Honey Lemon from Big Hero Six. If you are not familiar she has a purse that makes chemical mixtures. To make the purse as a co-play prop we need to have a motor turning a belt through the purse and around the shoulder strap as well as some led light flashing and a mini-fog machine. I currently have plans for making the mini-fog machine, but I need some advice on what products that I need to try and pull this together.
My idea is that she will flip a switch or push a switch and the doors will open, the LED lights will flash and cycle different colors, the fog machine will turn on and the motor will tun the fan belt in a variable sequence so that it stops and starts moving forward and backward. Total time of the sequence would be 4-6 seconds.
This is my first foray into this type of project and I’m just not sure of how all the pieces need to fit together or what pieces I need. I know that I need a motor as well as the light and a switch to start it all. As well as a way to turn the fog machine on which I think will be via the processor/board. And I will need a processor/board to control it all but after spending many hours looking at the various products I’m not sure what I need to purchase. Currently I am looking at the following.
-
Switch or push button to start the sequence looking at the Toggle switch and cover
-
Magnetic door switch set to open the doors
-
Way to start the fog machine (I think this is just via the processor/board)
-
Led light looking at the SMD LED - RGB APA102C-5050 do I need a driver for the light or is this done through the processor
-
Micro Gearmotor -130 RPM which based on the belt length with give a max of ~10 RPM for the belt. Or would the Planetary Gearmotor 140 rpm be a better option
-
Micro Gearmotor enclosure or mounting system for the planetary gearmotor
-
Power supply/driver for the motor: this is where I’m not sure what in need.
-
Timing belt about 3 feet with timing pulley’s: looking at the 15T pulley. As I understand it I will need the shaft mount pulley for the motor. Will this pulley also work for the non-motor pulley location and if so, is there a shaft system that I need?
-
Last the processor /board this is where I have no idea what I need.
Thank in advance for your help