Help with ESP 32 Connection with Sparkfun 15136 for RTK

Hi Datatron - I understand you are assembling it the same way, but if you could please take and post pictures of your assembly, it will help us figure out where the problems may be.

Plug the BlueSMiRF into your ZED-F9P. Power your system. Connect from your phone or computer to the BlueSMiRF. What output do you see? Anything?

I connect it to NTRIP (Lefebure), then connet to SWISSTOPO (RTK Server) it Downloads RTK DATA up to 100 KB, but the Accuracy stopps aprox. at 400-700 mm , and Download mor RTK dont Change something at the Accuracy at 400 - 700mm!
Unconnect BluesSMiRF, and connect Bluetooth Mate Gold, start connection to NTRIP
connect to SWISSTOPO Download RTK DATA, accuracy is 14.10mm (MAX)
Same Settings in NTRIP APP & Spakfun 15136.
Thank you very much, Michael

That’s very good feedback @Datatron !

To me, that would seem to indicate that too many constellations and/or Message types are turned ON in the F9P for the 2-way Bluetooth link to handle.

You seem to be right at the bandwidth threshold with the Bluetooth Mate Gold, but over the threshold for the BluesSMiRF. It may be something as simple as a slightly different overhead for the (2) links.

You could Configure the F9P with GPS & 1 other Constellation, and turn off unused NMEA Sentences to confirm. Then add back until the link becomes unreliable ?

There are several posts in the forum about which NMEA Sentences can be reduced or turned Off… if you want to try it.

reduce baudrate?

I Need the NMEA OUT !!

  • To be sure, set


    Do a test

  • Try using a computer with u-center via bluetooth instead of a phone. In u-center configure RTK in the menu Receiver → NTRIP Client…

  • Maybe your BlueSMiRF v2 unit is broken ?

I have 4 BlueSmiRF v2 , all with the exact same Problem. *I think not Broken.
Protocol OUT RTCM3 = no Correction!
With NMEA OUT, and Bluetooth Mate Gold or Silver the Units Accuracy is near to 5MM !!!
With Blue SMiRF v2 , no more Accuracy, only what Sparkfun 15136 can do without RTK.
It Downloads KBs of RTK -Data, but no Correction is working, stays at ca. 430mm..
I use Pay per Use, Preise und Bestellung

Thank you very much, Michael

No, I must appoligize. I was thinking about most of the other Sparkfun RTK products that include a ESP32 and run SparkFun Firmware. I’m used to configuring the F9P in the Sparkfun Firmware. I’m very sorry for any confusion.

You can keep NMEA Out, but be picky about any NMEA sentences being pushed over the Bluetooth link.
Again, I’m sorry for any confusion I might have caused.

There is no ready-made solution.

  • Have you tried another phone?

  • Can you read the set baud rate of BlueSMiRF v2?

    From your phone open the Serial Bluetooth App for android and connect to the BlueSMiRF v2.

    a) enter AT-mode by without pressing Enter type
    +++
    wait for an answer
    OK

    b) enter
    ATS
    the module will return
    115200,8,N,1

@JanW :

Again, you are posting bad, AI-generated content. Please stop.

The escape sequence for BlueSMiRF v2 is $$$ not +++. The full command set is described in the link below.

Paul

AI AI AI AI

@PaulZC

What do you think about AT-BluetoothEscapeCharacter from AT Command Reference - SparkFun BlueSMiRF v2 Hookup Guide ?

@bamarcant

LG290P AI AI AI AI

@JanW :

OK. That’s fair. I have corrected that single typo. AI does have some uses…

Regards,
Paul

AT Serial Speed 115200

That’s okay.

Have you tried:

  • another phone
    or
  • using a computer with u-center via bluetooth instead of a phone. In u-center configure RTK in the menu Receiver → NTRIP Client… ?

This would eliminate the possibility of your phone being incompatible with BlueSMiRF v2.

Have you checked ZED-F9P firmware version is up to date ?

Run u-center app

Connect the application to the module at menu Receiver->Connection->COM

Click on the menu View->Messages view

Navigate to UBX → MON → VER (Version)

Other Phone same Problem..

This indicates a problem with the BlueSMiRF v2 bluetooth module.

Read and compare the configurations of both bluetooth modules:

  1. From your phone open the Serial Bluetooth App for android and connect to the Mate Gold

    +++
    ATS
    AT+CHAN?
    AT+FLOW?
    
  2. From your phone open the Serial Bluetooth App for android and connect to the BlueSMiRF v2

    +++
    ATS
    AT+CHAN?
    AT+FLOW?
    

Firmware old..
Update Failed…


Firmware Update Done Perfect!
Checking RTK again…
I have not 1 Piece of Bluetooth Mate Gold or Silver!