Question on BlueSmirf

Hello, I am having a couple of questions for my BlueSmirf. First, I have come across a few devices that use DTR, DCE, and RLSD. Am I correct to say that the BlueSmirf is incompatible with these devices? Second, I am now trying to interface with rs-232 levels with a max3232. Will I need an inverter like a 74hc04 to invert the signals before it goes into the max3232 or is it good to go? Third, my blue smirf seems to be stuck in data mode, and it will no longer interface with hyperterminal. I am not sure why it’s stuck there. The only thing I changed was the baud rate to 57600, but I connected to it several times since I changed it. Then nothing. Is there a factory reset for this thing? The blue radios pdf said I could bring PIO4 high for 1 sec to reset to factory, but it also said not to bring any PIO high once it is an output. Since I don’t know how the module’s PIO4 is configured, I thought I’d better ask first.

Is there anyone from Sparkfun that can answer this?

Is there anyone from Sparkfun that actually reads these forums?

what did you do to reset the bluesmirf?

I have one bluesmirf that its in automaster mode and if there is not slave present, always it replies "NO ANSWER" every 40 seconds, and there its not way to put this bluesmirf in command mode sending the +++ command by serial hyperteminal COM1, I need to reconfigure this Bluesmirf and make a ATFRST to let it with factory settings.

The inicial configuration for automaster was:

atsma,00A096179A83,1101

atsw25,1,1,0,0

I have a second Bluesmirf that its worst and right now its completly unuseful, I made this configuration:

ATSW21,2560,11,2560,11

ATSW25,0,1,1,0

ATSW24,2,1,0,0

ATSW20,10,1,0,1

ATSW21,2560,11,2560,11 //Change scan intervals thus decreasing the

power consumption from 48mA to 2mA before the module is connected

ATSW25,0,1,1,0 //Prevent communication before connected

i.e. after this command, you can reconfigure BlueSmiRF only when it

Is connected, and you get out of the data mode using the escape sequence. This is important, because the randomly

received and translated IR bytes will be ignored, and will not

accidentally reconfigure the module.

ATSW24,2,1,0,0 //Turn off verbal responses. This is

important, because otherwise the BlueSmiRF will be talking to the RCX

each time you open or

close the port (CONNECT, NO CARRIER strings). After this command, the

BlueSmiRF will output only

data.

I had posted the message of topic <Bluesmirf, Auto-Master problem with BlueRadio>

viewtopic.php?t=7352&highlight=

HELP, PLEASE !!!

DIEGO GONZALEZ

EMAILS SENT TO SUPPORT OF SPARKFUN:

diego gonzalez wrote:

Hi Level1,

The Bluesmirf that connected doesn`t show any lights, I used the

following comands to change the configuration, I don´t remember the

order of those commands:

ATSW21,2560,11,2560,11

ATSW25,0,1,1,0

ATSW24,2,1,0,0

ATSW20,10,1,0,1

To the Bluesmirf configured as Master I used the following comands in

order:

ATFRST

ATSMA,00A09611FBBC,1101

ATSW25,1,1,0,0

//00A09611FBBC is the Slave direction.

Thank you for your help.

Diego Gonzalez


Date: Mon, 9 Jul 2007 13:34:25 -0600

From: level1@sparkfun.com

To: diegoagonzalez@hotmail.com

Subject: Re: PLEASE SOME HELP ABOUT BLUESMIRF !!!

Hi Diego,

Could you send me the exact set of commands you sent to the bluesmirf?

diego gonzalez wrote:

Hi Level1 of Sparkfun, I followed your instructions about the

Bluesmirf configured as Master: "first just power up the module with

no shorts in it, then open up hyperterminal at the 9600 baud rate

with

no flow control. Then type +++ and 1 “enter” character and let me

know

what happens."

I did the test sending the commands from PC-COM1 ↔ MAX232 ↔ RX

and TX BluesmiRF Master. there is no answer and if I send other

command like AT, there is not answer too.

When I did the test sending the commands from PC-COM1 ↔ MAX232

↔

RX and TX BluesmiRF Slave. there is no answer and if I send other

command like AT or ATSI,2 , I get answers like OK or the name of my

Bluesmirf.

There is another thing that I didn`t mencion before, Using My

Bluedongle and Bluesoleil , when I search for the Bluesmirf

configured as Master this is detected for one second when I turn

it on

but when I try get service I get the answer "SERVICE DISCOVERY

FAILED" so I refresh the searching and the Blusmirf is not detected

again, It´s only detected when It´s turned on while the Bluesoleil

program is searching for devices.

About the other issue, the Bluesmirf that connected doesn`t show any

lights, I used comands to change the configuration before to get that

state, the command were:

ATSW21,2560,11,2560,11 //Change scan intervals thus decreasing the

power consumption from 48mA to 2mA before the module is connected

ATSSN,UsarioSerial //Change service name (virtual serial

port service)

ATSW25,0,1,1,0 //Prevent communication before connected

  • i.e. after this command, you can reconfigure BlueSmiRF only when it

is connected, and you

get out of the data mode using the escape sequence. This is

important,

because the randomly

received and translated IR bytes will be ignored, and will not

accidentally reconfigure the module.

ATSW24,2,1,0,0 //Turn off verbal responses. This is

important, because otherwise the BlueSmiRF will be talking to the RCX

each time you open or

close the port (CONNECT, NO CARRIER strings). After this command, the

BlueSmiRF will output only

data.

ATSW20,10,1,0,1 //Change communication parameters to RCX

default: 2400-odd-1 and store them to flash.

after I made this configuration I lost contact with the Bluesmirf.

I hope this information give you the tools for get me a help with my

problems, If there is not solution I will send you back the

Bluesmirfs

with problems using the returns policy exposed in

http://www.sparkfun.com/commerce/return_policy.php.

I apreciate your help.

Diego Gonzalez.


Date: Thu, 5 Jul 2007 12:52:53 -0600

From: level1@sparkfun.com

To: diegoagonzalez@hotmail.com

Subject: Re: FW: PLEASE SOME HELP ABOUT BLUESMIRF !!!

Hi Diego,

For your first problem can you just confirm something for me,

first just power up the module with no shorts in it, then open up

hyperterminal at the 9600 baud rate with no flow control. Then

type +++

and 1 “enter” character and let me know what happens.

for your second problem it seems that you have probably killed the

dongle. We can have a look at it but it is probably dead and you

will

need to get a new one. If you would like to return it, please

review

the

returns policy here :

http://www.sparkfun.com/commerce/return_policy.php

Please note, depending on whether the device was altered or if

it was a

manufacturing defect will determine if we can service your

return. If

your order meets these requirements, please return the item to:

Spark Fun Electronics

Atn: Returns

2500 Central Ave.

Suite Q

Boulder, CO 80301

Please include the original order # and a note about what the

problem was.

-Support

diego gonzalez wrote:


Hi, I wrote you before ( 15 days a go) but I didn`t get any answer

from you.

I had posted two messages in your forum without an answer with the

author “diegoagonzalez”. This are the messages:

*SECOND MESSAGE

Posted: Wed Jun 27, 2007 5:48 pm Post subject: Bluesmirf

imposible to configure

-----FIRST PROBLEM-----

The situation:

I have 3 Bluesmirf and learning how to use the master and slave

configuration I get to made autoconnection configuring using my

BlueDongle and the BLuesoleil software:

ATDM,00A09611FBBC,1101

ATSW25,1,1,0,0

on my master, 00A09611FBBC is the Slave direction.

Both, Master and Slave are working with the factory default baud

rate.

They autoconnect and the red led turn on in both and the slave can

transmit data to the master, and if I use +++ I can to configure

the slave settings.

The Hardware configuration is:

PC-COM1 ↔ MAX232 ↔ RX and TX BluesmiRF Master

PC-COM2 ↔ MAX232 ↔ RX and TX BluesmiRF Slave

The BIG PROBLEM (Number one) is that I want to get back My Master

to Factory default settings but I can not access to it and make

the ATFRST command, there is no response to any command (+++;

ATUCL), The only thing I get is by my Hyperterminal COM1 is "NO

ANSWER" every 40 seconds and my Blue Dongle dont detect the Master

too.

I have try to get access to master connecting RX with TX, and

connecting RTS with CTS of the Bluesmirf, also try to reset

manually by putting a 5v voltage on PIO 4, but nothing change. The

normal state of the master if there is not a slave is flashing the

green light and leaving the message “NO ANSWER” every 40 seconds

on my COM1.

-----SECOND PROBLEM-----

Configuring one Bluesmirf I made some changes that I can not

remember now, the thing is that when I turn it on non of leds

(green or red) flash, The current goes down to 10 mA aproximatly.

Nor using my bluedongle neighter using the RX and TX of the

Bluesmirf to configure get to works, there is not answer to +++

command by any way.

PLEASE ANYONE HELP ME, IT´S FOR MY GRADUATION PROJECT!!!

*FIRST MESSAGE

Posted: Thu Jun 14, 2007 6:12 pm Post subject: Bluesmirf,

Auto-Master problem with BlueRadio

Hello,

My name is Diego and I 'm from Cali, Colombia. I bought several

Bluetooth Modem - BlueSMiRF from Spark Fun Electronics and I’m

configuring the Bluetooth Modems using ATMP COMMANDS.

The problem is that I configured a Bluetooth Modem to be as

Auto-Master (ATSW25,1,1,0,0) but I forgot to put the ATSMA command

with the Slave Address and the UUID, when I try to access the

Bluetooth Modem using the serial RX and TX I 'm not getting any

answer, I try also to using the +++ command from the Blue Dongle.

Talking about power compsution when I turn on the Blueradio the

Current is close to 40mA and after a few seconds (1 or 2) goes to

almost 1mA or nothing.

the version is 3.5.2.1.3.0. I tried putting 3.3V on PIO4 on the

start up of the Blueradio, but everything continues like it was.

I made the operation with other Bluetooth Modem as Master and I

can get to comunicate to it using the serial RX and TX.

What do I need to do?.. Anyone with the Same Problem?..

Thank for your help, I will apreciate your answer


Finally I measure the average current of my 3 Bluesmirfs:

INPUT VOLTAGE 3.3V:

Master Bluesmirf not connected (green light): 50mA

Slave Bluesmirf not connected (green light): 50mA

The Other Bluesmirf (no light): 10.34mA

Master Bluesmirf connected to Slave(red light): 30mA

Slave Bluesmirf connected to Master(red light): 18mA

INPUT VOLTAGE 5V:

Master Bluesmirf not connected (green light): 70mA

Slave Bluesmirf not connected (green light): 58mA

The Other Bluesmirf (no light): 14.4mA

Master Bluesmirf connected to Slave(red light): 35mA

Slave Bluesmirf connected to Master(red light): 21mA

I’ll apreciate a fast answer, thanks for your attention.

Diego Alejandro Gonzalez

University Javeriana

Cali

Colombia