help with this error? avrdude: Device signature = 0×000000

Hi I’m trying to follow this guide: http://hackaday.com/2010/10/25/avr-prog … -hardware/ to get started with AVR and I’m having some problems…

I’m using an AVR Dragon on OSX… I checked the connections and pins 10 times… I’m getting the following error:

avrdude: Device signature = 0×000000

avrdude: Yikes! Invalid device signature.

Double check connections and try again, or use -F to override this check.

NOTE: I’m using a 328 instead of a 168… but I checked the datasheet and the pinout is the same… Any advise?

Here is a screenshot of my terminal output and my wiring

Terminal Screenshot:

http://itslennysfault.com/stuff/AVRIssue.png

(also note I brought up the command I used at the bottom of the screenshot)

wiring photo:

http://itslennysfault.com/stuff/AVRIssueWires.jpg

Also, to further test the wiring I tried disconnecting the VCC wire from the ribbon cable and I got this error… which seems to say it’s hooked up correctly (in my mind)?

http://itslennysfault.com/stuff/AVRIssue2.png

Please note I’m a TOTAL beginner at this whole AVR thing (hence why i’m trying to make an LED blink) … My best guess so far is that it has something to do with the “fuse bits”? However, I have no idea how to check this or fix it…

I purchased this chip new from sparkfun… I have 2 (I tried both with the same outcome)… I do remember an option to have them install the aurduino bootloader (which i said no to) is there a chance they sent me one with the bootloader? would that cause this problem?

is there any way to do like a factory reset on the chip?

any help is MUCH appreciated. I usually NEVER ask questions as most things can be figured out with google, but since I’m TOTALLY new to this I don’t even know where to start.

thanks in advance

-Lenny

I MAY have found the answer here: http://support.atmel.no/knowledgebase/a … ooting.htm

says if it is returning 0x00

Problem: ISP Frequency is to high.

Solution: Lower ISP freq under the board settings

…problem is I have no idea exactly what it means or how to do this… any advise??