Hi speed analog acquisition?

I’ve used the following sketch (modified from a handy site about Teensy FFT) to time the acquisition of 512 ADC values, but it tops out at about 65kS/s. How are we to acquire at or near the very impressive Artemis MS/s rates?

/*dlp - Using an Artemis Redboard, found for the original 512 samples at 50khz, the measured freq is 38.1khz

if you specify 14 or 16-bit resolution it stays the same

200khz = 65.1

100khz = 65.1

90khz = 65.1

80khz = 52.5

70khz = 52.5

60khz = 43.8

50khz = 38.1 (23.8% low)

40khz = 33.5 (16.2% low)

30khz = 26.6 (11.3% low)

20khz = 17.9 (10.5% low)

*/

#define SAMPLES 512 //Must be a power of 2

#define SAMPLING_FREQUENCY 50000 //Hz

#define REFRESH_RATE 10 //Hz

unsigned long sampling_period_us;

unsigned long useconds_sampling;

unsigned long refresh_period_us;

unsigned long useconds_refresh;

float SamplesAcqFreq;

double vReal[SAMPLES];

double vImag[SAMPLES];

uint8_t analogpin = A0;

void setup() {

Serial.begin(115200);

//analogReadResolution(14); //Set resolution to 14 bit

//analogReadResolution(16); //Set resolution to 16 bit - will pad ADC output with two zeros

sampling_period_us = round(1000000*(1.0/SAMPLING_FREQUENCY));

refresh_period_us = round(1000000*(1.0/REFRESH_RATE));

pinMode(analogpin, INPUT);

}

void loop() {

useconds_refresh = micros();

/SAMPLING/

for(int i=0; i<SAMPLES; i++)

{

useconds_sampling = micros();

vReal = analogRead(analogpin);
vImag = 0;

while(micros() < (useconds_sampling + sampling_period_us)){
//wait…
}
}
SamplesAcqFreq = SAMPLES/((float(micros())-useconds_refresh)/1000000);
Serial.println(SamplesAcqFreq); //print sample freq
while(micros() < (useconds_refresh + refresh_period_us)){ //wait for refresh time
//wait…
}
}
https://www.norwegiancreations.com/2019 … -analysis/

You are doing calculations on sample time in your code. But those are just make-believe results or after-the-fact rates. You probably need to change some register settings to change the ADC clock prescaler to affect the real sample rate. I am unaware of where to find the datasheet of the processor because I am too unfamiliar with the board/chip architecture. But that would be where the solution lies.

I modified a C-code example found in the Ambiq-Micro SDK (adc_lpmode0_dma.c ) and it now works on the Artemis Redboard & Arduino IDE.

Single-channel, single-ended, 14bit acquisition, choosing frequencies that will include one complete wave in the 512-point buffer I measure the following S/s:

500Hz with AVG_8 = 140kS/s.

3kHz with AVG_1 = 1.11MS/s.

Here’s the sketch:

Edited by moderator to add code tags. Please use the code tag button above when posting code.

//*****************************************************************************
//
//! @file adc_lpmode0_dma.c
//!
//! @brief This example takes samples with the ADC at high-speed using DMA.
//!
//! Purpose: This example shows the CTIMER-A3 triggering repeated samples of an external
//! input at 1.2Msps in LPMODE0.  The example uses the CTIMER-A3 to trigger
//! ADC sampling.  Each data point is 8 sample average and is transferred
//! from the ADC FIFO into an SRAM buffer using DMA.

#include "am_bsp.h"

// Define a circular buffer to hold the ADC samples
//*****************************************************************************
#define ADC_EXAMPLE_DEBUG   1
#define ResolutionBits 14

// ADC Sample buffer.
#define ADC_SAMPLE_BUF_SIZE 512
uint32_t g_ui32ADCSampleBuffer[ADC_SAMPLE_BUF_SIZE];

am_hal_adc_sample_t SampleBuffer[ADC_SAMPLE_BUF_SIZE];

unsigned long useconds_refresh;

// ADC Device Handle.
//static void *g_ADCHandle;


// ADC DMA complete flag.
volatile bool                   g_bADCDMAComplete;

// ADC DMA error flag.
volatile bool                   g_bADCDMAError;

// Define the ADC SE0 pin to be used. (A4)
const am_hal_gpio_pincfg_t g_AM_PIN_16_ADCSE0 =
{
    .uFuncSel       = AM_HAL_PIN_16_ADCSE0,
};


// Interrupt handler for the ADC.
//*****************************************************************************
extern "C" void am_adc_isr()  //must use 'extern "C" ' for the Artemis
{
    uint32_t ui32IntMask;

    // Read the interrupt status.
    if (AM_HAL_STATUS_SUCCESS != am_hal_adc_interrupt_status(g_ADCHandle, &ui32IntMask, false))
    {
        //am_util_stdio_printf("Error reading ADC interrupt status\n");
        Serial.println("Error reading ADC interrupt status");
    }

    // Clear the ADC interrupt.
    if (AM_HAL_STATUS_SUCCESS != am_hal_adc_interrupt_clear(g_ADCHandle, ui32IntMask))
    {
        //am_util_stdio_printf("Error clearing ADC interrupt status\n");
        Serial.println("Error clearing ADC interrupt status");
    }

    // If we got a DMA complete, set the flag.
    if (ui32IntMask & AM_HAL_ADC_INT_DCMP)
    {
        g_bADCDMAComplete = true;
    }

    // If we got a DMA error, set the flag.
    if (ui32IntMask & AM_HAL_ADC_INT_DERR)
    {
        g_bADCDMAError = true;
    }
}

// Set up the core for sleeping, and then go to sleep.
//*****************************************************************************
void sleep()
{
    // Disable things that can't run in sleep mode.
//#if (0 == ADC_EXAMPLE_DEBUG)
//    am_bsp_debug_printf_disable();
//#endif

    // Go to Deep Sleep.
    am_hal_sysctrl_sleep(AM_HAL_SYSCTRL_SLEEP_DEEP);
    
    // Re-enable peripherals for run mode.
//#if (0 == ADC_EXAMPLE_DEBUG)
//    am_bsp_debug_printf_enable();
//#endif

}

// Configure the ADC.
//*****************************************************************************
void adc_config_dma()
{
    am_hal_adc_dma_config_t       ADCDMAConfig;

    // Configure the ADC to use DMA for the sample transfer.
    ADCDMAConfig.bDynamicPriority = true;
    ADCDMAConfig.ePriority = AM_HAL_ADC_PRIOR_SERVICE_IMMED;
    ADCDMAConfig.bDMAEnable = true;
    ADCDMAConfig.ui32SampleCount = ADC_SAMPLE_BUF_SIZE;
    ADCDMAConfig.ui32TargetAddress = (uint32_t)g_ui32ADCSampleBuffer;
    if (AM_HAL_STATUS_SUCCESS != am_hal_adc_configure_dma(g_ADCHandle, &ADCDMAConfig))
    {
        //am_util_stdio_printf("Error - configuring ADC DMA failed.\n");
        Serial.println("Error - configuring ADC DMA failed.");
    }
    // Reset the ADC DMA flags.
    g_bADCDMAComplete = false;
    g_bADCDMAError = false;
    
}


// Configure the ADC.
//*****************************************************************************
void adc_config()
{
    am_hal_adc_config_t           ADCConfig;
    am_hal_adc_slot_config_t      ADCSlotConfig;

    // Initialize the ADC and get the handle.
    if ( AM_HAL_STATUS_SUCCESS != am_hal_adc_initialize(0, &g_ADCHandle) )
    {
        //am_util_stdio_printf("Error - reservation of the ADC instance failed.\n");
        Serial.println("Error - reservation of the ADC instance failed.");
    }

    // Power on the ADC.
    if (AM_HAL_STATUS_SUCCESS != am_hal_adc_power_control(g_ADCHandle,
                                                          AM_HAL_SYSCTRL_WAKE,
                                                          false) )
    {
        //am_util_stdio_printf("Error - ADC power on failed.\n");
        Serial.println("Error - ADC power on failed.");
    }

    // Set up the ADC configuration parameters. These settings are reasonable
    // for accurate measurements at a low sample rate.
    ADCConfig.eClock             = AM_HAL_ADC_CLKSEL_HFRC;
    ADCConfig.ePolarity          = AM_HAL_ADC_TRIGPOL_RISING;
    ADCConfig.eTrigger           = AM_HAL_ADC_TRIGSEL_SOFTWARE;
    ADCConfig.eReference         = AM_HAL_ADC_REFSEL_INT_2P0;
    /*
    AM_HAL_ADC_REFSEL_INT_2P0,
    AM_HAL_ADC_REFSEL_INT_1P5,
    AM_HAL_ADC_REFSEL_EXT_2P0,
    AM_HAL_ADC_REFSEL_EXT_1P5
    */
    ADCConfig.eClockMode         = AM_HAL_ADC_CLKMODE_LOW_LATENCY;
    ADCConfig.ePowerMode         = AM_HAL_ADC_LPMODE0; 
    ADCConfig.eRepeat            = AM_HAL_ADC_REPEATING_SCAN; //AM_HAL_ADC_SINGLE_SCAN
    if (AM_HAL_STATUS_SUCCESS != am_hal_adc_configure(g_ADCHandle, &ADCConfig))
    {
        //am_util_stdio_printf("Error - configuring ADC failed.\n");
        Serial.println("Error - configuring ADC failed.");
    }

    // Set up an ADC slot
    ADCSlotConfig.eMeasToAvg      = AM_HAL_ADC_SLOT_AVG_1;
    ADCSlotConfig.ePrecisionMode  = AM_HAL_ADC_SLOT_14BIT;
    ADCSlotConfig.eChannel        = AM_HAL_ADC_SLOT_CHSEL_SE0; 
    ADCSlotConfig.bWindowCompare  = false;
    ADCSlotConfig.bEnabled        = true;
    /*
    AM_HAL_ADC_SLOT_AVG_1,
    AM_HAL_ADC_SLOT_AVG_2,
    AM_HAL_ADC_SLOT_AVG_4,
    AM_HAL_ADC_SLOT_AVG_8,
    AM_HAL_ADC_SLOT_AVG_16,
    AM_HAL_ADC_SLOT_AVG_32,
    AM_HAL_ADC_SLOT_AVG_64,
    AM_HAL_ADC_SLOT_AVG_128
    
    AM_HAL_ADC_SLOT_14BIT,
    AM_HAL_ADC_SLOT_12BIT,
    AM_HAL_ADC_SLOT_10BIT,
    AM_HAL_ADC_SLOT_8BIT

        // Single-ended channels
    AM_HAL_ADC_SLOT_CHSEL_SE0, (pad 16, ArtemisRB A4)
    AM_HAL_ADC_SLOT_CHSEL_SE1, (pad 29, ArtemisRB A0)
    AM_HAL_ADC_SLOT_CHSEL_SE2, (pad 11, ArtemisRB A1)
    AM_HAL_ADC_SLOT_CHSEL_SE3, (pad 31, ArtemisRB A5)
    AM_HAL_ADC_SLOT_CHSEL_SE4, (pad 32, ArtemisRB A8)
    AM_HAL_ADC_SLOT_CHSEL_SE5, (pad 33, ArtemisRB A3)
    AM_HAL_ADC_SLOT_CHSEL_SE6, (pad 34, ArtemisRB A2)
    AM_HAL_ADC_SLOT_CHSEL_SE7, (pad 35, ArtemisRB n/a)
    AM_HAL_ADC_SLOT_CHSEL_SE8, (pad 13, ArtemisRB A10)
    AM_HAL_ADC_SLOT_CHSEL_SE9, (pad 12, ArtemisRB A9)
    // Differential channels. 
    AM_HAL_ADC_SLOT_CHSEL_DF0, pads 12 (-), pad 13(+)
    AM_HAL_ADC_SLOT_CHSEL_DF1, pads 15 (-), pad 14(+) (ArtemisRB n/a)
    // Miscellaneous other signals.
    AM_HAL_ADC_SLOT_CHSEL_TEMP,
    AM_HAL_ADC_SLOT_CHSEL_BATT,
    AM_HAL_ADC_SLOT_CHSEL_VSS


     */
    if (AM_HAL_STATUS_SUCCESS != am_hal_adc_configure_slot(g_ADCHandle, 0, &ADCSlotConfig))
    {
        //am_util_stdio_printf("Error - configuring ADC Slot 0 failed.\n");
        Serial.println("Error - configuring ADC Slot 0 failed.");
    }

    // Configure the ADC to use DMA for the sample transfer.
    adc_config_dma();
    // For this example, the samples will be coming in slowly. This means we
    // can afford to wake up for every conversion.
    //
    am_hal_adc_interrupt_enable(g_ADCHandle, AM_HAL_ADC_INT_DERR | AM_HAL_ADC_INT_DCMP );

    // Enable the ADC.
    //
    if (AM_HAL_STATUS_SUCCESS != am_hal_adc_enable(g_ADCHandle))
    {
        //am_util_stdio_printf("Error - enabling ADC failed.\n");
        Serial.println("Error - enabling ADC failed.");
    }
}


// Initialize the ADC repetitive sample timer A3.
//*****************************************************************************
void init_timerA3_for_ADC()
{    
    // Start a timer to trigger the ADC periodically (1 second).?? Must be a hold-over from another version
    am_hal_ctimer_config_single(3, AM_HAL_CTIMER_TIMERA,
                                AM_HAL_CTIMER_HFRC_12MHZ    |
                                AM_HAL_CTIMER_FN_REPEAT     |
                                AM_HAL_CTIMER_INT_ENABLE);

    am_hal_ctimer_int_enable(AM_HAL_CTIMER_INT_TIMERA3);

    am_hal_ctimer_period_set(3, AM_HAL_CTIMER_TIMERA, 10, 5); //10 tick period, 5 ticks wide

    // Enable the timer A3 to trigger the ADC directly
    am_hal_ctimer_adc_trigger_enable();

    // Start the timer.
    am_hal_ctimer_start(3, AM_HAL_CTIMER_TIMERA);
}


void setup() {
     Serial.begin(115200);
     while (!Serial) {}
     Serial.println("Hi-speed ADC test");
    // Set the clock frequency.
     if (AM_HAL_STATUS_SUCCESS != am_hal_clkgen_control(AM_HAL_CLKGEN_CONTROL_SYSCLK_MAX, 0))
    {
        //am_util_stdio_printf("Error - configuring the system clock failed.\n");
        Serial.println("Error - configuring the system clock failed.");
    }

    // Set the default cache configuration and enable it.
    if (AM_HAL_STATUS_SUCCESS != am_hal_cachectrl_config(&am_hal_cachectrl_defaults))
    {
        //am_util_stdio_printf("Error - configuring the system cache failed.\n");
        Serial.println("Error - configuring the system cache failed.");
    }
    if (AM_HAL_STATUS_SUCCESS != am_hal_cachectrl_enable())
    {
        //am_util_stdio_printf("Error - enabling the system cache failed.\n");
        Serial.println("Error - enabling the system cache failed.");
    }

    // Configure the board for low power operation.
    am_bsp_low_power_init();

    // Enable only the first 512KB bank of Flash (0).  Disable Flash(1)
    if (AM_HAL_STATUS_SUCCESS != am_hal_pwrctrl_memory_enable(AM_HAL_PWRCTRL_MEM_FLASH_MIN))
    {
        //am_util_stdio_printf("Error - configuring the flash memory failed.\n");
        Serial.println("Error - configuring the flash memory failed.");
    }

    // Enable the first 32K of TCM SRAM.
    if (AM_HAL_STATUS_SUCCESS != am_hal_pwrctrl_memory_enable(AM_HAL_PWRCTRL_MEM_SRAM_32K_DTCM))
    {
        //am_util_stdio_printf("Error - configuring the SRAM failed.\n");
        Serial.println("Error - configuring the SRAM failed.");
    }

    // Start the ITM interface.
    am_bsp_itm_printf_enable();

    // Start the CTIMER A3 for timer-based ADC measurements.
    init_timerA3_for_ADC();

    // Enable interrupts.
    NVIC_EnableIRQ(ADC_IRQn);
    am_hal_interrupt_master_enable();

    // Set a pin to act as our ADC input
    am_hal_gpio_pinconfig(16, g_AM_PIN_16_ADCSE0); //artemis pad 16 is A4

    // Configure the ADC
    adc_config();

    // Trigger the ADC sampling for the first time manually.
    if (AM_HAL_STATUS_SUCCESS != am_hal_adc_sw_trigger(g_ADCHandle))
    {
        //am_util_stdio_printf("Error - triggering the ADC failed.\n");
        Serial.println("Error - triggering the ADC failed.");
    }

    // Print the banner.
    am_util_stdio_terminal_clear();
    //am_util_stdio_printf("ADC Example with 1.2Msps and LPMODE=0\n");
    Serial.println("ADC Example with 1.2Msps and LPMODE=0");

    // Allow time for all printing to finish.
    am_util_delay_ms(10);

    // We are done printing. Disable debug printf messages on ITM.
//#if (0 == ADC_EXAMPLE_DEBUG)
//    am_bsp_debug_printf_disable();
//#endif

  
}

void loop() {
        // Go to Deep Sleep.
        useconds_refresh = micros();
        if (!g_bADCDMAComplete)
        {
            sleep();
        }

        // Check for DMA errors.
        if (g_bADCDMAError)
        {
            //am_util_stdio_printf("DMA Error occured\n");
            Serial.println("DMA Error occured");
            while(1);
        }

        // Check if the ADC DMA completion interrupt occurred.
        if (g_bADCDMAComplete)
        {  
            for (int i=0; i<ADC_SAMPLE_BUF_SIZE; i++){
                  //14 bit is 0-16383 on a range of 0-2V  
                uint32_t result = g_ui32ADCSampleBuffer[i];//*(2.0 /16383.0);
                //Shift result depending on resolution, averaging
                result = result >> (6);
               // Serial.println(result);
                Serial.println(result*(2.0 /16383.0),3);
              }
             while(1){} 
#if ADC_EXAMPLE_DEBUG
            {
                uint32_t        ui32SampleCount;
                am_util_stdio_printf("DMA Complete\n");
                ui32SampleCount = ADC_SAMPLE_BUF_SIZE;
                if (AM_HAL_STATUS_SUCCESS != am_hal_adc_samples_read(g_ADCHandle, false,
                                                                     g_ui32ADCSampleBuffer,
                                                                     &ui32SampleCount,
                                                                     SampleBuffer))
                {
                    //am_util_stdio_printf("Error - failed to process samples.\n");
                    Serial.println("Error - failed to process samples.");
                }
            }
#endif

            // Reset the DMA completion and error flags.
            g_bADCDMAComplete = false;

            // Re-configure the ADC DMA.
            adc_config_dma();

            // Clear the ADC interrupts.
            if (AM_HAL_STATUS_SUCCESS != am_hal_adc_interrupt_clear(g_ADCHandle, 0xFFFFFFFF))
            {
                //am_util_stdio_printf("Error - clearing the ADC interrupts failed.\n");
                Serial.println("Error - clearing the ADC interrupts failed.");
            }

            // Trigger the ADC sampling for the first time manually.
            if (AM_HAL_STATUS_SUCCESS != am_hal_adc_sw_trigger(g_ADCHandle))
            {
                //am_util_stdio_printf("Error - triggering the ADC failed.\n");
                Serial.println("Error - triggering the ADC failed.");
            }
        } // if ()

}

There was a typo in the last working sketch for this so I’ll re-post it.

Now that I’ve got 1 channel working, I’m going for 2 channels, but it’s eluding me so far. Any thoughts?

Edited by moderator to add code tags.

//*****************************************************************************
//
//! @file adc_lpmode0_dma.c
//!
//! @brief This example takes samples with the ADC at high-speed using DMA.
//!
//! Purpose: This example shows the CTIMER-A3 triggering repeated samples of an external
//! input at 1.2Msps in LPMODE0.  The example uses the CTIMER-A3 to trigger
//! ADC sampling.  Each data point is 8 sample average and is transferred
//! from the ADC FIFO into an SRAM buffer using DMA.

#include "am_bsp.h"

// Define a circular buffer to hold the ADC samples
//*****************************************************************************
#define ADC_EXAMPLE_DEBUG   1
#define ResolutionBits 14

// ADC Sample buffer.
#define ADC_SAMPLE_BUF_SIZE 512
uint32_t g_ui32ADCSampleBuffer[ADC_SAMPLE_BUF_SIZE];

am_hal_adc_sample_t SampleBuffer[ADC_SAMPLE_BUF_SIZE];

unsigned long useconds_refresh;

// ADC Device Handle.
//static void *g_ADCHandle;


// ADC DMA complete flag.
volatile bool                   g_bADCDMAComplete;

// ADC DMA error flag.
volatile bool                   g_bADCDMAError;

// Define the ADC SE0 pin to be used. (A4)
const am_hal_gpio_pincfg_t g_AM_PIN_16_ADCSE0 =
{
    .uFuncSel       = AM_HAL_PIN_16_ADCSE0,
};


// Interrupt handler for the ADC.
//*****************************************************************************
extern "C" void am_adc_isr()  //must use 'extern "C" ' for the Artemis
{
    uint32_t ui32IntMask;

    // Read the interrupt status.
    if (AM_HAL_STATUS_SUCCESS != am_hal_adc_interrupt_status(g_ADCHandle, &ui32IntMask, false))
    {
        //am_util_stdio_printf("Error reading ADC interrupt status\n");
        Serial.println("Error reading ADC interrupt status");
    }

    // Clear the ADC interrupt.
    if (AM_HAL_STATUS_SUCCESS != am_hal_adc_interrupt_clear(g_ADCHandle, ui32IntMask))
    {
        //am_util_stdio_printf("Error clearing ADC interrupt status\n");
        Serial.println("Error clearing ADC interrupt status");
    }

    // If we got a DMA complete, set the flag.
    if (ui32IntMask & AM_HAL_ADC_INT_DCMP)
    {
        g_bADCDMAComplete = true;
    }

    // If we got a DMA error, set the flag.
    if (ui32IntMask & AM_HAL_ADC_INT_DERR)
    {
        g_bADCDMAError = true;
    }
}

// Set up the core for sleeping, and then go to sleep.
//*****************************************************************************
void sleep()
{
    // Disable things that can't run in sleep mode.
//#if (0 == ADC_EXAMPLE_DEBUG)
//    am_bsp_debug_printf_disable();
//#endif

    // Go to Deep Sleep.
    am_hal_sysctrl_sleep(AM_HAL_SYSCTRL_SLEEP_DEEP);
    
    // Re-enable peripherals for run mode.
//#if (0 == ADC_EXAMPLE_DEBUG)
//    am_bsp_debug_printf_enable();
//#endif

}

// Configure the ADC.
//*****************************************************************************
void adc_config_dma()
{
    am_hal_adc_dma_config_t       ADCDMAConfig;

    // Configure the ADC to use DMA for the sample transfer.
    ADCDMAConfig.bDynamicPriority = true;
    ADCDMAConfig.ePriority = AM_HAL_ADC_PRIOR_SERVICE_IMMED;
    ADCDMAConfig.bDMAEnable = true;
    ADCDMAConfig.ui32SampleCount = ADC_SAMPLE_BUF_SIZE;
    ADCDMAConfig.ui32TargetAddress = (uint32_t)g_ui32ADCSampleBuffer;
    if (AM_HAL_STATUS_SUCCESS != am_hal_adc_configure_dma(g_ADCHandle, &ADCDMAConfig))
    {
        //am_util_stdio_printf("Error - configuring ADC DMA failed.\n");
        Serial.println("Error - configuring ADC DMA failed.");
    }
    // Reset the ADC DMA flags.
    g_bADCDMAComplete = false;
    g_bADCDMAError = false;
    
}


// Configure the ADC.
//*****************************************************************************
void adc_config()
{
    am_hal_adc_config_t           ADCConfig;
    am_hal_adc_slot_config_t      ADCSlotConfig;

    // Initialize the ADC and get the handle.
    if ( AM_HAL_STATUS_SUCCESS != am_hal_adc_initialize(0, &g_ADCHandle) )
    {
        //am_util_stdio_printf("Error - reservation of the ADC instance failed.\n");
        Serial.println("Error - reservation of the ADC instance failed.");
    }

    // Power on the ADC.
    if (AM_HAL_STATUS_SUCCESS != am_hal_adc_power_control(g_ADCHandle,
                                                          AM_HAL_SYSCTRL_WAKE,
                                                          false) )
    {
        //am_util_stdio_printf("Error - ADC power on failed.\n");
        Serial.println("Error - ADC power on failed.");
    }

    // Set up the ADC configuration parameters. These settings are reasonable
    // for accurate measurements at a low sample rate.
    ADCConfig.eClock             = AM_HAL_ADC_CLKSEL_HFRC;
    ADCConfig.ePolarity          = AM_HAL_ADC_TRIGPOL_RISING;
    ADCConfig.eTrigger           = AM_HAL_ADC_TRIGSEL_SOFTWARE;
    ADCConfig.eReference         = AM_HAL_ADC_REFSEL_INT_2P0;
    /*
    AM_HAL_ADC_REFSEL_INT_2P0,
    AM_HAL_ADC_REFSEL_INT_1P5,
    AM_HAL_ADC_REFSEL_EXT_2P0,
    AM_HAL_ADC_REFSEL_EXT_1P5
    */
    ADCConfig.eClockMode         = AM_HAL_ADC_CLKMODE_LOW_LATENCY;
    ADCConfig.ePowerMode         = AM_HAL_ADC_LPMODE0; 
    ADCConfig.eRepeat            = AM_HAL_ADC_REPEATING_SCAN; //AM_HAL_ADC_SINGLE_SCAN
    if (AM_HAL_STATUS_SUCCESS != am_hal_adc_configure(g_ADCHandle, &ADCConfig))
    {
        //am_util_stdio_printf("Error - configuring ADC failed.\n");
        Serial.println("Error - configuring ADC failed.");
    }

    // Set up an ADC slot
    ADCSlotConfig.eMeasToAvg      = AM_HAL_ADC_SLOT_AVG_1;
    ADCSlotConfig.ePrecisionMode  = AM_HAL_ADC_SLOT_14BIT;
    ADCSlotConfig.eChannel        = AM_HAL_ADC_SLOT_CHSEL_SE0; 
    ADCSlotConfig.bWindowCompare  = false;
    ADCSlotConfig.bEnabled        = true;
    /*
    AM_HAL_ADC_SLOT_AVG_1,
    AM_HAL_ADC_SLOT_AVG_2,
    AM_HAL_ADC_SLOT_AVG_4,
    AM_HAL_ADC_SLOT_AVG_8,
    AM_HAL_ADC_SLOT_AVG_16,
    AM_HAL_ADC_SLOT_AVG_32,
    AM_HAL_ADC_SLOT_AVG_64,
    AM_HAL_ADC_SLOT_AVG_128
    
    AM_HAL_ADC_SLOT_14BIT,
    AM_HAL_ADC_SLOT_12BIT,
    AM_HAL_ADC_SLOT_10BIT,
    AM_HAL_ADC_SLOT_8BIT

        // Single-ended channels
    AM_HAL_ADC_SLOT_CHSEL_SE0, (pad 16, ArtemisRB A4)
    AM_HAL_ADC_SLOT_CHSEL_SE1, (pad 29, ArtemisRB A0)
    AM_HAL_ADC_SLOT_CHSEL_SE2, (pad 11, ArtemisRB A1)
    AM_HAL_ADC_SLOT_CHSEL_SE3, (pad 31, ArtemisRB A5)
    AM_HAL_ADC_SLOT_CHSEL_SE4, (pad 32, ArtemisRB A8)
    AM_HAL_ADC_SLOT_CHSEL_SE5, (pad 33, ArtemisRB A3)
    AM_HAL_ADC_SLOT_CHSEL_SE6, (pad 34, ArtemisRB A2)
    AM_HAL_ADC_SLOT_CHSEL_SE7, (pad 35, ArtemisRB n/a)
    AM_HAL_ADC_SLOT_CHSEL_SE8, (pad 13, ArtemisRB A10)
    AM_HAL_ADC_SLOT_CHSEL_SE9, (pad 12, ArtemisRB A9)
    // Differential channels. 
    AM_HAL_ADC_SLOT_CHSEL_DF0, pads 12 (-), pad 13(+)
    AM_HAL_ADC_SLOT_CHSEL_DF1, pads 15 (-), pad 14(+) (ArtemisRB n/a)
    // Miscellaneous other signals.
    AM_HAL_ADC_SLOT_CHSEL_TEMP,
    AM_HAL_ADC_SLOT_CHSEL_BATT,
    AM_HAL_ADC_SLOT_CHSEL_VSS


     */
    if (AM_HAL_STATUS_SUCCESS != am_hal_adc_configure_slot(g_ADCHandle, 0, &ADCSlotConfig))
    {
        //am_util_stdio_printf("Error - configuring ADC Slot 0 failed.\n");
        Serial.println("Error - configuring ADC Slot 0 failed.");
    }

    // Configure the ADC to use DMA for the sample transfer.
    adc_config_dma();
    // For this example, the samples will be coming in slowly. This means we
    // can afford to wake up for every conversion.
    //
    am_hal_adc_interrupt_enable(g_ADCHandle, AM_HAL_ADC_INT_DERR | AM_HAL_ADC_INT_DCMP );

    // Enable the ADC.
    //
    if (AM_HAL_STATUS_SUCCESS != am_hal_adc_enable(g_ADCHandle))
    {
        //am_util_stdio_printf("Error - enabling ADC failed.\n");
        Serial.println("Error - enabling ADC failed.");
    }
}


// Initialize the ADC repetitive sample timer A3.
//*****************************************************************************
void init_timerA3_for_ADC()
{    
    // Start a timer to trigger the ADC periodically (1 second).?? Must be a hold-over from another version
    am_hal_ctimer_config_single(3, AM_HAL_CTIMER_TIMERA,
                                AM_HAL_CTIMER_HFRC_12MHZ    |
                                AM_HAL_CTIMER_FN_REPEAT     |
                                AM_HAL_CTIMER_INT_ENABLE);

    am_hal_ctimer_int_enable(AM_HAL_CTIMER_INT_TIMERA3);

    am_hal_ctimer_period_set(3, AM_HAL_CTIMER_TIMERA, 10, 5); //10 tick period, 5 ticks wide

    // Enable the timer A3 to trigger the ADC directly
    am_hal_ctimer_adc_trigger_enable();

    // Start the timer.
    am_hal_ctimer_start(3, AM_HAL_CTIMER_TIMERA);
}


void setup() {
     Serial.begin(115200);
     while (!Serial) {}
     Serial.println("Hi-speed ADC test");
    // Set the clock frequency.
     if (AM_HAL_STATUS_SUCCESS != am_hal_clkgen_control(AM_HAL_CLKGEN_CONTROL_SYSCLK_MAX, 0))
    {
        //am_util_stdio_printf("Error - configuring the system clock failed.\n");
        Serial.println("Error - configuring the system clock failed.");
    }

    // Set the default cache configuration and enable it.
    if (AM_HAL_STATUS_SUCCESS != am_hal_cachectrl_config(&am_hal_cachectrl_defaults))
    {
        //am_util_stdio_printf("Error - configuring the system cache failed.\n");
        Serial.println("Error - configuring the system cache failed.");
    }
    if (AM_HAL_STATUS_SUCCESS != am_hal_cachectrl_enable())
    {
        //am_util_stdio_printf("Error - enabling the system cache failed.\n");
        Serial.println("Error - enabling the system cache failed.");
    }

    // Configure the board for low power operation.
    am_bsp_low_power_init();

    // Enable only the first 512KB bank of Flash (0).  Disable Flash(1)
    if (AM_HAL_STATUS_SUCCESS != am_hal_pwrctrl_memory_enable(AM_HAL_PWRCTRL_MEM_FLASH_MIN))
    {
        //am_util_stdio_printf("Error - configuring the flash memory failed.\n");
        Serial.println("Error - configuring the flash memory failed.");
    }

    // Enable the first 32K of TCM SRAM.
    if (AM_HAL_STATUS_SUCCESS != am_hal_pwrctrl_memory_enable(AM_HAL_PWRCTRL_MEM_SRAM_32K_DTCM))
    {
        //am_util_stdio_printf("Error - configuring the SRAM failed.\n");
        Serial.println("Error - configuring the SRAM failed.");
    }

    // Start the ITM interface.
    am_bsp_itm_printf_enable();

    // Start the CTIMER A3 for timer-based ADC measurements.
    init_timerA3_for_ADC();

    // Enable interrupts.
    NVIC_EnableIRQ(ADC_IRQn);
    am_hal_interrupt_master_enable();

    // Set a pin to act as our ADC input
    am_hal_gpio_pinconfig(16, g_AM_PIN_16_ADCSE0); //artemis pad 16 is A4

    // Configure the ADC
    adc_config();

    // Trigger the ADC sampling for the first time manually.
    if (AM_HAL_STATUS_SUCCESS != am_hal_adc_sw_trigger(g_ADCHandle))
    {
        //am_util_stdio_printf("Error - triggering the ADC failed.\n");
        Serial.println("Error - triggering the ADC failed.");
    }

    // Print the banner.
    am_util_stdio_terminal_clear();
    //am_util_stdio_printf("ADC Example with 1.2Msps and LPMODE=0\n");
    Serial.println("ADC Example with 1.2Msps and LPMODE=0");

    // Allow time for all printing to finish.
    am_util_delay_ms(10);

    // We are done printing. Disable debug printf messages on ITM.
//#if (0 == ADC_EXAMPLE_DEBUG)
//    am_bsp_debug_printf_disable();
//#endif

  
}

void loop() {
        // Go to Deep Sleep.
        useconds_refresh = micros();
        if (!g_bADCDMAComplete)
        {
            sleep();
        }

        // Check for DMA errors.
        if (g_bADCDMAError)
        {
            //am_util_stdio_printf("DMA Error occured\n");
            Serial.println("DMA Error occured");
            while(1);
        }

        // Check if the ADC DMA completion interrupt occurred.
        if (g_bADCDMAComplete)
        {  
            for (int i=0; i<ADC_SAMPLE_BUF_SIZE; i++){
                  //14 bit is 0-16383 on a range of 0-2V  
                uint32_t result = g_ui32ADCSampleBuffer[i];//*(2.0 /16383.0);
                //Shift result depending on resolution, averaging
                result = result >> (6);
               // Serial.println(result);
                Serial.println(result*(2.0 /16383.0),3);
              }
             while(1){}   //pause execution


            // Reset the DMA completion and error flags.
            g_bADCDMAComplete = false;

            // Re-configure the ADC DMA.
            adc_config_dma();

            // Clear the ADC interrupts.
            if (AM_HAL_STATUS_SUCCESS != am_hal_adc_interrupt_clear(g_ADCHandle, 0xFFFFFFFF))
            {
                //am_util_stdio_printf("Error - clearing the ADC interrupts failed.\n");
                Serial.println("Error - clearing the ADC interrupts failed.");
            }

            // Trigger the ADC sampling for the first time manually.
            if (AM_HAL_STATUS_SUCCESS != am_hal_adc_sw_trigger(g_ADCHandle))
            {
                //am_util_stdio_printf("Error - triggering the ADC failed.\n");
                Serial.println("Error - triggering the ADC failed.");
            }
        } // if ()

}

Here’s a mod to the sketch that will do 2 Channels at high speed. A 2kHz signal will put 2 completes waves in the buffer and I measure a sample frequency of 552kS/s per channel. As expected half the frequency of a single channel.

MODERATOR NOTE: PLEASE USE CODE TAGS WHEN INCLUDING CODE.

//*****************************************************************************
//
//! @file adc_lpmode0_dma.c
//!
//! @brief This example takes samples with the ADC at high-speed using DMA.
//!
//! Purpose: This example shows the CTIMER-A3 triggering repeated samples of an external
//! input at 1.2Msps in LPMODE0. The example uses the CTIMER-A3 to trigger
//! ADC sampling. Each data point is 8 sample average and is transferred
//! from the ADC FIFO into an SRAM buffer using DMA.

// uses bit-masking to parse out the data

#include "am_bsp.h"


// ADC Sample buffer.
 
#define ADC_SAMPLE_BUF_SIZE (1024) //2channels at 512 samples.  Ch1 and Ch2 alternate in the buffer

uint32_t g_ui32ADCSampleBuffer[ADC_SAMPLE_BUF_SIZE];

unsigned long useconds_refresh;

// ADC Device Handle. Already declared.
//static void *g_ADCHandle;

// ADC DMA complete flag.
volatile bool g_bADCDMAComplete;

// ADC DMA error flag.
volatile bool g_bADCDMAError;

// Define the ADC SE0 pin to be used. (A4)
const am_hal_gpio_pincfg_t g_AM_PIN_16_ADCSE0 =
{
  .uFuncSel = AM_HAL_PIN_16_ADCSE0,
};

// Define the ADC SE3 pin to be used. (A5)
const am_hal_gpio_pincfg_t g_AM_PIN_31_ADCSE3 =
{
  .uFuncSel = AM_HAL_PIN_31_ADCSE3,
};

// Interrupt handler for the ADC.
//*****************************************************************************
extern "C" void am_adc_isr() //must use 'extern "C" ' for the Artemis
{
  uint32_t ui32IntMask;

  // Read the interrupt status.
  if (AM_HAL_STATUS_SUCCESS != am_hal_adc_interrupt_status(g_ADCHandle, &ui32IntMask, false))
  {
    Serial.println("Error reading ADC interrupt status");
  }

  // Clear the ADC interrupt.
  if (AM_HAL_STATUS_SUCCESS != am_hal_adc_interrupt_clear(g_ADCHandle, ui32IntMask))
  {
    Serial.println("Error clearing ADC interrupt status");
  }

  // If we got a DMA complete, set the flag.
  if (ui32IntMask & AM_HAL_ADC_INT_DCMP)
  {
    g_bADCDMAComplete = true;
  }

  // If we got a DMA error, set the flag.
  if (ui32IntMask & AM_HAL_ADC_INT_DERR)
  {
    g_bADCDMAError = true;
  }
}

// Set up the core for sleeping, and then go to sleep.
//*****************************************************************************
void sleep()
{
  // Disable things that can't run in sleep mode.
  //#if (0 == ADC_EXAMPLE_DEBUG)
  // am_bsp_debug_printf_disable();
  //#endif

  // Go to Deep Sleep.
  am_hal_sysctrl_sleep(AM_HAL_SYSCTRL_SLEEP_DEEP);

  // Re-enable peripherals for run mode.
  //#if (0 == ADC_EXAMPLE_DEBUG)
  // am_bsp_debug_printf_enable();
  //#endif

}

// Configure the ADC.
//*****************************************************************************
void adc_config_dma()
{
  am_hal_adc_dma_config_t ADCDMAConfig;

  // Configure the ADC to use DMA for the sample transfer.
  ADCDMAConfig.bDynamicPriority = true;
  ADCDMAConfig.ePriority = AM_HAL_ADC_PRIOR_SERVICE_IMMED;
  ADCDMAConfig.bDMAEnable = true;
  ADCDMAConfig.ui32SampleCount = ADC_SAMPLE_BUF_SIZE;
  ADCDMAConfig.ui32TargetAddress = (uint32_t)g_ui32ADCSampleBuffer;
  if (AM_HAL_STATUS_SUCCESS != am_hal_adc_configure_dma(g_ADCHandle, &ADCDMAConfig))
  {
    Serial.println("Error - configuring ADC DMA failed.");
  }
  // Reset the ADC DMA flags.
  g_bADCDMAComplete = false;
  g_bADCDMAError = false;

}


// Configure the ADC.
//*****************************************************************************
void adc_config()
{
  am_hal_adc_config_t ADCConfig;
  am_hal_adc_slot_config_t ADCSlotConfig;

  // Initialize the ADC and get the handle.
  if ( AM_HAL_STATUS_SUCCESS != am_hal_adc_initialize(0, &g_ADCHandle) )
  {
    Serial.println("Error - reservation of the ADC instance failed.");
  }

  // Power on the ADC.
  if (AM_HAL_STATUS_SUCCESS != am_hal_adc_power_control(g_ADCHandle,
      AM_HAL_SYSCTRL_WAKE,
      false) )
  {
    //am_util_stdio_printf("Error - ADC power on failed.\n");
    Serial.println("Error - ADC power on failed.");
  }

  // Set up the ADC configuration parameters. These settings are reasonable
  // for accurate measurements at a low sample rate.
  ADCConfig.eClock = AM_HAL_ADC_CLKSEL_HFRC;
  ADCConfig.ePolarity = AM_HAL_ADC_TRIGPOL_RISING;
  ADCConfig.eTrigger = AM_HAL_ADC_TRIGSEL_SOFTWARE;
  ADCConfig.eReference = AM_HAL_ADC_REFSEL_INT_2P0;
  /*
    AM_HAL_ADC_REFSEL_INT_2P0,
    AM_HAL_ADC_REFSEL_INT_1P5,
    AM_HAL_ADC_REFSEL_EXT_2P0,
    AM_HAL_ADC_REFSEL_EXT_1P5
  */
  ADCConfig.eClockMode = AM_HAL_ADC_CLKMODE_LOW_LATENCY;
  ADCConfig.ePowerMode = AM_HAL_ADC_LPMODE0;
  ADCConfig.eRepeat = AM_HAL_ADC_REPEATING_SCAN; //AM_HAL_ADC_SINGLE_SCAN
  if (AM_HAL_STATUS_SUCCESS != am_hal_adc_configure(g_ADCHandle, &ADCConfig))
  {
    //am_util_stdio_printf("Error - configuring ADC failed.\n");
    Serial.println("Error - configuring ADC failed.");
  }

  // Set up an ADC slot 0
  ADCSlotConfig.eMeasToAvg = AM_HAL_ADC_SLOT_AVG_1;
  ADCSlotConfig.ePrecisionMode = AM_HAL_ADC_SLOT_14BIT;
  ADCSlotConfig.eChannel = AM_HAL_ADC_SLOT_CHSEL_SE0; //A4
  ADCSlotConfig.bWindowCompare = false;
  ADCSlotConfig.bEnabled = true;
  /*
    AM_HAL_ADC_SLOT_AVG_1,
    AM_HAL_ADC_SLOT_AVG_2,
    AM_HAL_ADC_SLOT_AVG_4,
    AM_HAL_ADC_SLOT_AVG_8,
    AM_HAL_ADC_SLOT_AVG_16,
    AM_HAL_ADC_SLOT_AVG_32,
    AM_HAL_ADC_SLOT_AVG_64,
    AM_HAL_ADC_SLOT_AVG_128

    AM_HAL_ADC_SLOT_14BIT,
    AM_HAL_ADC_SLOT_12BIT,
    AM_HAL_ADC_SLOT_10BIT,
    AM_HAL_ADC_SLOT_8BIT

    // Single-ended channels
    AM_HAL_ADC_SLOT_CHSEL_SE0, (pad 16, ArtemisRB A4)
    AM_HAL_ADC_SLOT_CHSEL_SE1, (pad 29, ArtemisRB A0)
    AM_HAL_ADC_SLOT_CHSEL_SE2, (pad 11, ArtemisRB A1)
    AM_HAL_ADC_SLOT_CHSEL_SE3, (pad 31, ArtemisRB A5)
    AM_HAL_ADC_SLOT_CHSEL_SE4, (pad 32, ArtemisRB A8)
    AM_HAL_ADC_SLOT_CHSEL_SE5, (pad 33, ArtemisRB A3)
    AM_HAL_ADC_SLOT_CHSEL_SE6, (pad 34, ArtemisRB A2)
    AM_HAL_ADC_SLOT_CHSEL_SE7, (pad 35, ArtemisRB n/a)
    AM_HAL_ADC_SLOT_CHSEL_SE8, (pad 13, ArtemisRB A10)
    AM_HAL_ADC_SLOT_CHSEL_SE9, (pad 12, ArtemisRB A9)
    // Differential channels.
    AM_HAL_ADC_SLOT_CHSEL_DF0, pads 12 (-), pad 13(+)
    AM_HAL_ADC_SLOT_CHSEL_DF1, pads 15 (-), pad 14(+) (ArtemisRB n/a)
    // Miscellaneous other signals.
    AM_HAL_ADC_SLOT_CHSEL_TEMP,
    AM_HAL_ADC_SLOT_CHSEL_BATT,
    AM_HAL_ADC_SLOT_CHSEL_VSS
  */

  if (AM_HAL_STATUS_SUCCESS != am_hal_adc_configure_slot(g_ADCHandle, 0, &ADCSlotConfig))
  {
    //am_util_stdio_printf("Error - configuring ADC Slot 0 failed.\n");
    Serial.println("Error - configuring ADC Slot 0 failed.");
  }

  // Set up an ADC slot 1
  ADCSlotConfig.eMeasToAvg = AM_HAL_ADC_SLOT_AVG_1;
  ADCSlotConfig.ePrecisionMode = AM_HAL_ADC_SLOT_14BIT;
  ADCSlotConfig.eChannel = AM_HAL_ADC_SLOT_CHSEL_SE3;  //A5
  ADCSlotConfig.bWindowCompare = false;
  ADCSlotConfig.bEnabled = true;
  if (AM_HAL_STATUS_SUCCESS != am_hal_adc_configure_slot(g_ADCHandle, 1, &ADCSlotConfig))
  {
    Serial.println("Error - configuring ADC Slot 0 failed.");
  }

  // Configure the ADC to use DMA for the sample transfer.
  adc_config_dma();
  
  //
  am_hal_adc_interrupt_enable(g_ADCHandle, AM_HAL_ADC_INT_DERR | AM_HAL_ADC_INT_DCMP );

  // Enable the ADC.
  if (AM_HAL_STATUS_SUCCESS != am_hal_adc_enable(g_ADCHandle))
  {
    Serial.println("Error - enabling ADC failed.");
  }
}


// Initialize the ADC repetitive sample timer A3.
//*****************************************************************************
void init_timerA3_for_ADC()
{
  // Start a timer to trigger the ADC periodically 
  am_hal_ctimer_config_single(3, AM_HAL_CTIMER_TIMERA,
                              AM_HAL_CTIMER_HFRC_12MHZ |
                              AM_HAL_CTIMER_FN_REPEAT |
                              AM_HAL_CTIMER_INT_ENABLE);

  am_hal_ctimer_int_enable(AM_HAL_CTIMER_INT_TIMERA3);

  am_hal_ctimer_period_set(3, AM_HAL_CTIMER_TIMERA, 10, 5); //10 tick period, 5 ticks wide

  // Enable the timer A3 to trigger the ADC directly
  am_hal_ctimer_adc_trigger_enable();

  // Start the timer.
  am_hal_ctimer_start(3, AM_HAL_CTIMER_TIMERA);
}


void setup() {
  Serial.begin(115200);
  while (!Serial) {}
  Serial.println("2 Channel Hi-speed ADC test");
  // Set the clock frequency.
  if (AM_HAL_STATUS_SUCCESS != am_hal_clkgen_control(AM_HAL_CLKGEN_CONTROL_SYSCLK_MAX, 0))
  {
    Serial.println("Error - configuring the system clock failed.");
  }

  // Set the default cache configuration and enable it.
  if (AM_HAL_STATUS_SUCCESS != am_hal_cachectrl_config(&am_hal_cachectrl_defaults))
  {
    Serial.println("Error - configuring the system cache failed.");
  }
  if (AM_HAL_STATUS_SUCCESS != am_hal_cachectrl_enable())
  {
    Serial.println("Error - enabling the system cache failed.");
  }

  // Configure the board for low power operation.
  am_bsp_low_power_init();

  // Enable only the first 512KB bank of Flash (0). Disable Flash(1)
  if (AM_HAL_STATUS_SUCCESS != am_hal_pwrctrl_memory_enable(AM_HAL_PWRCTRL_MEM_FLASH_MIN))
  {
    Serial.println("Error - configuring the flash memory failed.");
  }

  // Enable the first 32K of TCM SRAM.
  if (AM_HAL_STATUS_SUCCESS != am_hal_pwrctrl_memory_enable(AM_HAL_PWRCTRL_MEM_SRAM_32K_DTCM))
  {
    Serial.println("Error - configuring the SRAM failed.");
  }

  // Start the ITM interface.
  //am_bsp_itm_printf_enable();

  // Start the CTIMER A3 for timer-based ADC measurements.
  init_timerA3_for_ADC();

  // Enable interrupts.
  NVIC_EnableIRQ(ADC_IRQn);
  am_hal_interrupt_master_enable();

  // Set a pin to act as our ADC input
  am_hal_gpio_pinconfig(16, g_AM_PIN_16_ADCSE0); //artemis pad 16 is A4
   am_hal_gpio_pinconfig(31, g_AM_PIN_31_ADCSE3); //artemis pad 31 is A5

  // Configure the ADC
  adc_config();

  // Trigger the ADC sampling for the first time manually.
  if (AM_HAL_STATUS_SUCCESS != am_hal_adc_sw_trigger(g_ADCHandle))
  {
    Serial.println("Error - triggering the ADC failed.");
  }

  // Print the banner.
  am_util_stdio_terminal_clear();
  Serial.println("ADC Example with 1.2Msps and LPMODE=0");

  // Allow time for all printing to finish.
  am_util_delay_ms(10);

}

void loop() {
  // Go to Deep Sleep.
  useconds_refresh = micros();
  if (!g_bADCDMAComplete)
  {
    sleep();
  }

  // Check for DMA errors.
  if (g_bADCDMAError)
  {
    //am_util_stdio_printf("DMA Error occured\n");
    Serial.println("DMA Error occured");
    while (1);
  }

  // Check if the ADC DMA completion interrupt occurred.
  if (g_bADCDMAComplete)
  { 
    bool toggle = 0;
    for (int i = 0; i < ADC_SAMPLE_BUF_SIZE; i++) {
      //14 bit is 0-16383 on a range of 0-2V
      uint32_t result = g_ui32ADCSampleBuffer[i];
      uint32_t mask = 0xFFFC0;  // all ones for bits 6-19, other bits zeroed
      //Shift result depending on resolution, averaging
      result = result & mask; //get bits 6-19 data only
      result = result >> (6); //remove the fractional values

      // Serial.println(result);
      if (!toggle){
      Serial.print(result * (2.0 / 16383.0), 3);
      Serial.print(",");      
      }
      else{
        Serial.println(result * (2.0 / 16383.0), 3);
      }
      toggle = !toggle;
    }
    
    
    while (1) {}  // stop to view data


    // Reset the DMA completion and error flags.
    g_bADCDMAComplete = false;

    // Re-configure the ADC DMA.
    adc_config_dma();

    // Clear the ADC interrupts.
    if (AM_HAL_STATUS_SUCCESS != am_hal_adc_interrupt_clear(g_ADCHandle, 0xFFFFFFFF))
    {
      //am_util_stdio_printf("Error - clearing the ADC interrupts failed.\n");
      Serial.println("Error - clearing the ADC interrupts failed.");
    }

    // Trigger the ADC sampling for the first time manually.
    if (AM_HAL_STATUS_SUCCESS != am_hal_adc_sw_trigger(g_ADCHandle))
    {
      //am_util_stdio_printf("Error - triggering the ADC failed.\n");
      Serial.println("Error - triggering the ADC failed.");
    }
  } 

}

I noticed that this example no longer works. It gets to the line about enabling the first 32k of SRAM and hangs.

No errors are given.

So change this line:

  // Enable the first 32K of TCM SRAM.
  if (AM_HAL_STATUS_SUCCESS != am_hal_pwrctrl_memory_enable(AM_HAL_PWRCTRL_MEM_SRAM_32K_DTCM))
  {
    Serial.println("Error - configuring the SRAM failed.");
  }

To this and it works again:

    // Enable the first 128K of SRAM.

    if (AM_HAL_STATUS_SUCCESS != am_hal_pwrctrl_memory_enable(AM_HAL_PWRCTRL_MEM_SRAM_128K))
    {
        //am_util_stdio_printf("Error - configuring the SRAM failed.\n");
        Serial.println("Error - configuring the SRAM failed.");
    }

Hi dlp,

I have been making my way through your example code posted above on my Artemis Nano (with the most recent correction you noted in your second comment), however for some reason I am getting a Mbed OS Hard fault. I have traced it back to the function call am_bsp_low_power_init() in the code that initiates/sets the system into low power mode that seems to be causing the issue. Any ideas of suggestions as to why this might be causing the crash?

Thanks in advance!

I have created a simple API for using the DMA for high-speed sampling for the Artmis i.e. Apollo3 MCU.

You can achieve and impresive 2.66 MS/s running the ADC at 8 bits, 2 MS/s at 10 bits, 1.6 MS/s at 12 bits and 1.2 MS/s at 14 bits.

This ADC library uses a pre-defined buffer to store the ADC samples, once triggered the DMA will transfer the samples to the buffer, one can freely set the desired sample-frequency.
Due to integer division, the sampling frequency will not be guranteed. One can use a function, adc_get_true_smpl_frq… to get the true sampling frequency.

To use this.
Make a Arduino project, inside this project make a file called Apollo3_ADC_LIB.h and another called Apollo3_ADC_LIB.cpp.

Inside the project file, paste the following for an example:

#include "am_bsp.h"
#include "Apollo3_ADC_LIB.h"


#define ResolutionBits 14

#define ADC_SMPL_BUF_SIZE 256

int32_t SMPL_BUF[ADC_SMPL_BUF_SIZE];
adc_handle_t* x = adc_get_handle();


void setup() {
  // put your setup code here, to run once:
  Serial.begin(500000);
  adc_config(x, 2660000, 256, ADC_A1, OSR_1, ADC_14BIT);
  adc_setup(x, SMPL_BUF);
  delay(500);
}

void loop() {
  // put your main code here, to run repeatedly:
 if(adc_smpl_status(x) == 1) {
    adc_transfer_data(x, SMPL_BUF);
    adc_clear_status(x);
    for(uint16_t i = 0; i < 256; i++) {
      // int32_t result = SMPL_BUF[i];
      // result >>= 6; //bitshift due to the average in the register being of the format 14.6.
      // Serial.println(result*2.0/16383.0);
      Serial.println(SMPL_BUF[i]);
    }
    delay(1000);
    adc_software_trigger(x, SMPL_BUF);
 }
} 

Inside the .h file, paste the following:

#ifndef APOLLO3_ADC_LIB_H
#define APOLLO3_ADC_LIB_H

#include <Arduino.h>
#include "am_bsp.h"

#ifdef __cplusplus
extern "C" {
#endif

typedef enum {
  ADC_A0 = AM_HAL_ADC_SLOT_CHSEL_SE1,
  ADC_A1 = AM_HAL_ADC_SLOT_CHSEL_SE2,
  ADC_A2 = AM_HAL_ADC_SLOT_CHSEL_SE6,
  ADC_A3 = AM_HAL_ADC_SLOT_CHSEL_SE5,
  ADC_A4 = AM_HAL_ADC_SLOT_CHSEL_SE0,
  ADC_A5 = AM_HAL_ADC_SLOT_CHSEL_SE3
}adc_pin_t;

typedef enum {
  OSR_1 = AM_HAL_ADC_SLOT_AVG_1,
  OSR_2 = AM_HAL_ADC_SLOT_AVG_2,
  OSR_4 = AM_HAL_ADC_SLOT_AVG_4,
  OSR_8 = AM_HAL_ADC_SLOT_AVG_8,
  OSR_16 = AM_HAL_ADC_SLOT_AVG_16,
  OSR_32 = AM_HAL_ADC_SLOT_AVG_32,
  OSR_64 = AM_HAL_ADC_SLOT_AVG_64,
  OSR_128 = AM_HAL_ADC_SLOT_AVG_128
}osr_t;

typedef enum {
  ADC_8BIT = AM_HAL_ADC_SLOT_8BIT,
  ADC_10BIT = AM_HAL_ADC_SLOT_10BIT,
  ADC_12BIT = AM_HAL_ADC_SLOT_12BIT,
  ADC_14BIT = AM_HAL_ADC_SLOT_14BIT
}adc_resolution_bits_t;

typedef struct adc_handle_t adc_handle_t;

adc_handle_t* adc_get_handle(void);
int8_t adc_setup(struct adc_handle_t *handle, int32_t *smpl_buffer);
int8_t adc_software_trigger(struct adc_handle_t *handle, int32_t *smpl_buffer);
int8_t adc_smpl_status(struct adc_handle_t *handle);
int8_t adc_config(struct adc_handle_t *handle, uint32_t smpl_frq, uint32_t smpl_size, adc_pin_t pin, osr_t osr, adc_resolution_bits_t resolution);
int8_t adc_clear_status(struct adc_handle_t *handle);
int8_t adc_transfer_data(struct adc_handle_t *handle, int32_t *smpl_buffer);
int8_t adc_get_true_smpl_frq(struct adc_handle_t *handle, float *true_smpl_frq);

#ifdef __cplusplus
}
#endif

#endif

Inside the .cpp file paste:

#include "am_util_delay.h"
#include "am_util_stdio.h"
#include "am_hal_gpio.h"
#include "am_hal_interrupt.h"
#include "am_hal_adc.h"
#include <Arduino.h>
#include "am_bsp.h"
#include "Apollo3_ADC_LIB.h"


typedef struct adc_handle_t {
  struct cfg{
    struct adc_handle_t *selfAddr;
    void *hal_handle;
    volatile bool adc_dma_cmplt;
    volatile bool adc_dma_error;
    bool smpl_cmplt;
    am_hal_gpio_pincfg_t hal_adc_pin;
    uint32_t smpl_frq;
    float true_smpl_frq;
    osr_t osr_ratio;
    uint16_t smpl_size;
    int32_t dma_target_addr;
    adc_resolution_bits_t adc_resolution;
    adc_pin_t input_pin;
    int8_t (*get_timer_setting)(uint32_t, uint32_t*, uint32_t*, float*);
  }cfg;
  int8_t (*trig_adc)(void);
}adc_handle_t;



int8_t adc_cfg_dma(struct adc_handle_t *handle, int32_t *smpl_buffer);
int8_t adc_cfg(struct adc_handle_t *handle, int32_t *smpl_buffer);
int8_t get_timer_setting(struct adc_handle_t *handle, uint32_t smpl_frq, uint32_t *period, uint32_t *pulse, float *true_smpl_frq);
int8_t init_timer_A3_adc(struct adc_handle_t *hanlde);
void get_artemis_adc_pin(adc_pin_t pin, uint32_t *uFunc_pin, uint32_t *pad_sel);


static adc_handle_t adc_handler;



adc_handle_t* adc_get_handle(void){
  return &adc_handler;
}





extern "C" void am_adc_isr() {
  uint32_t ui32intMask;
  am_hal_adc_interrupt_status(adc_handler.cfg.hal_handle, &ui32intMask, 0);
  am_hal_adc_interrupt_clear(adc_handler.cfg.hal_handle, ui32intMask);
  if(ui32intMask & AM_HAL_ADC_INT_DCMP) {
    adc_handler.cfg.adc_dma_cmplt = 1;
  }
  if(ui32intMask & AM_HAL_ADC_INT_DERR) {
    adc_handler.cfg.adc_dma_error = 1;
  }
}

int8_t adc_config(struct adc_handle_t *handle, uint32_t smpl_frq, uint32_t smpl_size, adc_pin_t pin, osr_t osr, adc_resolution_bits_t resolution) {
  int8_t r = 0;
  if(handle != NULL) {
  handle->cfg.selfAddr = handle;
  handle->cfg.smpl_frq = smpl_frq;
  handle->cfg.smpl_size = smpl_size;
  handle->cfg.input_pin = pin;
  handle->cfg.osr_ratio = osr;
  handle->cfg.adc_resolution = resolution;
  } else r = -1;
  return r;
}

int8_t adc_transfer_data(struct adc_handle_t *handle, int32_t *smpl_buffer){
  int8_t r = 0;
  if(handle != NULL) {
    for(uint32_t i = 0; i < handle->cfg.smpl_size; i++) {
      smpl_buffer[i] >>= 6;
    }
  } else r = -1;
  return r;
}

int8_t adc_get_true_smpl_frq(struct adc_handle_t *handle, float *true_smpl_frq) {
  int8_t r = 0;
  if(handle != NULL) {
    *true_smpl_frq = handle->cfg.true_smpl_frq;
  } else r = -1;
  return r;
}

int8_t adc_smpl_status(struct adc_handle_t *handle){
  int8_t r = 0;
  if(handle != NULL) {
    if(handle -> cfg.adc_dma_cmplt) {
      r = 1;
    }
    if(handle -> cfg.adc_dma_error) {
      r = -2;
    }
  } else r = -1;
  return r;
}

int8_t adc_clear_status(struct adc_handle_t *handle) {
  int8_t r = 0;
  if(handle != NULL) {
    handle -> cfg.adc_dma_cmplt = 0;
    handle -> cfg.adc_dma_error = 0;
  } else r = -1;
  return r;
}

int8_t adc_cfg_dma(struct adc_handle_t *handle, int32_t *smpl_buffer){
  int8_t r = 0;
  if(handle != NULL) {
    am_hal_adc_dma_config_t adc_dma_cfg;

    adc_dma_cfg.bDynamicPriority = 1;
    adc_dma_cfg.ePriority = AM_HAL_ADC_PRIOR_SERVICE_IMMED;
    adc_dma_cfg.bDMAEnable = 1;
    adc_dma_cfg.ui32SampleCount = handle -> cfg.smpl_size;
    adc_dma_cfg.ui32TargetAddress = (int32_t)smpl_buffer;

    am_hal_adc_configure_dma(handle->cfg.hal_handle, &adc_dma_cfg);

    handle->cfg.adc_dma_cmplt = 0;
    handle->cfg.adc_dma_error = 0;
  } else r = -1;
  return r;
}

int8_t adc_cfg(struct adc_handle_t *handle, int32_t *smpl_buffer) {
  int8_t r = 0;
  if(handle != NULL) {
    am_hal_adc_config_t adc_cfg;
    am_hal_adc_slot_config_t adc_slot_cfg;

    am_hal_adc_initialize(0, &(handle->cfg.hal_handle));
    am_hal_adc_power_control(handle->cfg.hal_handle, AM_HAL_SYSCTRL_WAKE, 0);

    adc_cfg.eClock = AM_HAL_ADC_CLKSEL_HFRC;
    adc_cfg.ePolarity = AM_HAL_ADC_TRIGPOL_RISING;
    adc_cfg.eTrigger = AM_HAL_ADC_TRIGSEL_SOFTWARE;
    adc_cfg.eReference = AM_HAL_ADC_REFSEL_INT_2P0;
    adc_cfg.eClockMode = AM_HAL_ADC_CLKMODE_LOW_LATENCY;
    adc_cfg.ePowerMode = AM_HAL_ADC_LPMODE0;
    adc_cfg.eRepeat = AM_HAL_ADC_REPEATING_SCAN;

    am_hal_adc_configure(handle->cfg.hal_handle, &adc_cfg);
    

    adc_slot_cfg.eMeasToAvg = (am_hal_adc_meas_avg_e)(handle -> cfg.osr_ratio);
    adc_slot_cfg.ePrecisionMode = (am_hal_adc_slot_prec_e)(handle -> cfg.adc_resolution);
    adc_slot_cfg.eChannel = (am_hal_adc_slot_chan_e)(handle -> cfg.input_pin);
    adc_slot_cfg.bWindowCompare = 0;
    adc_slot_cfg.bEnabled = 1;

    am_hal_adc_configure_slot(handle->cfg.hal_handle, 0, &adc_slot_cfg);

    adc_cfg_dma(handle, smpl_buffer);
    am_hal_adc_interrupt_enable(handle->cfg.hal_handle, AM_HAL_ADC_INT_DERR | AM_HAL_ADC_INT_DCMP);
    am_hal_adc_enable(handle->cfg.hal_handle);    
  } else r = -1;
  return r;
}

int8_t get_timer_setting(struct adc_handle_t *handle, uint32_t smpl_frq, uint32_t *period, uint32_t *pulse, float *true_smpl_frq) {
  int8_t r = 0;
  if(handle != NULL) {
    uint32_t max_frq = 1200000;
    adc_resolution_bits_t adc_res = handle->cfg.adc_resolution;
    switch(adc_res) {
      case(ADC_8BIT):
        max_frq = 2400000;
        break;
      case(ADC_10BIT):
        max_frq = 2000000;
        break;
      case(ADC_12BIT):
        max_frq = 1500000;
        break;
      case(ADC_14BIT):
        max_frq = 1200000;
        break;
    }
    if(smpl_frq > max_frq) {
      smpl_frq = max_frq;
    }
    uint32_t k = ((uint32_t)(12000000.0/((float)smpl_frq)));
    *period = (k-1);
    *pulse = (uint32_t)(k/2.0);
    *true_smpl_frq = 12000000.0/((float)k);
  } else r = -1;
  return r;
}

int8_t init_timer_A3_adc(struct adc_handle_t *handle) {
  int8_t r = 0;
  if(handle != NULL) {
    uint32_t period = 0;
    uint32_t pulse = 0;

    get_timer_setting(handle,handle -> cfg.smpl_frq, &period, &pulse, &(handle->cfg.true_smpl_frq));

    am_hal_ctimer_config_single(3, AM_HAL_CTIMER_TIMERA,
    AM_HAL_CTIMER_HFRC_12MHZ | AM_HAL_CTIMER_FN_REPEAT | AM_HAL_CTIMER_INT_ENABLE);
    am_hal_ctimer_int_enable(AM_HAL_CTIMER_INT_TIMERA3);
    am_hal_ctimer_period_set(3, AM_HAL_CTIMER_TIMERA, period, pulse);
    am_hal_ctimer_adc_trigger_enable();
    am_hal_ctimer_start(3, AM_HAL_CTIMER_TIMERA);
  } else r = -1;
  return r;
}


void get_artemis_adc_pin(adc_pin_t pin, uint32_t *uFunc_pin, uint32_t *pad_sel) {
  uint32_t sel_pin = 0;
  uint32_t sel_pad = 0;
  switch(pin) {
    case(ADC_A0):
      sel_pin = AM_HAL_PIN_29_ADCSE1;
      sel_pad = 29;
      break;
    case(ADC_A1):
      sel_pin = AM_HAL_PIN_11_ADCSE2;
      sel_pad = 11;
      break;
    case(ADC_A2):
      sel_pin = AM_HAL_PIN_34_ADCSE6;
      sel_pad = 34;
      break;
    case(ADC_A3):
      sel_pin = AM_HAL_PIN_33_ADCSE5;
      sel_pad = 33;
      break;
    case(ADC_A4):
      sel_pin = AM_HAL_PIN_16_ADCSE0;
      sel_pad = 16;
      break;
    case(ADC_A5):
      sel_pin = AM_HAL_PIN_31_ADCSE3;
      sel_pad = 31;
      break;
  }
  *uFunc_pin = sel_pin;
  *pad_sel = sel_pad;
}


int8_t adc_setup(struct adc_handle_t *handle, int32_t *smpl_buffer){
  int8_t r = 0;
  if(handle != NULL) {
    uint32_t pin_cfg;
    uint32_t pad_cfg;
    get_artemis_adc_pin(handle->cfg.input_pin, &pin_cfg, &pad_cfg);
    handle->cfg.hal_adc_pin = {.uFuncSel = pin_cfg,};
    
    am_bsp_itm_printf_enable();
    init_timer_A3_adc(handle);
    NVIC_EnableIRQ(ADC_IRQn);
    am_hal_interrupt_master_enable();
    am_hal_gpio_pinconfig(pad_cfg, handle->cfg.hal_adc_pin);

    adc_cfg(handle, smpl_buffer);

    am_hal_adc_sw_trigger(handle->cfg.hal_handle);
    am_util_stdio_terminal_clear();
    am_util_delay_ms(10);
    
  } else r = -1;
  return r;
}

int8_t adc_software_trigger(struct adc_handle_t *handle, int32_t *smpl_buffer){
  int8_t r = 0;
  if(handle != NULL) {
    handle -> cfg.smpl_cmplt = 0;
    handle -> cfg.adc_dma_cmplt = 0;

    adc_cfg_dma(handle, smpl_buffer);

    am_hal_adc_interrupt_clear(handle->cfg.hal_handle, 0XFFFFFFFF);
    am_hal_adc_sw_trigger(handle->cfg.hal_handle);
  } else r = -1;
  return r;
}

Very cool! Thanks for sharing your hard work

I am creating an FFT library using the core’s DSP instructions. Let me know if this would be of interest to you as well.

Sure! We welcome any useful contributions - posting them here makes them searchable/findable via google and such :slight_smile: