How can i combine these two codes? I am getting an "expected unqualifier error" and need to run them both simultaneously

#include<TimerOne.h>

int signal1 = {23, 25, 27};

int signal2 = {46, 48, 50};

int signal3 = {47, 49, 51};

int signal4 = {36, 38, 40};

int redDelay = 2000;

int yellowDelay = 1000;

volatile int triggerpin1 = 31;

volatile int echopin1 = 29;

volatile int triggerpin2 = 44;

volatile int echopin2 = 42;

volatile int triggerpin3 = 41;

volatile int echopin3 = 43;

volatile int triggerpin4 = 34;

volatile int echopin4 = 32;

volatile long time; // Variable for storing the time traveled

volatile int S1, S2, S3, S4; // Variables for storing the distance covered

int t = 5; // distance under which it will look for vehicles.

void setup(){

Serial.begin(115200);

Timer1.initialize(100000); //Begin using the timer. This function must be called first. “microseconds” is the period of time the timer takes.

Timer1.attachInterrupt(softInterr); //Run a function each time the timer period finishes.

// Declaring LED pins as output

for(int i=0; i<3; i++){

pinMode(signal1*, OUTPUT);*
pinMode(signal2, OUTPUT);
pinMode(signal3, OUTPUT);
pinMode(signal4, OUTPUT);
}
// Declaring ultrasonic sensor pins as output
pinMode(triggerpin1, OUTPUT);
pinMode(echopin1, INPUT);
pinMode(triggerpin2, OUTPUT);
pinMode(echopin2, INPUT);
pinMode(triggerpin3, OUTPUT);
pinMode(echopin3, INPUT);
pinMode(triggerpin4, OUTPUT);
pinMode(echopin4, INPUT);
}
void loop()
{
// If there are vehicles at signal 1
if(S1<t)
{
signal1Function();
}
// If there are vehicles at signal 2
if(S2<t)
{
signal2Function();
}
// If there are vehicles at signal 3
if(S3<t)
{
signal3Function();
}
// If there are vehicles at signal 4
if(S4<t)
{
signal4Function();
}
}
// This is interrupt function and it will run each time the timer period finishes. The timer period is set at 100 milli seconds.
void softInterr()
{
// Reading from first ultrasonic sensor
digitalWrite(triggerpin1, LOW);
delayMicroseconds(2);
digitalWrite(triggerpin1, HIGH);
delayMicroseconds(10);
digitalWrite(triggerpin1, LOW);
time = pulseIn(echopin1, HIGH);
S1= time*0.034/2;
// Reading from second ultrasonic sensor
digitalWrite(triggerpin2, LOW);
delayMicroseconds(2);
digitalWrite(triggerpin2, HIGH);
delayMicroseconds(10);
digitalWrite(triggerpin2, LOW);
time = pulseIn(echopin2, HIGH);
S2= time*0.034/2;
// Reading from third ultrasonic sensor
digitalWrite(triggerpin3, LOW);
delayMicroseconds(2);
digitalWrite(triggerpin3, HIGH);
delayMicroseconds(10);
digitalWrite(triggerpin3, LOW);
time = pulseIn(echopin3, HIGH);
S3= time*0.034/2;
// Reading from fourth ultrasonic sensor
digitalWrite(triggerpin4, LOW);
delayMicroseconds(2);
digitalWrite(triggerpin4, HIGH);
delayMicroseconds(10);
digitalWrite(triggerpin4, LOW);
time = pulseIn(echopin4, HIGH);
S4= time*0.034/2;
// Print distance values on serial monitor for debugging
Serial.print("S1: ");
Serial.print(S1);
Serial.print(" S2: ");
Serial.print(S2);
Serial.print(" S3: ");
Serial.print(S3);
Serial.print(" S4: ");
Serial.println(S4);
}
void signal1Function()
{
Serial.println(“1”);
low();
// Make RED LED LOW and make Green HIGH for 5 seconds
digitalWrite(signal1[0], LOW);
digitalWrite(signal1[2], HIGH);
delay(redDelay);
// if there are vehicels at other signals
if(S2<t || S3<t || S4<t)
{
// Make Green LED LOW and make yellow LED HIGH for 2 seconds
digitalWrite(signal1[2], LOW);
digitalWrite(signal1[1], HIGH);
delay(yellowDelay);
}
}
void signal2Function()
{
Serial.println(“2”);
low();
digitalWrite(signal2[0], LOW);
digitalWrite(signal2[2], HIGH);
delay(redDelay);

if(S1<t || S3<t || S4<t)
{
digitalWrite(signal2[2], LOW);
digitalWrite(signal2[1], HIGH);
delay(yellowDelay);
}
}
void signal3Function()
{
Serial.println(“3”);
low();
digitalWrite(signal3[0], LOW);
digitalWrite(signal3[2], HIGH);
delay(redDelay);
if(S1<t || S2<t || S4<t)
{
digitalWrite(signal3[2], LOW);
digitalWrite(signal3[1], HIGH);
delay(yellowDelay);
}
}
void signal4Function()
{
Serial.println(“4”);
low();
digitalWrite(signal4[0], LOW);
digitalWrite(signal4[2], HIGH);
delay(redDelay);
if(S1<t || S2<t || S3<t)
{
digitalWrite(signal4[2], LOW);
digitalWrite(signal4[1], HIGH);
delay(yellowDelay);
}
}
// Function to make all LED’s LOW except RED one’s.
void low()
{
for(int i=1; i<3; i++)
{
digitalWrite(signal1, LOW);
digitalWrite(signal2, LOW);
digitalWrite(signal3, LOW);
digitalWrite(signal4, LOW);
}
for(int i=0; i<1; i++)
{
digitalWrite(signal1, HIGH);
digitalWrite(signal2, HIGH);
digitalWrite(signal3*, HIGH);*
digitalWrite(signal4*, HIGH);*
}
}
int pir=7;
unsigned long startFlag;
unsigned long startTime;
unsigned long previousTime;
unsigned long duration=10000;
unsigned long times;
unsigned long sec;
long unsigned int lowIn;
long unsigned int pause = 5000;
boolean lockLow = true;
boolean takeLowTime;
int pin;
int i;
int led1= 14;
int led2=15;
int led3=16;
int pled1=17;
int pled2=11;
//button
const int buttonPin = 18; // the number of the pushbutton pin
// the number of the LED pin
// Variables will change:
int ledState = LOW; // the current state of the output pin
int buttonState; // the current reading from the input pin
int lastButtonState = HIGH; // the previous reading from the input pin
// the following variables are long’s because the time, measured in miliseconds,
// will quickly become a bigger number than can be stored in an int.
long lastDebounceTime = 0; // the last time the output pin was toggled
long debounceDelay = 50;
//display
int pin1 = 8;
int pin2 = 13; // --6–
int pin3 = 2; // 5 | | 7
int pin4 = 3; // |–4–|
int pin5 = 4; // 1 | | 3
int pin6 = 5; // --2–
int pin7 = 6;
int gnd1 = 10; // gnd1 is display 1’s gnd
int gnd2 = 9; // gnd2 is display 2’s gnd
int timer = 50; // A timer, to run the for loop 10 times, which turns out as 1 second.
int value;
int calibrationTime = 10; // The value, part of the FADING display
int stat;
int rumple=0;
//int led = 12;
int ledPin = 12;
void setup() {
// put your setup code here, to run once:
pinMode(pir, INPUT);
Serial.begin(9600);
//pinMode(ledPin, OUTPUT);
//pinMode(led, OUTPUT);
pinMode(buttonPin, INPUT);
pinMode(led1, OUTPUT);
pinMode(led2, OUTPUT);
pinMode(led3, OUTPUT);
pinMode(ledPin, OUTPUT);
pinMode(pled1, OUTPUT);
pinMode(pled2, OUTPUT);
// display
pinMode(pin1, OUTPUT);
pinMode(pin2, OUTPUT);
pinMode(pin3, OUTPUT);
pinMode(pin4, OUTPUT); //The following sets up all of the pins for use.
pinMode(pin5, OUTPUT);
pinMode(pin6, OUTPUT);
pinMode(pin7, OUTPUT);
pinMode(gnd1, OUTPUT);
pinMode(gnd2, OUTPUT);
digitalWrite(pir, LOW);
Serial.print("calibrating sensor ");
for(int i = 0; i < calibrationTime; i++){
Serial.print(“.”);
delay(1000);
}
Serial.println(" done");
Serial.println(“SENSOR ACTIVE”);
delay(50);
digitalWrite(led1,HIGH);
digitalWrite(pled1, LOW);
digitalWrite(pled2, HIGH);

}
void loop()
{
int reading = digitalRead(buttonPin);
// check to see if you just pressed the button
// (i.e. the input went from LOW to HIGH), and you’ve waited
// long enough since the last press to ignore any noise:
// If the switch changed, due to noise or pressing:
if (reading != lastButtonState) {
// reset the debouncing timer
lastDebounceTime = millis();
}
if ((millis() - lastDebounceTime) > debounceDelay) {
// whatever the reading is at, it’s been there for longer
// than the debounce delay, so take it as the actual current state:
// if the button state has changed:
if (reading != buttonState) {
buttonState = reading;
// only toggle the LED if the new button state is HIGH
if (buttonState == HIGH) {
ledState = !ledState;
//Serial.println(ledState);
}
}
}
// set the LED:

// save the reading. Next time through the loop,
// it’ll be the lastButtonState:
lastButtonState = reading;

if (((digitalRead(pir) == HIGH)||(ledState == HIGH)) && (startFlag == 0)){ // start new time sequence
digitalWrite(ledPin, HIGH);
if(lockLow){
lockLow = false;
}
takeLowTime = true;
startFlag = 1;
startTime = millis();
previousTime = startTime;
}
if((ledState == HIGH))
{
digitalWrite(ledPin, HIGH);
delay(2000);
startFlag = 0;
ledState = LOW;
goto a;
digitalWrite(ledPin, LOW);
}
if ( (startFlag ==1) && ((millis() - previousTime) >= duration) ) { // duration = 100, sample 10 times a second
previousTime = previousTime + duration;
Serial.println(buttonState);
if ((millis() - startTime )<=5000){ // still waiting it out
if (digitalRead(pir) == LOW ){
// pin went low
startFlag = 0;
digitalWrite(ledPin, LOW);
}
}
if ((millis() - startTime) >15000){
if (digitalRead(pir) == LOW){
// pin went low
startFlag = 0;
digitalWrite(ledPin, LOW);
}
else{ // made it!
rumple = 1;
digitalWrite(ledPin, HIGH);

startFlag = 0;
}
if(rumple == 1)
{
a:
//digitalWrite(led, HIGH);
digitalWrite(led1, LOW);

digitalWrite(ledPin, LOW);
sec = millis();
Serial.println(sec);
delay(250);
digitalWrite(led2, HIGH);
delay(3000);
digitalWrite(led2, LOW);
delay(300);
digitalWrite(led2, HIGH);
delay(800);
digitalWrite(led2, LOW);
delay(200);
digitalWrite(led2, HIGH);
delay(800);
digitalWrite(led2, LOW);
delay(200);
digitalWrite(led2, HIGH);
delay(800);
digitalWrite(led2, LOW);
delay(1000);
digitalWrite(led2, LOW);
digitalWrite(led3, HIGH);
delay(2500);
digitalWrite(pled1, HIGH);
digitalWrite(pled2, LOW);
for (int i=0; i<timer; i++){ // The for loop, for running the program 10 times.
digitalWrite(pin1, B1);
digitalWrite(pin2, B1);
digitalWrite(pin3, B0);
digitalWrite(pin4, B1);
digitalWrite(pin5, B0);
digitalWrite(pin6, B1);
digitalWrite(pin7, B1);
digitalWrite(gnd1, B0);
digitalWrite(gnd2, B1);
delay(10); // Writes 20 to the display.
digitalWrite(pin1, B1);
digitalWrite(pin2, B1);
digitalWrite(pin3, B1);
digitalWrite(pin4, B0);
digitalWrite(pin5, B1);
digitalWrite(pin6, B1);
digitalWrite(pin7, B1);
digitalWrite(gnd1, B1);
digitalWrite(gnd2, B0);
delay(10);

}

for (int i=0; i<timer; i++){
digitalWrite(pin1, B0);
digitalWrite(pin2, B0);
digitalWrite(pin3, B1);
digitalWrite(pin4, B0);
digitalWrite(pin5, B0);
digitalWrite(pin6, B0);
digitalWrite(pin7, B1);
digitalWrite(gnd1, B0);
digitalWrite(gnd2, B1);
delay(10); // Writes 19 to the display.
digitalWrite(pin1, B0);
digitalWrite(pin2, B0);
digitalWrite(pin3, B1);
digitalWrite(pin4, B1);
digitalWrite(pin5, B1);
digitalWrite(pin6, B1);
digitalWrite(pin7, B1);
digitalWrite(gnd1, B1);
digitalWrite(gnd2, B0);
delay(10);

}
for (int i=0; i<timer; i++){
digitalWrite(pin1, B0);
digitalWrite(pin2, B0);
digitalWrite(pin3, B1);
digitalWrite(pin4, B0);
digitalWrite(pin5, B0);
digitalWrite(pin6, B0);
digitalWrite(pin7, B1);
digitalWrite(gnd1, B0);
digitalWrite(gnd2, B1);
delay(10); // Writes 18 to the display.
digitalWrite(pin1, B1);
digitalWrite(pin2, B1);
digitalWrite(pin3, B1);
digitalWrite(pin4, B1);
digitalWrite(pin5, B1);
digitalWrite(pin6, B1);
digitalWrite(pin7, B1);
digitalWrite(gnd1, B1);
digitalWrite(gnd2, B0);
delay(10);

}
for (int i=0; i<timer; i++){
digitalWrite(pin1, B0);
digitalWrite(pin2, B0);
digitalWrite(pin3, B1);
digitalWrite(pin4, B0);
digitalWrite(pin5, B0);
digitalWrite(pin6, B0);
digitalWrite(pin7, B1);
digitalWrite(gnd1, B0);
digitalWrite(gnd2, B1);
delay(10); // Writes 17 to the display.
digitalWrite(pin1, B0);
digitalWrite(pin2, B0);
digitalWrite(pin3, B1);
digitalWrite(pin4, B0);
digitalWrite(pin5, B0);
digitalWrite(pin6, B1);
digitalWrite(pin7, B1);
digitalWrite(gnd1, B1);
digitalWrite(gnd2, B0);
delay(10);

}
for (int i=0; i<timer; i++){
digitalWrite(pin1, B0);
digitalWrite(pin2, B0);
digitalWrite(pin3, B1);
digitalWrite(pin4, B0);
digitalWrite(pin5, B0);
digitalWrite(pin6, B0);
digitalWrite(pin7, B1);
digitalWrite(gnd1, B0);
digitalWrite(gnd2, B1);
delay(10); // Writes 16 to the display.
digitalWrite(pin1, B1);
digitalWrite(pin2, B1);
digitalWrite(pin3, B1);
digitalWrite(pin4, B1);
digitalWrite(pin5, B1);
digitalWrite(pin6, B1);
digitalWrite(pin7, B0);
digitalWrite(gnd1, B1);
digitalWrite(gnd2, B0);
delay(10);

}
for (int i=0; i<timer; i++){
digitalWrite(pin1, B0);
digitalWrite(pin2, B0);
digitalWrite(pin3, B1);
digitalWrite(pin4, B0);
digitalWrite(pin5, B0);
digitalWrite(pin6, B0);
digitalWrite(pin7, B1);
digitalWrite(gnd1, B0);
digitalWrite(gnd2, B1);
delay(10); // Writes 15 to the display.
digitalWrite(pin1, B0);
digitalWrite(pin2, B1);
digitalWrite(pin3, B1);
digitalWrite(pin4, B1);
digitalWrite(pin5, B1);
digitalWrite(pin6, B1);
digitalWrite(pin7, B0);
digitalWrite(gnd1, B1);
digitalWrite(gnd2, B0);
delay(10);

}
for (int i=0; i<timer; i++){
digitalWrite(pin1, B0);
digitalWrite(pin2, B0);
digitalWrite(pin3, B1);
digitalWrite(pin4, B0);
digitalWrite(pin5, B0);
digitalWrite(pin6, B0);
digitalWrite(pin7, B1);
digitalWrite(gnd1, B0);
digitalWrite(gnd2, B1);
delay(10); // Writes 14 to the display.
digitalWrite(pin1, B0);
digitalWrite(pin2, B0);
digitalWrite(pin3, B1);
digitalWrite(pin4, B1);
digitalWrite(pin5, B1);
digitalWrite(pin6, B0);
digitalWrite(pin7, B1);
digitalWrite(gnd1, B1);
digitalWrite(gnd2, B0);
delay(10);

}
for (int i=0; i<timer; i++){
digitalWrite(pin1, B0);
digitalWrite(pin2, B0);
digitalWrite(pin3, B1);
digitalWrite(pin4, B0);
digitalWrite(pin5, B0);
digitalWrite(pin6, B0);
digitalWrite(pin7, B1);
digitalWrite(gnd1, B0);
digitalWrite(gnd2, B1);
delay(10); // Writes 13 to the display.
digitalWrite(pin1, B0);
digitalWrite(pin2, B1);
digitalWrite(pin3, B1);
digitalWrite(pin4, B1);
digitalWrite(pin5, B0);
digitalWrite(pin6, B1);
digitalWrite(pin7, B1);
digitalWrite(gnd1, B1);
digitalWrite(gnd2, B0);
delay(10);

}
for (int i=0; i<timer; i++){
digitalWrite(pin1, B0);
digitalWrite(pin2, B0);
digitalWrite(pin3, B1);
digitalWrite(pin4, B0);
digitalWrite(pin5, B0);
digitalWrite(pin6, B0);
digitalWrite(pin7, B1);
digitalWrite(gnd1, B0);
digitalWrite(gnd2, B1);
delay(10); // Writes 12 to the display.
digitalWrite(pin1, B1);
digitalWrite(pin2, B1);
digitalWrite(pin3, B0);
digitalWrite(pin4, B1);
digitalWrite(pin5, B0);
digitalWrite(pin6, B1);
digitalWrite(pin7, B1);
digitalWrite(gnd1, B1);
digitalWrite(gnd2, B0);
delay(10);

}
for (int i=0; i<timer; i++){
digitalWrite(pin1, B0);
digitalWrite(pin2, B0);
digitalWrite(pin3, B1);
digitalWrite(pin4, B0);
digitalWrite(pin5, B0);
digitalWrite(pin6, B0);
digitalWrite(pin7, B1);
digitalWrite(gnd1, B0);
digitalWrite(gnd2, B1);
delay(10); // Writes 11 to the display.
digitalWrite(pin1, B0);
digitalWrite(pin2, B0);
digitalWrite(pin3, B1);
digitalWrite(pin4, B0);
digitalWrite(pin5, B0);
digitalWrite(pin6, B0);
digitalWrite(pin7, B1);
digitalWrite(gnd1, B1);
digitalWrite(gnd2, B0);
delay(10);

}
for (int i=0; i<timer; i++){
digitalWrite(pin1, B0);
digitalWrite(pin2, B0);
digitalWrite(pin3, B1);
digitalWrite(pin4, B0);
digitalWrite(pin5, B0);
digitalWrite(pin6, B0);
digitalWrite(pin7, B1);
digitalWrite(gnd1, B0);
digitalWrite(gnd2, B1);
delay(10); // Writes 10 to the display.
digitalWrite(pin1, B1);
digitalWrite(pin2, B1);
digitalWrite(pin3, B1);
digitalWrite(pin4, B0);
digitalWrite(pin5, B1);
digitalWrite(pin6, B1);
digitalWrite(pin7, B1);
digitalWrite(gnd1, B1);
digitalWrite(gnd2, B0);
delay(10);

}
for (int i=0; i<timer; i++){
digitalWrite(pin1, B1);
digitalWrite(pin2, B1);
digitalWrite(pin3, B1);
digitalWrite(pin4, B0);
digitalWrite(pin5, B1);
digitalWrite(pin6, B1);
digitalWrite(pin7, B1);
digitalWrite(gnd1, B0);
digitalWrite(gnd2, B1);
delay(10); // Writes 09 to the display.
digitalWrite(pin1, B0);
digitalWrite(pin2, B0);
digitalWrite(pin3, B1);
digitalWrite(pin4, B1);
digitalWrite(pin5, B1);
digitalWrite(pin6, B1);
digitalWrite(pin7, B1);
digitalWrite(gnd1, B1);
digitalWrite(gnd2, B0);
delay(10);

}

for (int i=0; i<timer; i++){
digitalWrite(pin1, B1);
digitalWrite(pin2, B1);
digitalWrite(pin3, B1);
digitalWrite(pin4, B0);
digitalWrite(pin5, B1);
digitalWrite(pin6, B1);
digitalWrite(pin7, B1);
digitalWrite(gnd1, B0);
digitalWrite(gnd2, B1);
delay(10); // Writes 08 to the display.
digitalWrite(pin1, B1);
digitalWrite(pin2, B1);
digitalWrite(pin3, B1);
digitalWrite(pin4, B1);
digitalWrite(pin5, B1);
digitalWrite(pin6, B1);
digitalWrite(pin7, B1);
digitalWrite(gnd1, B1);
digitalWrite(gnd2, B0);
delay(10);

}
for (int i=0; i<timer; i++){
digitalWrite(pin1, B1);
digitalWrite(pin2, B1);
digitalWrite(pin3, B1);
digitalWrite(pin4, B0);
digitalWrite(pin5, B1);
digitalWrite(pin6, B1);
digitalWrite(pin7, B1);
digitalWrite(gnd1, B0);
digitalWrite(gnd2, B1);
delay(10); // Writes 07 to the display.
digitalWrite(pin1, B0);
digitalWrite(pin2, B0);
digitalWrite(pin3, B1);
digitalWrite(pin4, B0);
digitalWrite(pin5, B0);
digitalWrite(pin6, B1);
digitalWrite(pin7, B1);
digitalWrite(gnd1, B1);
digitalWrite(gnd2, B0);
delay(10);

}
for (int i=0; i<timer; i++){
digitalWrite(pin1, B1);
digitalWrite(pin2, B1);
digitalWrite(pin3, B1);
digitalWrite(pin4, B0);
digitalWrite(pin5, B1);
digitalWrite(pin6, B1);
digitalWrite(pin7, B1);
digitalWrite(gnd1, B0);
digitalWrite(gnd2, B1);
delay(10); // Writes 06 to the display.
digitalWrite(pin1, B1);
digitalWrite(pin2, B1);
digitalWrite(pin3, B1);
digitalWrite(pin4, B1);
digitalWrite(pin5, B1);
digitalWrite(pin6, B1);
digitalWrite(pin7, B0);
digitalWrite(gnd1, B1);
digitalWrite(gnd2, B0);
delay(10);

}
for (int i=0; i<timer; i++){
digitalWrite(pin1, B1);
digitalWrite(pin2, B1);
digitalWrite(pin3, B1);
digitalWrite(pin4, B0);
digitalWrite(pin5, B1);
digitalWrite(pin6, B1);
digitalWrite(pin7, B1);
digitalWrite(gnd1, B0);
digitalWrite(gnd2, B1);
delay(10); // Writes 05 to the display.
digitalWrite(pin1, B0);
digitalWrite(pin2, B1);
digitalWrite(pin3, B1);
digitalWrite(pin4, B1);
digitalWrite(pin5, B1);
digitalWrite(pin6, B1);
digitalWrite(pin7, B0);
digitalWrite(gnd1, B1);
digitalWrite(gnd2, B0);
delay(10);

}
for (int i=0; i<timer; i++){
digitalWrite(pin1, B1);
digitalWrite(pin2, B1);
digitalWrite(pin3, B1);
digitalWrite(pin4, B0);
digitalWrite(pin5, B1);
digitalWrite(pin6, B1);
digitalWrite(pin7, B1);
digitalWrite(gnd1, B0);
digitalWrite(gnd2, B1);
delay(10); // Writes 04 to the display.
digitalWrite(pin1, B0);
digitalWrite(pin2, B0);
digitalWrite(pin3, B1);
digitalWrite(pin4, B1);
digitalWrite(pin5, B1);
digitalWrite(pin6, B0);
digitalWrite(pin7, B1);
digitalWrite(gnd1, B1);
digitalWrite(gnd2, B0);
delay(10);

}
for (int i=0; i<timer; i++){
digitalWrite(pin1, B1);
digitalWrite(pin2, B1);
digitalWrite(pin3, B1);
digitalWrite(pin4, B0);
digitalWrite(pin5, B1);
digitalWrite(pin6, B1);
digitalWrite(pin7, B1);
digitalWrite(gnd1, B0);
digitalWrite(gnd2, B1);
delay(10); // Writes 03 to the display.
digitalWrite(pin1, B0);
digitalWrite(pin2, B1);
digitalWrite(pin3, B1);
digitalWrite(pin4, B1);
digitalWrite(pin5, B0);
digitalWrite(pin6, B1);
digitalWrite(pin7, B1);
digitalWrite(gnd1, B1);
digitalWrite(gnd2, B0);
delay(10);

}
for (int i=0; i<timer; i++){
digitalWrite(pin1, B1);
digitalWrite(pin2, B1);
digitalWrite(pin3, B1);
digitalWrite(pin4, B0);
digitalWrite(pin5, B1);
digitalWrite(pin6, B1);
digitalWrite(pin7, B1);
digitalWrite(gnd1, B0);
digitalWrite(gnd2, B1);
delay(10); // Writes 02 to the display.
digitalWrite(pin1, B1);
digitalWrite(pin2, B1);
digitalWrite(pin3, B0);
digitalWrite(pin4, B1);
digitalWrite(pin5, B0);
digitalWrite(pin6, B1);
digitalWrite(pin7, B1);
digitalWrite(gnd1, B1);
digitalWrite(gnd2, B0);
delay(10);

}
for (int i=0; i<timer; i++){
digitalWrite(pin1, B1);
digitalWrite(pin2, B1);
digitalWrite(pin3, B1);
digitalWrite(pin4, B0);
digitalWrite(pin5, B1);
digitalWrite(pin6, B1);
digitalWrite(pin7, B1);
digitalWrite(gnd1, B0);
digitalWrite(gnd2, B1);
delay(10); // Writes 01 to the display.
digitalWrite(pin1, B0);
digitalWrite(pin2, B0);
digitalWrite(pin3, B1);
digitalWrite(pin4, B0);
digitalWrite(pin5, B0);
digitalWrite(pin6, B0);
digitalWrite(pin7, B1);
digitalWrite(gnd1, B1);
digitalWrite(gnd2, B0);
delay(10);

}
for (int i=0; i<timer; i++){
digitalWrite(pin1, B1);
digitalWrite(pin2, B1);
digitalWrite(pin3, B1);
digitalWrite(pin4, B0);
digitalWrite(pin5, B1);
digitalWrite(pin6, B1);
digitalWrite(pin7, B1);
digitalWrite(gnd1, B0);
digitalWrite(gnd2, B1);
delay(10); // Writes 00 to the display.
digitalWrite(pin1, B1);
digitalWrite(pin2, B1);
digitalWrite(pin3, B1);
digitalWrite(pin4, B0);
digitalWrite(pin5, B1);
digitalWrite(pin6, B1);
digitalWrite(pin7, B1);
digitalWrite(gnd1, B1);
digitalWrite(gnd2, B0);
delay(10);

}
digitalWrite(pled2, HIGH);
digitalWrite(pled1, LOW);
delay(75);
digitalWrite(pled1, HIGH);
delay(500);
digitalWrite(pled1, LOW);

for(i=0;i<2;i++)
{
for(value = 0 ; value <= 255; value+=5) // fade in (from min to max)
{
analogWrite(gnd1, value); // sets the value (range from 0 to 255)
analogWrite(gnd2, value); // sets the value (range from 0 to 255)
delay(10); // waits for 30 milli seconds to see the dimming effect
}
for(value = 255; value >=0; value-=5) // fade out (from max to min)
{
analogWrite(gnd1, value); // sets the value (range from 0 to 255)
analogWrite(gnd2, value); // sets the value (range from 0 to 255)
delay(10);
}
}

// delay(10000);

//delay(2000);
digitalWrite(led3, LOW);
digitalWrite(led1, HIGH);
rumple=0;

}
}
// do other stuff while time is passing
}
}
// THANKS IN ADVANCE