hi! hope that you can help me ![]()
Im making a project with a ESP8266 Wemos D1 Mini. This is connected to a neopixel led. i see that this led have 3 pins but i havent this led. the conection is the next:
Solder the 5v jumper to 5v, the GND jumper to GND, and the Data jumper to D1 on the microcontroller.
https://content.instructables.com/ORIG/ … 46617d7f60
but I want to connected the ESP to a lilypad leds. is possible? how can i connect? the lilypad leds have 2 pins + and -, but dont have D1.
i know that the neopixel led can change the colour but the lilypad have just one color, it dont matter, i just want to change the frequency for make a secuence like 1 second on ,1 second off, 2 seconds on, 2 seconds off…
thankyou! ![]()