Good afternoon~brothers
I’m coming again.Would you like to know which question I brought? :dance: OK, let’s go into the subject.
I learn NRF24L01 not long ago.Recently I am confusing about this question a long time when I’m adjusting program.I hope I can find the answer from this forum.
I send the program according to the adjusting way–disability response,disabled automatic retransmission and receive channel 0 in the disability. If it can send successfully the STATUS should be 0*2e (46), there are not problem.
However! ! The another fifo_status should be 011,but here just 001, what mean that TX_FIFO is no empty…so I add spi_rw_reg(flush_tx,0) which set before delivery mode when I sent the program.II have try it even add it in the main function, , , , , , Unfortunately,It’s always 0*01.I have no choice. What I can do is post it to the forum and I hope there are manipulators to help me. :doh:
Thank you for taking time to reading my questions,all your advice will be appreciated!
Wishes!