Hi,
I have followed the tutorial to make a DYI GNSS reference station with an ESP32 and this works well. (https://learn.sparkfun.com/tutorials/ho … p-option-2)
However, I would like to modify the .ino code for the NTRIP server on the ESP32, so it starts automatically without needing a key input.
I fail to understand how, or why it even waits for a key input as there isn’t any function like cin.get() in c++ or getchar() in c, etc.
I’m looking specifically at this piece of code:
void loop()
{
if (Serial.available())
beginServing();
Serial.println(F("Press any key to start serving"));
delay(1000);
}
I have looked through the beginServing function as well and couldn’t find anything regarding keystrokes, besides another line printing
Serial.println("User pressed a key");
Serial.println("Disconnecting...");
ntripCaster.stop();
You can find the whole code here: https://github.com/sparkfun/SparkFun_u- … Server.ino
I have researched beforehand and found this thread on the arduino forums: https://forum.arduino.cc/t/pause-a-sket … d/495039/7
Does this mean I just need to flush and do Serial.read() to get it running with manual input?
→ I’m looking for a way to automatically start the NTRIP server on a ESP32 which is connected to a ZED-F9P, once it has power.
Please excuse the question if this sounds silly, I don’t usually program arduino ![]()
Thanks in advance ![]()
John