How to communicate with LPC-E2294 BootLoader ?

Hi,

I am using LPC-E2294 board and have a question regarding how to communicate with BootLoader.

I set Jumper 1 (JRST) and Jumper 2 (BSL) to Enable ICSP programming, then i connect it to on board RS232 port (i think it is UART1) to talk to LPC flash utility v2.2.1, it doesn’t work !

Should I use UART0, but it is used by USB, is that the problerm ? Thanks.

Daniel

the bootloader is on UART0 which is connected to the USB converter

you should assign the virtual com port number to Philips ISP

Tsvetan