I want to create library files (.a) of the arduino core library, eventually also the other libraries (SPI, …), with a makefile, but I can’t get it to work!
This is my makefile:
CC=avr-gcc
CPP=avr-g++
MCU=-mmcu=atmega328p
CPU_SPEED=-DF_CPU=16000000UL
CFLAGS=$(MCU) $(CPU_SPEED) -g2 -gstabs -Os -Wall \
-ffunction-sections -fdata-sections -fno-exceptions
INCLUDE=-I./arduinoCORE
CFILES=$(wildcard ./arduinoCORE/*.c)
CPPFILES=$(wildcard ./arduinoCORE/*.cpp)
OBJ=$(CFILES:.c=.o) $(CPPFILES:.cpp=.o)
default: $(OBJ)
avr-ar -r libarduinoUNO.a $^
%.o : %.c
$(CC) $< $(CFLAGS) -c -o $@
%.o : %.cpp
$(CPP) $< $(CFLAGS) -c -o $@
(all header and source files are in arduinoCORE; even pins_arduino.h)
After $ make in directory above arduinoCORE I get this error message:
avr-g++ arduinoCORE/CDC.cpp -mmcu=atmega328p -DF_CPU=16000000UL -g2 -gstabs -Os -Wall -ffunction-sections -fdata-sections -fno-exceptions -c -o arduinoCORE/CDC.o
In file included from arduinoCORE/Print.h:27:0,
from arduinoCORE/Stream.h:26,
from arduinoCORE/HardwareSerial.h:28,
from arduinoCORE/Arduino.h:193,
from arduinoCORE/Platform.h:15,
from arduinoCORE/CDC.cpp:19:
arduinoCORE/Printable.h:23:17: fatal error: new.h: No such file or directory
#include <new.h>
^
compilation terminated.
make: *** [arduinoCORE/CDC.o] Error 1
The problem is, that new.h is actually in arduinoCORE! Does anyone know how to manage this?