Ok, I have returned with more ideas…First, try this more reliable upload procedure:
- In the Arduino IDE, click the “Upload” button first
- Wait until you see “Waiting for upload port…” in the console
- Only then double-click the reset button on the board
- The upload should complete before the bootloader times out
If that doesn’t work, we can try a more aggressive approach:
- Open Terminal
- Run:
ls -l /dev/tty.usb*to confirm no board is present - Create a loop to watch for the device:
bash
while true; do ls /dev/tty.usb*; sleep 0.5; done
- In another Terminal window, prepare this command but don’t run it yet:
bash
/Users/zach/Library/Arduino15/packages/arduino/tools/avrdude/6.3.0-arduino17/bin/avrdude -C/Users/zach/Library/Arduino15/packages/arduino/tools/avrdude/6.3.0-arduino17/etc/avrdude.conf -v -patmega32u4 -cavr109 -P/dev/tty.usbmodem5101 -b57600 -D -Uflash:w:[YOUR_HEX_FILE_PATH]:i
- Double-press the reset button
- As soon as you see the device appear in the first Terminal window, quickly run the avrdude command in the second window
If these methods don’t work, we can try:
- If available, trying a different computer to rule out OS-specific issues
- Upload Workaround**
bash
# Terminal command to force persistent port recognition
screen /dev/cu.usbmodem5101 1200
Run this immediately after resetting the board to keep the port active