how to load binary from SD card in Artemis board ?

how i can load new binary file in boot section of Artemis ATP from external SD card using Arduino IDE ?

To load new code onto your Artemis module using the Ambiq bootloader toolchain.

Select the Ambiq Secure Bootloader option in the Arduino Tools —> Bootloader menu. These tools will modify your binary and package them with various security headers.

The code will load at 115200bps and may fail. Hit upload again if the process fails.

You can not load code into the Artemis ATP via uSD, you must upload it serially from the Arduino IDE.

Hello! I’m looking into making a TASbot implementation on the ESP32 for the Sega Genesis. I essentially have a ~200kb binary “input file” of just raw 2 byte values that I want to be able to #include at compile time somehow so the ESP32 to be able to use 2 bytes of it at a time during runtime. This way, one could swap out the input file for another one and reupload it with the sketch. I know serial/SD card are options, but I’d rather avoid the extra hardware.

Any ideas?

[www.myaarpmedicare.com login](https://www.myaarpmedicare.work/)

@Bergstrom

What does this have to do with loading code onto a Artemis?