How to update GNSS Flex pHAT - ZED-X20P firmware with u-center 2

I tried to follow the u-blox guide on YouTube to update firmware. The guide was created for the u-blox EVK-X20P evaluation kit, so I tried to follow it the best I could. I can’t get it to work.

I connected the USB-C port on the pHat to a USB-A port on my laptop running Windows 11. I can receive satellites. When I try to update firmware, I get a warning after a few seconds that COM5 is disconnected. I see more error messages, and then an traceback for an uncaught JavaScript exception. The only way I can reconnect is to power down the Pi completely and restart.

How can I update my X20P firmware?

Hi Steve (@steve.talent ),

The ZED-X20P can only be updated via UART1. Sadly, it is not possible to update via its built-in USB port. This is a quirk of the X20P, other u-blox modules can be updated via USB.

The easiest solution is to buy the new Flex Breakout - at the link below - transfer your ZED-X20P Flex module to that and update using the “UART” USB connection. Channel A of the CH342 provides direct access to the ZED UART1.

It is possible to update the X20P while it is mounted on the pHAT, but it is much more involved:

  • Remove the pHAT from the Raspberry Pi
  • Connect pHAT USB-C to a power source (computer port, wall wart or battery pack)
  • Use a male-male jumper wire to link the 2x20-way GPIO header Pin 2 (5V) to Pin 1 (normally 3.3V)
    • This enables the main 3.3V regulator on the pHAT, providing 3.3V power to the ZED
    • Don’t connect anything to Pin 17 (normally 3.3V) as this will now be 5V
  • Use a 3.3V FTDI USB-UART cable or breakout and jumper wires to interface to:
    • GPIO Pin 8 (normally GPIO14/TXD) : this is connected to ZED RXD1
    • GPIO Pin 10 (normally GPIO15/RXD) : this is connected to ZED TXD1
    • GPIO Pin 6 : GND

Sorry for the inconvenience. Let me know if you need more help - or diagrams.

Best wishes,
Paul

I have a similar question: what are the steps to update the firmware for the GPS-28962?

Hi @eizo ,

GPS-28962 is the GNSS Flex Breakout. Which GNSS Flex Module do you want to upgrade? The ZED-X20P (GPS-29362) - or another one?

If it is the ZED-X20P (GPS-29362):

  • The procedure is almost the same as shown in the u-blox video for the EVK-X20P - link below
  • The GNSS Flex Breakout uses a CH342 USB-UART interface chip
  • Connect your PC to the “UART” USB-C connector on the Breakout
  • The ZED-X20P UART1 is connected to the CH342 Channel A
  • UART1 defaults to 38400 Baud
  • If needed, the official CH342 drivers can be downloaded at the second link below

I hope this helps. Let us know if you need more information.

Best wishes,
Paul

The correct model is GPS-28871.

Is the update procedure the same for this model?

Hi @eizo ,

On GPS-28871, you need to connect a 3.3V “FTDI” (USB-UART) cable or breakout to the UART1 breakout pins and perform the upgrade using that. Please see the suggestions below.

It is not possible to upgrade over the X20P’s built-in USB connection. The USB-C connector on GPS-28871 can not be used for firmware upgrades.

  • It is OK to power the GPS-28871 via the USB-C for the upgrade
  • Connect GND on the X20P Breakout to GND / 0V on your FTDI Breakout
  • Connect TX1 on the X20P Breakout to the RX In pin on your FTDI Breakout
  • Connect RX1 on the X20P Breakout to the TX Out pin on your FTDI Breakout

The FTDI chip will appear as a COM port in u-center. Connect at 38400 Baud. Then follow the procedure in the video to upgrade.

I hope this helps,
Paul

SparkFun Beefy 3 - FTDI Basic Breakout

SparkFun Serial Basic Breakout - CH340C and USB-C
Two products are introduced, but can both be updated using the same operations?

Hi @eizo ,

Both will work for the Firmware upgrade. The only differences are price, drivers and connectors. You may need to install different drivers for the FTDI Breakout (micro-B) vs. the CH340C Breakout (USB-C).

You should be able to use any 3.3V USB-UART converter. Those are the two I would recommend from SparkFun.

Best,
Paul

Just to follow-up on this, and only for interest:

It is possible to update the X20P via I2C. But, you need a board to act as the USB to I2C interface, emulating a UART interface. And you need to be careful with the I2C bus speed and hence the emulated Baud rate. The following worked for me:

void setup()
{

    delay(2000); // Wait for ESP32 and GNSS to start up

    mySerial.begin(38400); // Baud rate for u-center

    myWire.begin();          // Start I2C
    myWire.setClock(100000); // 100kHz
  • Connect the Thing Plus to your Windows PC over USB
  • Upload the modified sketch onto the Thing Plus - using the Arduino IDE
  • Use a Qwiic cable to connect the Thing Plus to the X20P Breakout
  • Be careful with I2C pull-ups. The X20P has built-in active pull-ups on the I2C bus. Additional external pull-ups can cause problems.
  • If you open a serial console / terminal emulator at 38400 Baud, you should see the standard NMEA stream from the X20P. You may need to reset the ESP32 before you see any NMEA. Close the serial console / terminal emulator afterwards!
  • Run the u-blox UBX Firmware Update executable (ubxfwupdate.exe) from a command prompt. ubxfwupdate.exe is installed with u-center.
  • I have the Thing Plus connected as COM10. I called ubxfwupdate.exe with:
"C:\Program Files (x86)\u-blox\u-center_v25.03\ubxfwupdate.exe" -p \\.\COM10 -b 38400:38400:38400 --no-fis 1 -s 1 -v 2 --fast 1 --max-num 1 -C 1 -t 0 "C:\Users\pc235\Documents\GNSS\UBX_20_HPG_202_ZED_F20P.329facb56ce18631d607fe15177834dc.bin"
  • The update takes about 5 minutes to complete:
----------CMD line arguments-----------
Image file:        C:\Users\pc235\Documents\GNSS\UBX_20_HPG_202_ZED_F20P.329facb56ce18631d607fe15177834dc.bin
Flash:             <compiled-in>
Fis:               flash.xml
Port:              \\.\COM10
Baudrates:         38400/38400/38400
Safeboot:          1
Reset:             1
AutoBaud:          0
Verbose:           2
Erase all:         1
Erase only:        0
Training sequence: 0
Chip erase:        1
Merging FIS:       1
Update RAM:        0
Use USB alt:       0
---------------------------------------
  0.0 u-blox Firmware Update Tool version 24.11
  0.0 Updating Firmware 'C:\Users\pc235\Documents\GNSS\UBX_20_HPG_202_ZED_F20P.329facb56ce18631d607fe15177834dc.bin' of receiver over '\\.\COM10'
  0.0   - Opening and buffering image file
  0.0   - Verifying image
  0.0   - Got an encrypted image with footer info
  0.0   - CRC Value             :    737F7768
  0.0   - Footer Version        :    1
  0.0   - Number of Images      :    2
  0.0   - Footer Size           :    28
  0.0   - Image Config Size     :    40
  0.0   - Image 0 Size          :    668336
  0.0   - Image 1 Size          :    426320
  0.0   - Trying to open port \\.\COM10
  0.0   - Setting baudrate to 38400
  0.3   - Received Version information
  0.3   - Receiver currently running SW 'ROM LDR 1.00 (d225d8)'
  0.3   - Receiver HW '000B0000', Generation 20.0
  0.3   - Sending ROM CRC Poll
  0.3 ROM CRC: 0x22018AE9
  0.3 u-blox20 ROM1.00 hardware detected (0x22018AE9)
  0.3  Getting Port connection to receiver
  2.2   - Connected port is: I2C
  2.2  Starting LDR TSK
  2.2   - LDR TSK started successfully
  2.2  Identify flash loader
  2.3   - Uploader version 5.3 detected
  2.3  Detecting Flash manufacturer and device IDs
  2.3   - Flash ManId: 0x009D DevId: 0x6016
  2.4   - Not merging anything
  2.4   - Flash size:   4194304
  2.4   -  Flash block:  1024 x 4096
  2.4 Stable clock enabled successfully
  2.5   - Setting baudrate to 38400
  2.8  Start Flash retention
  3.9   - flash retention success
  3.9 Chip erase started
  3.9  Receiver info collected, downloading to flash...

WWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWW
WWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWW
WWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWW
WWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWW
WWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWW
WWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWW
WWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWW
WWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWWW
max retries: e: 0(  0) w: 0(  0)
311.2 FW download complete
311.2  Verifying Image on hardware
313.6  Firmware Verification and Flash update complete
313.6  Verify Flash retention
313.6  flash retention success
313.6  Rebooting receiver
313.6 Firmware Update SUCCESS

313.6   - Transfer time duration: 313.639404 sec

Like I say, this is purely for interest. I’m not recommending you update your X20P this way. I’m just saying that it is possible. It could be useful if I2C is your only option.

If anything goes wrong during the update, turn the GNSS off and back on again, and start again. The process is very robust. The GNSS will only apply the firmware update if it passes verification.

Enjoy!
Paul

Thank you very much. I followed your advice exactly and the update was successful.

This turned out to be quite convoluted

at least with 2.0.0 firmware, USB upgrade doesn’t seem to work
can’t get ESP32 as USB to UART to complete the upgrade as the process requires changing baud rate / training sequence which gets tricky when you need to manage both baud to esp32 and to X20P
and per integration manual, you need to put it in safeboot mode (`-s 1`, no such option in the ucenter2 UI) for firmware upgrade (otherwise keep getting flash retention related errors)