Did you have a fix on this issue? I have the same problem with Facing same issue but no response from anyone and couldnt find this topic troubleshooting in google.MaverickThomas:
I have got a sparkfun edge board and a redboard. i have tried the examples codes from ambiq sdk and sparkfun example tensorflow on edge board using the given python scripts and it was working fine.Now i want to try the same examples from ambiq sdk(i2c, ble…) on the redboard but unable to upload the firmware using the sparkfun uart_wired_update_sparkfun.py i have also tried the ambiq wired update script but couldn’t update it. (As edge board and red board have different bootloaders)
i have also tried arduino to upload and it was working, so i have used artemis_svl.py script from the .arduino15 to program using the makefile but some port issues are coming.
${PROGRAMMER_SCRIPT} -b 115200 -f $(CONFIG)/main_nonsecure_wire.bin -v -t 0.50 $(SERIAL_PORT)