Okay I think I’m going to just use the adafruit trinket + servo + switch + Battery (w/inline spst to shut off for storage), and then use the micro + lcd + volmtetering. So i need to cut the code in 2 now… i think i can do this myself, just saying. I could also go the powered usb hub but i mean that would mean buying extra stuff, it’s not really cheaper than just using a trinket that i already have. it is tempting but it’s not promised that it works and damn this has taken way too long.
code for lcd + micro just run plainly off usb:
#include <LiquidCrystal.h>
//declare the constants to be used
#define LEDPIN 13 //pin attached to LED
#define servoPIN 9 //Servo control line
#define SWitchPIN 2 //input from N.O. momentary switch
#define redPIN 10 //PWM pin for red LED backlight
#define greenPIN 11 //PWM pin for green LED backlight
#define bluePIN 12 //PWM pin for blue LED backlight
#define rsPIN 8 //reset pin for LCD
#define enablePIN 3 //enable pin for LCD
#define d4PIN 4 //data pin4 for LCD
#define d5PIN 5 //data pin5 for LCD
#define d6PIN 6 //data pin6 for LCD
#define d7PIN 7 //data pin7 for LCD
// these constants won't change. But you can change the size of
// your LCD using them:
const int numRows = 4;
const int numCols = 20;
const int ignoreMAX = 6; //ignore this many characters
const unsigned long wait = 50;//wait time for ADC update after last Smartie cmd
#define posOpenCMD 1900 //Define Clockwise Servo position in usec
#define posCloseCMD 600 //Define CounterClockwise Servo position in usec
#define DBdelay 2000 //Min time needed btw any 2 button presses, in msec
#define fastSPD 100 //speed setting; 1 = slowest, 255 is fastest (???)
#define slowSPD 15 //Speed Servo/Door opens and closes (15 is good average)
#define DIV_1 1.0 //gain correction for A0 channel
#define DIV_2 1.0 //note it's 1.0, not 1, to get full floating point accuracy
#define V_REF 2.61 //use the measured Aref voltage
//declare the variables used
boolean updateFlag = false; //flag to refresh ADC readings
volatile boolean doorOPEN = false; //desired door state set to closed
byte rxbyte = 0; //rxbyte is the received byte from Smartie
byte temp = 0;
int ignoreCNT = 0; //count of characters to ignore
int row = 0; //index of last row position
int col = 0; //index of last col position
int rowA0 = 0; //index of A0 row position
int colA0 = 0; //index of A0 col position
int rowA1 = 0; //index of A1 row position
int colA1 = 0; //index of A1 col position
unsigned long MSGtime = 0; //holds the time of the last cursor cmd
volatile unsigned long SWtime = 0; //holds the time of the last valid switch push
float voltage1 = 0.0; // calculated voltage for A0
float voltage2 = 0.0; // calculated voltage for A1
LiquidCrystal lcd(rsPIN, enablePIN, d4PIN, d5PIN, d6PIN, d7PIN);
void setup() {
//set the pins to be ins or outs
pinMode(LEDPIN, OUTPUT);
digitalWrite(LEDPIN, LOW); //turn LED off
pinMode(servoPIN, OUTPUT);
pinMode(SWitchPIN, INPUT_PULLUP);
pinMode(redPIN, OUTPUT);
pinMode(greenPIN, OUTPUT);
pinMode(bluePIN, OUTPUT);
Serial.begin(9600);
lcd.begin(numCols, numRows);
delay(50);
lcd.clear();
delay(5);
analogWrite(bluePIN,0); //Blue brightness 255-0
analogWrite(redPIN,255); //Red brightness 255-0
analogWrite(greenPIN,255); //Green brightness 255-0
analogReference(INTERNAL); //use the internal 2.56v ADC reference
//put a hello world on the LCD
lcd.print("Line 1");
lcd.setCursor(3, 1);
lcd.print("Line 2");
lcd.setCursor(8, 2);
lcd.print("Line 3");
lcd.setCursor(13, 3);
lcd.print("Line 4");
delay(2000);
}
//this function is used by the smartie code to get data from the PC
byte serial_getch(){
int incoming;
while (Serial.available()==0){
//check to see if enough time has passed since last message from PC
if((millis() - MSGtime > wait) && (updateFlag == true)){
updateADC();
}
}
// read the incoming byte:
incoming = Serial.read();
return (byte) (incoming &0xff);
}
//this function will update the ADC readings if the [ or ] have been sent
void updateADC(){
updateFlag = false;
if(colA0 > 0){
voltage1 = DIV_1 * float(analogRead(A0)) * V_REF/1023.0;
lcd.setCursor(colA0, rowA0);
lcd.print(voltage1, 3);
}
if(colA1 > 0){
voltage2 = DIV_2 * float(analogRead(A1)) * V_REF/1023.0;
lcd.setCursor(colA1, rowA1);
lcd.print(voltage2, 3);
}
}
//the main loop is now just the hacked version of the Arduino Smartie code
void loop(){
rxbyte = serial_getch(); //this calls the 'function' serial_getch(), stores result in rxbyte
if (rxbyte == 254) //Matrix uses 254 for commands, if rxbyte = 254 the the code below runs
{
ignoreCNT == 0; //turn off character ignoring whenever a command is sent
switch (serial_getch()) //calls serial_getch() to get the next byte from the PC
{
case 66: //former backlight on command
break;
case 70: //former backlight off command
break;
case 71: //set cursor position
MSGtime = millis(); //remember time that cursor cmd was sent
updateFlag = true; //set flag to update ADC readings
row = 0;
col = 0;
temp = (serial_getch() - 1); //get column byte
switch (serial_getch()) //get row byte
{
//line 1 is already set up
case 2:
row = 1;
temp += 0x40;
break;
case 3:
row = 2;
temp += 0x14;
break;
case 4:
row = 3;
temp += 0x54;
break;
default:
break;
}
lcd.command(0b10000000 + temp);
break;
case 72: //cursor home (reset display position)
lcd.command(2);
break;
case 74: //show underline cursor
lcd.command(0b00001110);
break;
case 75: //underline cursor off
case 84: //block cursor off
lcd.command(0b00001100);
break;
case 76: //move cursor left
lcd.command(16);
break;
case 77: //move cursor right
lcd.command(20);
break;
case 78: //define custom char
lcd.command(64 + (serial_getch() * 8)); //get+set char address
for (temp = 7; temp != 0; temp--)
{
lcd.print(serial_getch()); //get each pattern byte
}
break;
case 83: //show blinking block cursor
lcd.command(0b00001111);
break;
case 86: //GPO OFF
//implement later
break;
case 87: //GPO ON
/*temp = serial_getch();
if (temp == 1)
{
GPO1 = GPO_ON;
}*/
break;
case 88: //clear display, cursor home
lcd.command(1);
break;
case 152: //set and remember (doesn't save value, though)
case 153: //set backlight brightness
//not implemented
break;
//these commands ignored (no parameters)
case 35: //read serial number
case 36: //read version number
case 55: //read module type
case 59: //exit flow-control mode
case 65: //auto transmit keypresses
case 96: //auto-repeat mode off (keypad)
case 67: //auto line-wrap on
case 68: //auto line-wrap off
case 81: //auto scroll on
case 82: //auto scroll off
case 104: //init horiz bar graph
case 109: //init med size digits
case 115: //init narrow vert bar graph
case 118: //init wide vert bar graph
break;
default:
//all other commands ignored and parameter byte discarded
temp = serial_getch(); //dump the command code
break;
}
return;
} //END OF COMMAND HANDLER
//change accented char to plain, detect and change descenders
//NB descenders only work on 5x10 displays. This lookup table works
// with my DEM-20845 (Display Elektronik GmbH) LCD using KS0066 chip.
switch (rxbyte)
{
//chars that have direct equivalent in LCD charmap
/* case 0x67: //g
rxbyte = 0xE7;
break;
case 0x6A: //j
rxbyte = 0xEA;
break;
case 0x70: //p
rxbyte = 0xF0;
break;
case 0x71: //q
rxbyte = 0xF1;
break;
case 0x79: //y
rxbyte = 0xF9;
break;
*/
case 0x5B: //Formerly [, now does A0 ADC
voltage1 = DIV_1 * float(analogRead(A0)) * V_REF/1023.0;
lcd.print(voltage1, 3);
rxbyte = 0x76; //will cause v to be displayed
ignoreCNT = ignoreMAX; //ignore characters replaced by ADC reading
updateFlag = false; //reset ADC update flag
rowA0 = row; //store row of A0 reading
colA0 = col; //store col of A0 reading
break;
case 0x5D: //Formerly ], now does A1 ADC
voltage2 = DIV_2 * float(analogRead(A1)) * V_REF/1023.0;
lcd.print(voltage2, 3);
rxbyte = 0x76; //will cause v to be displayed
ignoreCNT = ignoreMAX; //ignore characters replaced by ADC reading
updateFlag = false; //reset ADC update flag
rowA1 = row; //store row of A1 reading
colA1 = col; //store col of A1 reading
break;
case 0xE4: //ASCII "a" umlaut
rxbyte = 0xE1;
break;
case 0xF1: //ASCII "n" tilde
rxbyte = 0xEE;
break;
case 0xF6: //ASCII "o" umlaut
rxbyte = 0xEF; //was wrong in v0.86
break;
case 0xFC: //ASCII "u" umlaut
rxbyte = 0xF5;
break;
//accented -> plain equivalent
//and misc symbol translation
case 0xA3: //sterling (pounds)
rxbyte = 0xED;
break;
/* case 0xB0: //degrees symbol
rxbyte = 0xDF;
break;
*/
case 0xB5: //mu
rxbyte = 0xE4;
break;
case 0xC0: //"A" variants
case 0xC1:
case 0xC2:
case 0xC3:
case 0xC4:
case 0xC5:
rxbyte = 0x41;
break;
case 0xC8: //"E" variants
case 0xC9:
case 0xCA:
case 0xCB:
rxbyte = 0x45;
break;
case 0xCC: //"I" variants
case 0xCD:
case 0xCE:
case 0xCF:
rxbyte = 0x49;
break;
case 0xD1: //"N" tilde -> plain "N"
rxbyte = 0x43;
break;
case 0xD2: //"O" variants
case 0xD3:
case 0xD4:
case 0xD5:
case 0xD6:
case 0xD8:
rxbyte = 0x4F;
break;
case 0xD9: //"U" variants
case 0xDA:
case 0xDB:
case 0xDC:
rxbyte = 0x55;
break;
case 0xDD: //"Y" acute -> "Y"
rxbyte = 0x59;
break;
/* case 0xDF: //beta //mucks up LCDSmartie's degree symbol??
rxbyte = 0xE2;
break;
*/
case 0xE0: //"a" variants except umlaut
case 0xE1:
case 0xE2:
case 0xE3:
case 0xE5:
rxbyte = 0x61;
break;
case 0xE7: //"c" cedilla -> "c"
rxbyte = 0x63;
break;
case 0xE8: //"e" variants
case 0xE9:
case 0xEA:
case 0xEB:
rxbyte = 0x65;
break;
case 0xEC: //"i" variants
case 0xED:
case 0xEE:
case 0xEF:
rxbyte = 0x69;
break;
case 0xF2: //"o" variants except umlaut
case 0xF3:
case 0xF4:
case 0xF5:
case 0xF8:
rxbyte = 0x6F;
break;
case 0xF7: //division symbol
rxbyte = 0xFD;
break;
case 0xF9: //"u" variants except umlaut
case 0xFA:
case 0xFB:
rxbyte = 0x75;
break;
default:
break;
}
if(ignoreCNT > 0){
ignoreCNT--;
}
if(ignoreCNT == 0){
col++; //increment column position counter
lcd.write(rxbyte); //otherwise a plain char so we print it to lcd
}
}
So my problem right now is that the VCORE and VRIN values ([ and ] as the placeholders i believe) are showing wack values. They fluctuate, but they are not accurate.
I dont remember which is which, but [ and ] show ~1.692 and 1.602 respectively while VRIN and VCORE are really at 0.744v and 1.788v (verified with voltmeter). I measured VREF and it’s at 2.61, which I changed in the code above. So I don’t know why the voltmeter is wacked out.
I think there’s some code in there leftover for the servo and servo interrupt detection and turning off the lcd when power is not on analgoue 3 that are still in that code but I think these are easily solvable problems!